<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC9S08QG8 SPI Interface to 3 1/2 Dight Display in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143019#M6461</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello John,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Another approach is to use a shift register device (e.g. 74HC595 or 74HC164) to provide the interface between the SPI, and an alphanumeric LCD display operating in 4-bit mode.&amp;nbsp; If the display is required during development and test only, I assume the shift register and display would be part of a "test jig".&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Each shift register type would require a slightly different approach, but you will need one further output signal from the MCU, in addition to the three signals associated with the SPI bus.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Yet another approach&amp;nbsp;would be to&amp;nbsp;incorporate an additional MCU within the test jig, to provide the&amp;nbsp;SPI&amp;nbsp;interface.&amp;nbsp; This will eliminate much of the additional code, required for the LCD communications and formatting, from the QG8 device within the equipment.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Aug 2007 10:42:05 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2007-08-15T10:42:05Z</dc:date>
    <item>
      <title>MC9S08QG8 SPI Interface to 3 1/2 Dight Display</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143016#M6458</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi Group,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I am designing a motor control application using the MC9S08QG8 utializing the SPI Interface.&lt;/DIV&gt;&lt;DIV&gt;Can someone recommed a 3 1/2 Digit LCD display component with an SPI interface?&lt;/DIV&gt;&lt;DIV&gt;Is there some example code available?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;John&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Aug 2007 20:31:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143016#M6458</guid>
      <dc:creator>JohnB3</dc:creator>
      <dc:date>2007-08-14T20:31:56Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08QG8 SPI Interface to 3 1/2 Dight Display</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143017#M6459</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Dear John,&lt;/DIV&gt;&lt;DIV&gt;what do you intend for 3 1/2 digit display? It's only a numeric display? How big must it be and which technology?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I think that any SPI interfaced display is a quite exotic one: i.e. very few models and&amp;nbsp;rather costly.&lt;/DIV&gt;&lt;DIV&gt;Have you considered using a standard low-cost alphanumeric display? There are hundreds of models to chose from and many are surprisingly cheap, with the advantage of permitting display of a full text string in addition to simple numbers.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;You can use a nibble driver approach needing only 7 gp I/O lines, i.e. less than 1 full 8-bit port with a moderate software increased difficulty or a&amp;nbsp;full byte driver, with a simpler approach and 11 I/O lines needed.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If your 9S08QG has not enough lines (very easy even with the nibble driver), I suggest to change it in favour of a slightly bigger MCU like an 9S08GT8A, with plenty of I/O lines and a budget price of 1.40$ vs. 1.13$ of the smaller one. The added lines may prove useful to you or not, but the price is very small. And a simple 14 or 16 wires flat cable is&amp;nbsp;all you will need to&amp;nbsp;connect the display to the controller board.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Encoder&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Aug 2007 23:58:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143017#M6459</guid>
      <dc:creator>Encoder</dc:creator>
      <dc:date>2007-08-14T23:58:45Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08QG8 SPI Interface to 3 1/2 Dight Display</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143018#M6460</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;This display will be used during development to didplay various parameters and status information.&amp;nbsp; I am using SPI interface for quad D/A and quad A/D converters to read &amp;amp; control environmental parameters.&amp;nbsp; The SPI serial bus allows for smaller packages in a seriously space cramped application and still allows for fast (enough) data communication for proper control.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I will look at the other microcintroller you suggested for other applications, but I would really like to be able to locate a SPI interface display component for the development.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;John&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Aug 2007 00:23:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143018#M6460</guid>
      <dc:creator>JohnB3</dc:creator>
      <dc:date>2007-08-15T00:23:30Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08QG8 SPI Interface to 3 1/2 Dight Display</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143019#M6461</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello John,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Another approach is to use a shift register device (e.g. 74HC595 or 74HC164) to provide the interface between the SPI, and an alphanumeric LCD display operating in 4-bit mode.&amp;nbsp; If the display is required during development and test only, I assume the shift register and display would be part of a "test jig".&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Each shift register type would require a slightly different approach, but you will need one further output signal from the MCU, in addition to the three signals associated with the SPI bus.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Yet another approach&amp;nbsp;would be to&amp;nbsp;incorporate an additional MCU within the test jig, to provide the&amp;nbsp;SPI&amp;nbsp;interface.&amp;nbsp; This will eliminate much of the additional code, required for the LCD communications and formatting, from the QG8 device within the equipment.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Aug 2007 10:42:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143019#M6461</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2007-08-15T10:42:05Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08QG8 SPI Interface to 3 1/2 Dight Display</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143020#M6462</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi Mac,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks for the suggestions.&amp;nbsp; Both are viable.&amp;nbsp; The shift register suggestion I actually had thought of but put aside until I had heard from folks who might be more familiar with what is out there to use.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The second processor I had not thought of.&amp;nbsp; As you said, this is just for development, I have a spare QG8, and if nothing else shows up at a reasonable price, that may be the way to go.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks for the suggestions.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;John&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Aug 2007 18:19:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143020#M6462</guid>
      <dc:creator>JohnB3</dc:creator>
      <dc:date>2007-08-15T18:19:09Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08QG8 SPI Interface to 3 1/2 Dight Display</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143021#M6463</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi John,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If you add a display to the existing SPI bus then you probably need another CS from the QG.&lt;/DIV&gt;&lt;DIV&gt;If you have a spare pin on the QG then can't you free up the TxD pin and implement an output only RS232 to a dumb terminal emulator on a PC. If this is possible it would be easier within the QG and open up far more possibilities for output over a 3.5 digit display.&lt;/DIV&gt;&lt;DIV&gt;Just a thought!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Aug 2007 18:28:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143021#M6463</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2007-08-15T18:28:09Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08QG8 SPI Interface to 3 1/2 Dight Display</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143022#M6464</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi Peg,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;WOW!&amp;nbsp; Now that is a quantem leap over where my '8-bit-single-board-computer' level brain operates.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I need to go back &amp;amp; look at the design again.&amp;nbsp; The SPI requires certain dedicated pins and I need to use it to talk to the SPI A/D &amp;amp; D/A converters, but I will look at it &amp;amp; see if I have enough brain cells left to grasp how to set up your suggestion.&amp;nbsp; It opens up the possibilities of vastly improved status monitoring, even grapging the ramp, etc.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;John&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Aug 2007 19:18:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143022#M6464</guid>
      <dc:creator>JohnB3</dc:creator>
      <dc:date>2007-08-15T19:18:48Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08QG8 SPI Interface to 3 1/2 Dight Display</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143023#M6465</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;John,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Consider also the MC14499 serial to 7 segment driver.&amp;nbsp; It isn't SPI per se, but it can be easily adapted for use with an SPI interface.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Mitch&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Aug 2007 18:41:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143023#M6465</guid>
      <dc:creator>MidonDesign</dc:creator>
      <dc:date>2007-08-17T18:41:52Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08QG8 SPI Interface to 3 1/2 Dight Display</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143024#M6466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Thanks, Mitch.&lt;/DIV&gt;&lt;DIV&gt;I'll check it out.&lt;/DIV&gt;&lt;DIV&gt;John&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Aug 2007 19:28:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143024#M6466</guid>
      <dc:creator>JohnB3</dc:creator>
      <dc:date>2007-08-17T19:28:24Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08QG8 SPI Interface to 3 1/2 Dight Display</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143025#M6467</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Might be worth having a look at New Japan Radio's range of SPI LCD drivers:-&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;A href="http://www.njr.com/index4.html" rel="nofollow" target="_blank"&gt;http://www.njr.com/index4.html&lt;/A&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Although they don't actually incorporate an LCD, they should drive a standard off the shelf part OK...&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Gary&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Aug 2007 14:43:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143025#M6467</guid>
      <dc:creator>airbusboy20</dc:creator>
      <dc:date>2007-08-29T14:43:07Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08QG8 SPI Interface to 3 1/2 Dight Display</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143026#M6468</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Thanks, Gary.&amp;nbsp; I had not run across this source before.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Aug 2007 23:05:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143026#M6468</guid>
      <dc:creator>JohnB3</dc:creator>
      <dc:date>2007-08-31T23:05:43Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08QG8 SPI Interface to 3 1/2 Dight Display</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143027#M6469</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Check out my project&lt;/DIV&gt;&lt;DIV&gt;&lt;A href="http://www.rasmicro.com/DS18B20.htm" rel="nofollow" target="_blank"&gt;http://www.rasmicro.com/DS18B20.htm&lt;/A&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;for a hardware and software example of exactly this.&lt;/DIV&gt;&lt;DIV&gt;Roger Schaefer&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Sep 2007 23:46:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143027#M6469</guid>
      <dc:creator>RogerSchaefer</dc:creator>
      <dc:date>2007-09-28T23:46:17Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08QG8 SPI Interface to 3 1/2 Dight Display</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143028#M6470</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi&amp;nbsp;Roger,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;This is what I was looking for, but I really appreciate the brainstorming from several others who responded.&amp;nbsp; It served to open my eyes to several posibilities in directions I had never even thought about.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;John&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Sep 2007 00:40:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143028#M6470</guid>
      <dc:creator>JohnB3</dc:creator>
      <dc:date>2007-09-29T00:40:40Z</dc:date>
    </item>
    <item>
      <title>www.rasmicro.com is a great resource for electronicians</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143029#M6471</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hello Roger,&lt;BR /&gt;&lt;BR /&gt;&lt;B&gt;&lt;A href="http://www.rasmicro.com/" rel="nofollow" target="_blank"&gt;http://www.rasmicro.com/&lt;/A&gt;&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;is really a great resource for the electronician. Thank you for sharing this URL &lt;IMG alt=":smileyvery-happy:" class="emoticon emoticon-smileyvery-happy" id="smileyvery-happy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-very-happy.gif" title="Smiley Very Happy" /&gt;&lt;BR /&gt;&lt;BR /&gt;Cheers,&lt;BR /&gt;Alban.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;EDIT: link corrected + signature forgotten&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by Alban on &lt;SPAN class="date_text"&gt;2007-09-28&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;08:06 PM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Sep 2007 02:04:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143029#M6471</guid>
      <dc:creator>Alban</dc:creator>
      <dc:date>2007-09-29T02:04:49Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08QG8 SPI Interface to 3 1/2 Dight Display</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143030#M6472</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is great.&amp;nbsp; It is about at the level I need.&amp;nbsp; This device would be used to debug the development - not part of the final design.&amp;nbsp; I plan to send out 3 digit status and "location" within the program execution, so just a simple set of 3 shift registers and 3 bytes shifted out to drive segments to create the numbers should show the status.&amp;nbsp; Later I may find a use for a small graphics display if I can find a driver IC that will talk SPI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the suggestion.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Oct 2012 19:26:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-SPI-Interface-to-3-1-2-Dight-Display/m-p/143030#M6472</guid>
      <dc:creator>johnbeaty</dc:creator>
      <dc:date>2012-10-04T19:26:43Z</dc:date>
    </item>
  </channel>
</rss>