<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: bigger eval board than DEMO9S08QG8? in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/bigger-eval-board-than-DEMO9S08QG8/m-p/142561#M6283</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Rob,&lt;BR /&gt;&lt;BR /&gt;Due to the same restrictions I have developed my own prototyping board based on the AW60 chip.&lt;BR /&gt;&lt;BR /&gt;Every I/O pin is mapped to the edge connectors and you can optionally switch in the two serial ports via a MAX232, switch in a RS-485 controller and switch in optional driving devices to power and drive a standard LCD module.&lt;BR /&gt;&lt;BR /&gt;You can use almost any xtal - from 32Khz or prefably 9.8304Mhz or even 20Mhz&lt;BR /&gt;&lt;BR /&gt;The BDM connecter is edge-wired seperately&lt;BR /&gt;&lt;BR /&gt;It has an embedded 1A switching supply which can take 9 - 20 VAC input in a "power-over-RS-485" configuration.&lt;BR /&gt;&lt;BR /&gt;Board size is 70 x 95 mm&lt;BR /&gt;&lt;BR /&gt;You are welcome to the design, PCB Gerbers etc.&lt;BR /&gt;&lt;BR /&gt;Let me know&lt;BR /&gt;&lt;BR /&gt;John&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 13 Jan 2007 16:36:02 GMT</pubDate>
    <dc:creator>Jaux</dc:creator>
    <dc:date>2007-01-13T16:36:02Z</dc:date>
    <item>
      <title>bigger eval board than DEMO9S08QG8?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/bigger-eval-board-than-DEMO9S08QG8/m-p/142556#M6278</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hey everybody. I've loved my Axiom DEMO9S08QG8 demo board. Only problem I have right now is I'm running out of I/O for some bigger projects.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've looked at the &lt;/SPAN&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.softecmicro.com%2Fproducts.html%3Ftype%3Ddetail%26title%3DPK-HCS08GB60" rel="nofollow" target="_blank"&gt;softecmicro PK-HCS08GB60 starter kit&lt;/A&gt;&lt;SPAN&gt;. It's also USB, has a row of LEDs, an analog pot, but only one user switch. But there doesn't appear to be a BDM out port to program target parts.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It's based on the MC9S08GB60, so it has four 8-bit ports.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any other suggestions for a bigger, better demo board?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jan 2007 05:43:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/bigger-eval-board-than-DEMO9S08QG8/m-p/142556#M6278</guid>
      <dc:creator>irob</dc:creator>
      <dc:date>2007-01-12T05:43:18Z</dc:date>
    </item>
    <item>
      <title>Re: bigger eval board than DEMO9S08QG8?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/bigger-eval-board-than-DEMO9S08QG8/m-p/142557#M6279</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hi Irob. I think that you hardly will actually find a better demo board than DEMO9S08AW60 for the same price for the 9S08 family.&lt;/P&gt;&lt;P&gt;It has a lot of I/O on board and many leds and pushbuttons to experiment with other than 2 RS232 and USB BDM. Not to talk of the expensive 64 pin QFP socket which would cost you more than the whole board if bought as a spare part and which is invaluable to permit to replace a possibly blown cpu (unfortunately I found the AW60 quite delicate on the ESD side).&lt;/P&gt;&lt;P&gt;Yes, the accelerometer is completely unusefull but the potentiometer and the light sensor may be good. I have at least 6 or 7 HC08xx demo board but I abandoned all them for DEMO9S08AW60 which permits you to work either on 3 or 5V supply environment and, most af all has BDM interface.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Encoder&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jan 2007 17:53:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/bigger-eval-board-than-DEMO9S08QG8/m-p/142557#M6279</guid>
      <dc:creator>Encoder</dc:creator>
      <dc:date>2007-01-12T17:53:39Z</dc:date>
    </item>
    <item>
      <title>Re: bigger eval board than DEMO9S08QG8?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/bigger-eval-board-than-DEMO9S08QG8/m-p/142558#M6280</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;You can unplug the QG8 chip form the DEMO9S08QG8 and use it as a USB-BDM tool. I used that for a BT16A chip that I wired myself. Works greate. The switches, LEDs,&amp;nbsp;photo-detector, etc. on the DEMO9S08QG8 can be used too.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jan 2007 23:51:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/bigger-eval-board-than-DEMO9S08QG8/m-p/142558#M6280</guid>
      <dc:creator>OldMan</dc:creator>
      <dc:date>2007-01-12T23:51:06Z</dc:date>
    </item>
    <item>
      <title>Re: bigger eval board than DEMO9S08QG8?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/bigger-eval-board-than-DEMO9S08QG8/m-p/142559#M6281</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;OldMan, you are right about the QG8 demo board. It's very nice in that there is the BDM port available. That's what I've been using primarily, but recently ran out of I/O.&lt;BR /&gt;&lt;BR /&gt;Encoder, where can I buy an AW60 demo board? That thing sound great!&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 13 Jan 2007 01:19:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/bigger-eval-board-than-DEMO9S08QG8/m-p/142559#M6281</guid>
      <dc:creator>irob</dc:creator>
      <dc:date>2007-01-13T01:19:36Z</dc:date>
    </item>
    <item>
      <title>Re: bigger eval board than DEMO9S08QG8?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/bigger-eval-board-than-DEMO9S08QG8/m-p/142560#M6282</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Depending where you are, you may easily buy it from DigiKey in USA or from Farnell or RS-components in Europe: all they usually have it in stock and you may have it in a couple of days as I did. The price may slightly vary.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;But many other classic distributors like Avnet or Arrow have it. And you may order it&amp;nbsp;also from Freescale Direct Buy Service for 84.99$, but I do not know if its is available in stock.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Informations, electric diagrams, guides&amp;nbsp;and everything&amp;nbsp;are completely available on this Freescale site.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Encoder&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 13 Jan 2007 04:44:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/bigger-eval-board-than-DEMO9S08QG8/m-p/142560#M6282</guid>
      <dc:creator>Encoder</dc:creator>
      <dc:date>2007-01-13T04:44:38Z</dc:date>
    </item>
    <item>
      <title>Re: bigger eval board than DEMO9S08QG8?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/bigger-eval-board-than-DEMO9S08QG8/m-p/142561#M6283</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Rob,&lt;BR /&gt;&lt;BR /&gt;Due to the same restrictions I have developed my own prototyping board based on the AW60 chip.&lt;BR /&gt;&lt;BR /&gt;Every I/O pin is mapped to the edge connectors and you can optionally switch in the two serial ports via a MAX232, switch in a RS-485 controller and switch in optional driving devices to power and drive a standard LCD module.&lt;BR /&gt;&lt;BR /&gt;You can use almost any xtal - from 32Khz or prefably 9.8304Mhz or even 20Mhz&lt;BR /&gt;&lt;BR /&gt;The BDM connecter is edge-wired seperately&lt;BR /&gt;&lt;BR /&gt;It has an embedded 1A switching supply which can take 9 - 20 VAC input in a "power-over-RS-485" configuration.&lt;BR /&gt;&lt;BR /&gt;Board size is 70 x 95 mm&lt;BR /&gt;&lt;BR /&gt;You are welcome to the design, PCB Gerbers etc.&lt;BR /&gt;&lt;BR /&gt;Let me know&lt;BR /&gt;&lt;BR /&gt;John&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 13 Jan 2007 16:36:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/bigger-eval-board-than-DEMO9S08QG8/m-p/142561#M6283</guid>
      <dc:creator>Jaux</dc:creator>
      <dc:date>2007-01-13T16:36:02Z</dc:date>
    </item>
    <item>
      <title>Re: bigger eval board than DEMO9S08QG8?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/bigger-eval-board-than-DEMO9S08QG8/m-p/142562#M6284</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rob&lt;BR /&gt;since i hate the usual demo boards i have developed the HC(S)08 system. The idea is to have a "mainboard" and different modules for your MPU as well as a lot of "addons" to get started with your prototype. I wanted to include a simple OS witch has become my EBS08 as a base for the software (i am using Motorola/freescale MPU for about 20 years now) having a lot of modules beside. Then for every hardware module i have also the schematics as a module, so once i have finished the software and having tested it i do the layout based on my modules. All this save a lot of time and is kind of foolproof! (at least i do the mistakes normally only once!).&lt;BR /&gt;For more infos visit &lt;A href="http://www.systech-gmbh.ch/"&gt;www.systech-gmbh.ch&lt;/A&gt;&lt;SPAN&gt; -&amp;gt; HC(S)08 system for the hardware and -&amp;gt; EBS08 for the software. If you need help ask here or send a mail to &lt;/SPAN&gt;&lt;A class="jive-link-email-small" href="mailto:info@systech-gmbh.ch"&gt;info@systech-gmbh.ch&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Saluti Joerg&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 13 Jan 2007 23:55:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/bigger-eval-board-than-DEMO9S08QG8/m-p/142562#M6284</guid>
      <dc:creator>joerg</dc:creator>
      <dc:date>2007-01-13T23:55:42Z</dc:date>
    </item>
    <item>
      <title>Re: bigger eval board than DEMO9S08QG8?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/bigger-eval-board-than-DEMO9S08QG8/m-p/142563#M6285</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;John, thanks for the kind offer. I sent you a private message.&lt;BR /&gt;&lt;BR /&gt;Joerg, your site has quite a wealth of information. I love your module-based approach to the Freescale MCUs. Very cool. Thanks for the help, everyone!&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jan 2007 00:41:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/bigger-eval-board-than-DEMO9S08QG8/m-p/142563#M6285</guid>
      <dc:creator>irob</dc:creator>
      <dc:date>2007-01-16T00:41:01Z</dc:date>
    </item>
    <item>
      <title>Re: bigger eval board than DEMO9S08QG8?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/bigger-eval-board-than-DEMO9S08QG8/m-p/142564#M6286</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello John,&lt;/FONT&gt;&lt;/DIV&gt;&lt;BLOCKQUOTE dir="ltr"&gt;&lt;DIV&gt;&lt;HR /&gt;&lt;FONT size="2"&gt;Jaux wrote:&lt;BR /&gt;&lt;BR /&gt;It has an embedded 1A switching supply which can take 9 - 20 VAC input in a "power-over-RS-485" configuration.&lt;BR /&gt;&lt;BR /&gt;&lt;/FONT&gt;&lt;HR /&gt;&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;FONT size="2"&gt;I would be interested to find out a little more about the details of&amp;nbsp;your "power over RS485" concept.&amp;nbsp; Thanks in advance.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Regards,&lt;BR /&gt;Mac&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;BR /&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jan 2007 00:57:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/bigger-eval-board-than-DEMO9S08QG8/m-p/142564#M6286</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2007-01-16T00:57:57Z</dc:date>
    </item>
    <item>
      <title>Re: bigger eval board than DEMO9S08QG8?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/bigger-eval-board-than-DEMO9S08QG8/m-p/142565#M6287</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Mac,&lt;BR /&gt;&lt;BR /&gt;OK - basically what I am doing is using a 4-core screened cable for the multi-drop.&lt;BR /&gt;&lt;BR /&gt;2 + screen is used in RS-485 communication and two wires cary the AC which get regulated, smoothed and switch-regulated to 5 or 3.3V. I have used the 12V lighting transformers with success.&lt;BR /&gt;&lt;BR /&gt;If you need more detail - let me know and I will do a little app-note style technical document.&lt;BR /&gt;&lt;BR /&gt;BR, John&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jan 2007 02:29:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/bigger-eval-board-than-DEMO9S08QG8/m-p/142565#M6287</guid>
      <dc:creator>Jaux</dc:creator>
      <dc:date>2007-01-16T02:29:52Z</dc:date>
    </item>
    <item>
      <title>Re: bigger eval board than DEMO9S08QG8?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/bigger-eval-board-than-DEMO9S08QG8/m-p/142566#M6288</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello John,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;For&amp;nbsp; a moment, I thought you might have been distributing power over the same pair as the communications, or&amp;nbsp;using some sort of common mode arrangement&amp;nbsp;- but realize this is probably not possible for RS485.&amp;nbsp; I have previously used spare pairs on Cat. 5 cable for the purpose of distributing low current DC power, in some cases from a standby battery and battery charger combination.&amp;nbsp; I presume your use of a switching regulator gives much wider voltage compiance than a linear regulator, and with lower dissipation - be it for somewhat higher cost.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;I am currently updating the design of my RS485 based equipment, and propose to use an&amp;nbsp;isolated RS485 interface to eliminate earth loops for the wiring to the slave equipment, in a multi-drop master/slave system.&amp;nbsp; To supply power to the isolated side of the interface, I seem to have the choice of using an isolated&amp;nbsp;DC-DC converter supplied from the non-isolated side (expensive?), or to remotely supply the DC power from the common master location.&amp;nbsp; For the latter alternative, it would be hard to justify the use of a switching regulator at&amp;nbsp;each slave.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;This was why I was interested in your post.&amp;nbsp; Incidently, I am also thinking of upgrading to the AW32 device (in the 44-pin package) for this project, assuming I can actually get hold of the silicon here (in Australia) - not always possible in more moderate quantities.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;Message Edited by bigmac on &lt;SPAN class="date_text"&gt;2007-01-16&lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;11:02 AM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jan 2007 08:59:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/bigger-eval-board-than-DEMO9S08QG8/m-p/142566#M6288</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2007-01-16T08:59:31Z</dc:date>
    </item>
    <item>
      <title>Re: bigger eval board than DEMO9S08QG8?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/bigger-eval-board-than-DEMO9S08QG8/m-p/142567#M6289</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Mac,&lt;BR /&gt;&lt;BR /&gt;Just round the corner from me ( Cape Town, South Africa) - nice see somebody from down South.&lt;BR /&gt;&lt;BR /&gt;I have tried to contrust an arrangement using the data pairs for conveying the AC, but the problem is that in oder to get any reasonable distance on RS-485 one has to watch the baud-rate and even using 115 kB, the seperation from 50 Hz is tricky, and the isolation transformer is bulky, expensive and does not work very well. So the 4-core screened cable is pretty standard what we use for normal RS-232 comms. Also, the 4-Cs cable is cheaper than CAT-5 cable.&lt;BR /&gt;&lt;BR /&gt;I am using a LM2575T (~ USD1.2 ea )( switching regulator soldered directly to a copper-pour area on the PCB. See attached pic. I agree it is a little expensive, but this arrangement take away all headaches of a typlical noisy industrial deployment. Using this arrangement will eliminate your earth-loop problems.&lt;BR /&gt;&lt;BR /&gt;I love the AW60 and AW32 chip - We have standardized on this for all our 8-bit applications. Try asking Freescale for samples if you need one or two for prototyping, or you can buy small quantities directly from Freescale ( shipping however is expensive )&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/files/community_files/8BITCOMM/4310_dsc00119.jpg" rel="nofollow" target="_self"&gt;dsc00119.jpg&lt;/A&gt;&lt;/P&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by t.dowe on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-09-22&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;12:00 PM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jan 2007 16:51:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/bigger-eval-board-than-DEMO9S08QG8/m-p/142567#M6289</guid>
      <dc:creator>Jaux</dc:creator>
      <dc:date>2007-01-16T16:51:19Z</dc:date>
    </item>
  </channel>
</rss>