<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollersのトピック32.789 kHz crystal with HCS08DZ60</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/32-789-kHz-crystal-with-HCS08DZ60/m-p/142355#M6176</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm working over a project employing a HCS08DZ60. We use a crystal oscillator with 32.789 kHz frequency, and then internally I multiply this frequency by 1024 with FLL. I connected this crystal with two 22p cap over ground, a 10M res in parallel to the crystal, and a 100k from XTAL and one of the crystal pins, with the classic pierce configuration.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In the micro I configured for external crystal oscillator, low power mode, and enabled bus clock output on PTA0 for debugging purposes.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The oscillator starts with no problem, but the uP works bad and continues to reset itself.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;What I see is that the frequency on PTA0 is sometime stuttering, and when it happens, the uP restarts.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;What is really strange is that it does in this way also if I disabled clock monitor feature.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried to change a little the configuration by changing the series resistor to 330k and to 47k, with no change.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried also to disconnect the crystal and connect in place an external generator coupled with an 10n capacitor on pin EXTAL (input of the uP), giving 1Vpp and a frequency of 32.789 kHz, or other frequencies.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;What happens is the same, but also the stability seems to be better if the frequency is around 34 kHz or so, but it could be just a case.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried to increase also the level of the signal, with no difference at all.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I would exclude in this way that it is a matter of noise, unstable oscillator or wrong external components, because I used a very stable R&amp;amp;S generator, and in any case the crystal oscillator alone works good.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried to switch to internal oscillator, in this way all works good.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It seems to be a problem related to the FLL, I could also suppose that something happens when you use a frequency that in some way is near the internal generated frequency.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Any idea to solve this problem?&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Aug 2007 14:44:45 GMT</pubDate>
    <dc:creator>shadoooo</dc:creator>
    <dc:date>2007-08-08T14:44:45Z</dc:date>
    <item>
      <title>32.789 kHz crystal with HCS08DZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/32-789-kHz-crystal-with-HCS08DZ60/m-p/142355#M6176</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm working over a project employing a HCS08DZ60. We use a crystal oscillator with 32.789 kHz frequency, and then internally I multiply this frequency by 1024 with FLL. I connected this crystal with two 22p cap over ground, a 10M res in parallel to the crystal, and a 100k from XTAL and one of the crystal pins, with the classic pierce configuration.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In the micro I configured for external crystal oscillator, low power mode, and enabled bus clock output on PTA0 for debugging purposes.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The oscillator starts with no problem, but the uP works bad and continues to reset itself.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;What I see is that the frequency on PTA0 is sometime stuttering, and when it happens, the uP restarts.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;What is really strange is that it does in this way also if I disabled clock monitor feature.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried to change a little the configuration by changing the series resistor to 330k and to 47k, with no change.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried also to disconnect the crystal and connect in place an external generator coupled with an 10n capacitor on pin EXTAL (input of the uP), giving 1Vpp and a frequency of 32.789 kHz, or other frequencies.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;What happens is the same, but also the stability seems to be better if the frequency is around 34 kHz or so, but it could be just a case.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried to increase also the level of the signal, with no difference at all.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I would exclude in this way that it is a matter of noise, unstable oscillator or wrong external components, because I used a very stable R&amp;amp;S generator, and in any case the crystal oscillator alone works good.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried to switch to internal oscillator, in this way all works good.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It seems to be a problem related to the FLL, I could also suppose that something happens when you use a frequency that in some way is near the internal generated frequency.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Any idea to solve this problem?&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Aug 2007 14:44:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/32-789-kHz-crystal-with-HCS08DZ60/m-p/142355#M6176</guid>
      <dc:creator>shadoooo</dc:creator>
      <dc:date>2007-08-08T14:44:45Z</dc:date>
    </item>
    <item>
      <title>Re: 32.789 kHz crystal with HCS08DZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/32-789-kHz-crystal-with-HCS08DZ60/m-p/142356#M6177</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I'm also interested in making sure this works, as I intend to use an external 32k clock source...&lt;BR /&gt;&lt;BR /&gt;It would be worth posting your initialization code to check the registers are set up for the correct clock mode/division etc.&lt;BR /&gt;&lt;BR /&gt;Also, I don't understand why have you ac coupled your external clock with a capacitor rather than just connecting directly to EXTAL - Wouldn't ac coupling take it below 0v?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Aug 2007 20:53:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/32-789-kHz-crystal-with-HCS08DZ60/m-p/142356#M6177</guid>
      <dc:creator>RichC</dc:creator>
      <dc:date>2007-08-14T20:53:52Z</dc:date>
    </item>
    <item>
      <title>Re: 32.789 kHz crystal with HCS08DZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/32-789-kHz-crystal-with-HCS08DZ60/m-p/142357#M6178</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I did the initialization through the bean of processor expert. So the code is generated accordingly by it.&lt;BR /&gt;I used a capacitor as the EXTAL line as well as the XTAL is biased by circa 500mV when used in crystal mode. So using a crystal I see a sinusoidal signal that oscillates between 0V and 1V, so 1Vpp biased at 500mV. This means that connecting the pin to a generator biased with 0V causes a current drain on the pin.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Aug 2007 14:42:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/32-789-kHz-crystal-with-HCS08DZ60/m-p/142357#M6178</guid>
      <dc:creator>shadoooo</dc:creator>
      <dc:date>2007-08-27T14:42:00Z</dc:date>
    </item>
    <item>
      <title>Re: 32.789 kHz crystal with HCS08DZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/32-789-kHz-crystal-with-HCS08DZ60/m-p/142358#M6179</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I forgot to mention that I found an ERRATA on "mask set errata for mask 3M05C", particularly "MCGV1 Can Cause a Very Short Clock Pulse" paragraph, SE128C-MCGV1.&lt;BR /&gt;It seems to me that the problem descripted is the same I experience this days.&lt;BR /&gt;However I would to be really sure that this is the same problem I have, because I'm using the mask 2M05C (older ?!) and not the 3M05C, and of course that it will be solved in the final mask.&lt;BR /&gt;I&lt;B&gt;f the problem has been already solved, I would know in which mask the fix was introduced, in way to request from Freescale a sample of the corrected chip&lt;/B&gt;, to be sure that I have no other problem to solve for the final production.&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Aug 2007 15:54:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/32-789-kHz-crystal-with-HCS08DZ60/m-p/142358#M6179</guid>
      <dc:creator>shadoooo</dc:creator>
      <dc:date>2007-08-27T15:54:51Z</dc:date>
    </item>
  </channel>
</rss>