<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Active Interruption of timer channel 0  in Code Warrior in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Active-Interruption-of-timer-channel-0-in-Code-Warrior/m-p/142051#M6119</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;As in all messages, you need to tell which device you are targetting.&lt;BR /&gt;And, for CodeWarrior questions, they should naturally be asked in the proper CodeWarrior board and specify which CodeWarrior version is used.&lt;BR /&gt;&lt;BR /&gt;There is no universal answer to your question.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Alban.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Aug 2007 16:50:38 GMT</pubDate>
    <dc:creator>Alban</dc:creator>
    <dc:date>2007-08-03T16:50:38Z</dc:date>
    <item>
      <title>Active Interruption of timer channel 0  in Code Warrior</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Active-Interruption-of-timer-channel-0-in-Code-Warrior/m-p/142050#M6118</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I need active an interruption in Code Warrior for the Timer in the channel 0 when it finish the counting...i need to reset the program execution...&lt;/DIV&gt;&lt;DIV&gt;thanks...&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Aug 2007 06:45:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Active-Interruption-of-timer-channel-0-in-Code-Warrior/m-p/142050#M6118</guid>
      <dc:creator>Johanny</dc:creator>
      <dc:date>2007-08-03T06:45:15Z</dc:date>
    </item>
    <item>
      <title>Re: Active Interruption of timer channel 0  in Code Warrior</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Active-Interruption-of-timer-channel-0-in-Code-Warrior/m-p/142051#M6119</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;As in all messages, you need to tell which device you are targetting.&lt;BR /&gt;And, for CodeWarrior questions, they should naturally be asked in the proper CodeWarrior board and specify which CodeWarrior version is used.&lt;BR /&gt;&lt;BR /&gt;There is no universal answer to your question.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Alban.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Aug 2007 16:50:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Active-Interruption-of-timer-channel-0-in-Code-Warrior/m-p/142051#M6119</guid>
      <dc:creator>Alban</dc:creator>
      <dc:date>2007-08-03T16:50:38Z</dc:date>
    </item>
  </channel>
</rss>