<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: MC68HC908AP32 with 60K flash?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC68HC908AP32-with-60K-flash/m-p/142028#M6113</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello Polo,&lt;BR /&gt;&lt;BR /&gt;This does happen and is not a mistake.&lt;BR /&gt;Creating a brand new masks costs a lot of money and some masks are used for several devices.&lt;BR /&gt;&lt;BR /&gt;The extra memory and features that you may have will not have been tested.&lt;BR /&gt;So, it may work as it may not work.&lt;BR /&gt;&lt;BR /&gt;Cheers,&lt;BR /&gt;Alban.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Aug 2007 23:25:51 GMT</pubDate>
    <dc:creator>Alban</dc:creator>
    <dc:date>2007-08-02T23:25:51Z</dc:date>
    <item>
      <title>MC68HC908AP32 with 60K flash?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC68HC908AP32-with-60K-flash/m-p/142026#M6111</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;Hi, first sorry for my english &lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-sad.gif"&gt;&lt;IMG alt=":smileysad:" class="emoticon emoticon-smileysad" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-sad.gif" title="Smiley Sad" /&gt;&lt;/A&gt;, I soldered a MC68HC908AP32 QFP44 by mistake instead of a HC908AP64. When I tried to save a 55K program&amp;nbsp;... it worked! &lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-surprised.gif"&gt;&lt;IMG alt=":smileysurprised:" class="emoticon emoticon-smileysurprised" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-surprised.gif" title="Smiley Surprised" /&gt;&lt;/A&gt; . I double check flash an it was all there, no errors at all&amp;nbsp;&lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif"&gt;&lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/A&gt; And the program running at 7.32MHz works ok.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;So my question is how reliable can be flash above 32K in a HC908AP32? Or is this a Freescale mistake?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;PD: I tested an old AP32 QFP44 purchased almost 2 years ago same mask and it also has 60K flash! Is this normal? &lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-indifferent.gif"&gt;&lt;IMG alt=":smileyindifferent:" class="emoticon emoticon-smileyindifferent" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-indifferent.gif" title="Smiley Indifferent" /&gt;&lt;/A&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks a lot&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Aug 2007 22:38:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC68HC908AP32-with-60K-flash/m-p/142026#M6111</guid>
      <dc:creator>polosoft</dc:creator>
      <dc:date>2007-08-02T22:38:50Z</dc:date>
    </item>
    <item>
      <title>Re: MC68HC908AP32 with 60K flash?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC68HC908AP32-with-60K-flash/m-p/142027#M6112</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Check this similar thread:&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://forums.freescale.com/freescale/board/message?board.id=8BITCOMM&amp;amp;thread.id=1756" target="test_blank"&gt;http://forums.freescale.com/freescale/board/message?board.id=8BITCOMM&amp;amp;thread.id=1756&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Aug 2007 22:57:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC68HC908AP32-with-60K-flash/m-p/142027#M6112</guid>
      <dc:creator>tonyp</dc:creator>
      <dc:date>2007-08-02T22:57:30Z</dc:date>
    </item>
    <item>
      <title>Re: MC68HC908AP32 with 60K flash?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC68HC908AP32-with-60K-flash/m-p/142028#M6113</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello Polo,&lt;BR /&gt;&lt;BR /&gt;This does happen and is not a mistake.&lt;BR /&gt;Creating a brand new masks costs a lot of money and some masks are used for several devices.&lt;BR /&gt;&lt;BR /&gt;The extra memory and features that you may have will not have been tested.&lt;BR /&gt;So, it may work as it may not work.&lt;BR /&gt;&lt;BR /&gt;Cheers,&lt;BR /&gt;Alban.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Aug 2007 23:25:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC68HC908AP32-with-60K-flash/m-p/142028#M6113</guid>
      <dc:creator>Alban</dc:creator>
      <dc:date>2007-08-02T23:25:51Z</dc:date>
    </item>
  </channel>
</rss>