<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: 9.8304MHz Crystal For HC908AP Run Mode</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141941#M6089</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;On second thought a 4.9152MHz crystal would be better so I can handle loss of power and only have to power the MCU from the battery. I will change the divider (set by PTB0) in monitor mode so the 9600 baud rate can be used.&lt;BR /&gt;&lt;BR /&gt;A user earlier posted:&lt;BR /&gt;&amp;gt;&amp;gt;Actually, you shouldn't use a 9.8304MHz crystal at all. The HC908APxxA only supports &amp;gt;&amp;gt;crystals in the range of 1MHz to 8MHz.&lt;BR /&gt;&lt;BR /&gt;According to the 5V Oscillator Characteristics table in the data sheet 100KHz is the maximum Fxtalclk. The monitor mode schematic shows a 4.9152MHz crystal being used. Am I misunderstanding something about the data sheet table? Also why would the lower limit be 1MHz if the PLL circuitry typically uses 32KHz?&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 Jan 2007 23:28:25 GMT</pubDate>
    <dc:creator>Byar</dc:creator>
    <dc:date>2007-01-05T23:28:25Z</dc:date>
    <item>
      <title>9.8304MHz Crystal For HC908AP Run Mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141937#M6085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Is it possible to use the same 9.8304MHz crystal for both the flash programming in monitor mode and normal run mode? I would like to avoid having to have a 9.8304MHz crystal for programming and a 32KHz crystal for run mode.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for any help.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Lucas&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jan 2007 07:58:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141937#M6085</guid>
      <dc:creator>Byar</dc:creator>
      <dc:date>2007-01-05T07:58:32Z</dc:date>
    </item>
    <item>
      <title>Re: 9.8304MHz Crystal For HC908AP Run Mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141938#M6086</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi, Lucas:&lt;BR /&gt;&lt;BR /&gt;Actually, you shouldn't use a 9.8304MHz crystal at all. The HC908APxxA only supports crystals in the range of 1MHz to 8MHz. It supports oscillators from DC to 32MHz, however.&lt;BR /&gt;&lt;BR /&gt;If you use a 9.8304MHz oscillator for monitor mode, you could certainly use it also for your normal operating mode. The Phase-Lock-Loop in the Clock-Generator-Module should allow you to program the bus-clock to almost anything you might need, all from the 9.8304MHz oscillator.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jan 2007 09:32:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141938#M6086</guid>
      <dc:creator>rocco</dc:creator>
      <dc:date>2007-01-05T09:32:26Z</dc:date>
    </item>
    <item>
      <title>Re: 9.8304MHz Crystal For HC908AP Run Mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141939#M6087</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;A 9.8304MHz oscillator will work as well.&lt;BR /&gt;&lt;BR /&gt;I think I have a handle on this now. If I use a 9.8304MHz oscillator I can get the 9600 baud programming setup correctly. When I go into run mode I will leave the BCS (base clock selector) bit low which will make CGMOUT = 9.8304/2. The SIM module will then divide CGMOUT by 2 to get a bus clock of 9.8304/4.&lt;BR /&gt;&lt;BR /&gt;This avoids having to use the PLL.&lt;BR /&gt;&lt;BR /&gt;If you see anything wrong with what I said please chime in and correct me.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jan 2007 23:08:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141939#M6087</guid>
      <dc:creator>Byar</dc:creator>
      <dc:date>2007-01-05T23:08:09Z</dc:date>
    </item>
    <item>
      <title>Re: 9.8304MHz Crystal For HC908AP Run Mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141940#M6088</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;You are both right:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;A 9.8304MHz fundamental crystal will probably "&lt;STRONG&gt;work as well&lt;/STRONG&gt;", but "&lt;STRONG&gt;you shouldn't use&lt;/STRONG&gt;" it !&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The datasheet restricts the guarantee of functionality up to 8MHz fundamental crystals.&lt;/DIV&gt;&lt;DIV&gt;If you are using a higher frequency, it is at your own risks.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Cheers,&lt;/DIV&gt;&lt;DIV&gt;Alban.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jan 2007 23:19:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141940#M6088</guid>
      <dc:creator>Alban</dc:creator>
      <dc:date>2007-01-05T23:19:30Z</dc:date>
    </item>
    <item>
      <title>Re: 9.8304MHz Crystal For HC908AP Run Mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141941#M6089</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;On second thought a 4.9152MHz crystal would be better so I can handle loss of power and only have to power the MCU from the battery. I will change the divider (set by PTB0) in monitor mode so the 9600 baud rate can be used.&lt;BR /&gt;&lt;BR /&gt;A user earlier posted:&lt;BR /&gt;&amp;gt;&amp;gt;Actually, you shouldn't use a 9.8304MHz crystal at all. The HC908APxxA only supports &amp;gt;&amp;gt;crystals in the range of 1MHz to 8MHz.&lt;BR /&gt;&lt;BR /&gt;According to the 5V Oscillator Characteristics table in the data sheet 100KHz is the maximum Fxtalclk. The monitor mode schematic shows a 4.9152MHz crystal being used. Am I misunderstanding something about the data sheet table? Also why would the lower limit be 1MHz if the PLL circuitry typically uses 32KHz?&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jan 2007 23:28:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141941#M6089</guid>
      <dc:creator>Byar</dc:creator>
      <dc:date>2007-01-05T23:28:25Z</dc:date>
    </item>
    <item>
      <title>Re: 9.8304MHz Crystal For HC908AP Run Mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141942#M6090</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;Alban wrote:&lt;BR /&gt;&lt;DIV&gt;Hello,&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;You are both right:&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;A 9.8304MHz fundamental crystal will probably "&lt;STRONG&gt;work as well&lt;/STRONG&gt;", but "&lt;STRONG&gt;you shouldn't use&lt;/STRONG&gt;" it !&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;The datasheet restricts the guarantee of functionality up to 8MHz fundamental crystals.&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;If you are using a higher frequency, it is at your own risks.&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;Cheers,&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;Alban.&lt;/DIV&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Can you point out where in the datasheet it gives the fundamental crystal limits?&lt;BR /&gt;&lt;BR /&gt;Thanks&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Jan 2007 00:20:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141942#M6090</guid>
      <dc:creator>Byar</dc:creator>
      <dc:date>2007-01-06T00:20:45Z</dc:date>
    </item>
    <item>
      <title>Re: 4.9152MHz Crystal For HC908AP Run Mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141943#M6091</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello Byar,&lt;BR /&gt;&lt;BR /&gt;OK I see where the confusion is coming from.&lt;BR /&gt;&lt;BR /&gt;You, Byar, are talking about the AP64.&lt;BR /&gt;Me, was reading after rocco who was talking about the AP64A.&lt;BR /&gt;&lt;BR /&gt;The A derivative is the high speed crystal version of the AP64.&lt;BR /&gt;As you were talking about a high speed crystal we thought you just cropped the A...&lt;BR /&gt;&lt;BR /&gt;About where values are:&lt;BR /&gt;- MC68HC908AP64.pdf Rev3 of 8/2005 Table 22-6 page 301 line 3&lt;BR /&gt;- MC68HC908AP64A.pdf Rev1 of 3/2005 Table 22-6 page 297 line 3 &lt;BR /&gt;&lt;BR /&gt;Now to use your 4.9152MHz crystal, you need a AP64A version. Otherwise just use a 32kHz crystal on the AP64.&lt;BR /&gt;&lt;BR /&gt;In term of programming, you don't need an absolute reliability (as opposed to on the field). So even with the AP64, you could use a 4MHz crystal for the programming. &lt;BR /&gt;The oscillator internal circuitry gain is different to accommodate the different crystal speeds.&lt;BR /&gt;&lt;BR /&gt;Alban.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Jan 2007 05:47:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141943#M6091</guid>
      <dc:creator>Alban</dc:creator>
      <dc:date>2007-01-06T05:47:36Z</dc:date>
    </item>
    <item>
      <title>Re: 9.8304MHz Crystal For HC908AP Run Mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141944#M6092</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi Byar,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Its all spelled out in the Electrical Specs:&lt;/DIV&gt;&lt;DIV&gt;Table 22-6, Section 22-7 5V Oscillator haracteristics in MC68HC908APA Rev1 3/2005&lt;/DIV&gt;&lt;DIV&gt;Fxtalclk 1MHz to 8MHz.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards&lt;/DIV&gt;&lt;DIV&gt;Peg&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Jan 2007 05:48:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141944#M6092</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2007-01-06T05:48:55Z</dc:date>
    </item>
    <item>
      <title>Re: 9.8304MHz Crystal For HC908AP Run Mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141945#M6093</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi Byar,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Well we were all well and truly confused!&lt;/DIV&gt;&lt;DIV&gt;The CGM is very different between A and non-A versions.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The non-A is meant to use a low frequency xtal (32.768kHz typ.)&lt;/DIV&gt;&lt;DIV&gt;For monitor mode this only works as a clock source when the device is blank. So you usually need to push a high freq. clock in with an oscillator to re-programme it. (or erase it from the inside)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The A version is meant to use a 1 to 8 MHz xtal and so can be arranged to use the same clock to run it and non-blank re-programme it.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The schematic for monitor mode in the non-A manual is wrong it should say 32k next to the xtal circuit.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards&lt;/DIV&gt;&lt;DIV&gt;Peg&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Jan 2007 06:10:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141945#M6093</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2007-01-06T06:10:17Z</dc:date>
    </item>
    <item>
      <title>Re: 9.8304MHz Crystal For HC908AP Run Mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141946#M6094</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Peg,&lt;BR /&gt;&lt;BR /&gt;I don't think the schematics is wrong for AP64.&lt;BR /&gt;32kHz gives a too low baud rate for the communication to be reliable/possible.&lt;BR /&gt;That's why it is also showing a 4MHz XTAL.&lt;BR /&gt;&lt;BR /&gt;Cheers,&lt;BR /&gt;Alban.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Jan 2007 06:21:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141946#M6094</guid>
      <dc:creator>Alban</dc:creator>
      <dc:date>2007-01-06T06:21:36Z</dc:date>
    </item>
    <item>
      <title>Re: 9.8304MHz Crystal For HC908AP Run Mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141947#M6095</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi Alban,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I don't know this device but if we modify the schematic as I suggest it makes it very similar if not the same as the GP32 (which I do know).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If the schematic is correct then the monitor entry table and the notes thereunder are wrong! (two pages on in the manual).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards&lt;/DIV&gt;&lt;DIV&gt;Peg&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Jan 2007 06:47:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141947#M6095</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2007-01-06T06:47:08Z</dc:date>
    </item>
    <item>
      <title>Re: 9.8304MHz Crystal For HC908AP Run Mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141948#M6096</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I'm afraid I don't follow you Peg.&lt;BR /&gt;&lt;BR /&gt;The schematics shows the switch on /IRQ between Vtst or Vdd, which matches the note 1 and 2 to enter MON08. It also matches Table 8-1 description.&lt;BR /&gt;&lt;BR /&gt;It describes it is only possible to use a 32kHz crystal to program from an erased part by putting /IRQ to an unusual Vdd (which is not available in the schematics). But in this case, the baud rate is generated via the PLL and not via usual Bus Speed = Crystal / x (x= 2 or 4, depending on MCU and its potential config via PTC3).&lt;BR /&gt;&lt;BR /&gt;Can you please detail what I miss ? It's starting to be late here in the UK, could be why &lt;IMG alt=":smileytongue:" class="emoticon emoticon-smileytongue" id="smileytongue" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-tongue.gif" title="Smiley Tongue" /&gt;&lt;BR /&gt;&lt;BR /&gt;Cheers,&lt;BR /&gt;Alban.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Jan 2007 07:06:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141948#M6096</guid>
      <dc:creator>Alban</dc:creator>
      <dc:date>2007-01-06T07:06:05Z</dc:date>
    </item>
    <item>
      <title>Re: 9.8304MHz Crystal For HC908AP Run Mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141949#M6097</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Hi Alban,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;&lt;/DIV&gt;&lt;BLOCKQUOTE&gt;&lt;DIV&gt;&lt;HR /&gt;Alban wrote:&lt;BR /&gt;I'm afraid I don't follow you Peg.&lt;BR /&gt;&lt;BR /&gt;The schematics shows the switch on /IRQ between Vtst or Vdd, which matches the note 1 and 2 to enter MON08. It also matches Table 8-1 description.&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;DIV&gt;Yes I agree, no problem here.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;BR /&gt;&lt;BLOCKQUOTE&gt;&lt;DIV&gt;&lt;HR /&gt;It describes it is only possible to use a 32kHz crystal to program from an erased part by putting /IRQ to an unusual Vdd (which is not available in the schematics).&lt;HR /&gt;&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;BR /&gt;&lt;DIV&gt;I think you mean GND here. This is the same as for GP32! They show a 3 pos. switch in the GP manual.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I think the key things here are:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;1. Note. 2 under Table 8.1. There is only two possible clock sources for monitor entry, 32k XTAL&amp;nbsp;or high frequency OSCILLATOR.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;2. The last paragraph on page 117 also re-asserts that an OSCILLATOR is required on blank entry with IRQ at Vdd. (Also that it should be 9.8MHz for 9600 baud as well!)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;3. The Oscillator is designed for a low frequency xtal and I doubt it would work properly 49 times over its spec. plus I doubt they would design this in just for 1 possible entry method.&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Also if I am correct the schematic should probably also show a series resistor on the 32k xtal as well.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards&lt;/DIV&gt;&lt;DIV&gt;Peg&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;Message Edited by peg on &lt;SPAN class="date_text"&gt;2007-01-06&lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;10:19 AM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Jan 2007 08:01:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141949#M6097</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2007-01-06T08:01:51Z</dc:date>
    </item>
    <item>
      <title>Re: 9.8304MHz Crystal For HC908AP Run Mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141950#M6098</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BLOCKQUOTE dir="ltr" style="MARGIN-RIGHT: 0px"&gt;&lt;P style="MARGIN-RIGHT: 0px"&gt;&lt;/P&gt;&lt;HR /&gt;&lt;P&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;BLOCKQUOTE&gt;&lt;BLOCKQUOTE dir="ltr"&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;BLOCKQUOTE dir="ltr" style="MARGIN-RIGHT: 0px"&gt;&lt;P&gt;&amp;nbsp;It describes it is only possible to use a 32kHz crystal to program from an erased part by putting /IRQ to an unusual Vdd (which is not available in the schematics).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;HR /&gt;&lt;P&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;DIV&gt;&lt;BR /&gt;&lt;/DIV&gt;&lt;DIV&gt;I think you mean GND here. This is the same as for GP32! They show a 3 pos. switch in the GP manual. &lt;HR /&gt;&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;DIV&gt;Hi, I do agree with you.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The series resistor would be to damp the oscillator signal. It's up to the user to determine the best values based on the Negative Resistance value measured.&lt;/DIV&gt;&lt;DIV&gt;HC08s have a very good Safety Factor on oscillators and a resistor will be welcomed to limit EMI.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Cheers,&lt;/DIV&gt;&lt;DIV&gt;Alban.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jan 2007 23:08:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9-8304MHz-Crystal-For-HC908AP-Run-Mode/m-p/141950#M6098</guid>
      <dc:creator>Alban</dc:creator>
      <dc:date>2007-01-09T23:08:45Z</dc:date>
    </item>
  </channel>
</rss>