<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: WARNING - Device is secure. Flash is not accessible in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/WARNING-Device-is-secure-Flash-is-not-accessible/m-p/141802#M6038</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi susy,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Sometimes it says it is secure because it can't talk for some other reason (broken?)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;But if it really is just secured, then use load on the PEDebug menu select your code and burn it in.&lt;/DIV&gt;&lt;DIV&gt;It will do a mass erase first which will get rid of the security.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Perhaps it is secured as additional protection for a bootloader programmed into it???&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Hope this helps&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards&lt;/DIV&gt;&lt;DIV&gt;Peg&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Jan 2007 13:59:47 GMT</pubDate>
    <dc:creator>peg</dc:creator>
    <dc:date>2007-01-03T13:59:47Z</dc:date>
    <item>
      <title>WARNING - Device is secure. Flash is not accessible</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/WARNING-Device-is-secure-Flash-is-not-accessible/m-p/141801#M6037</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello! I recently bought Panasonic's PAN802154HAR00 Zigbee nodes. They are based on the GT60 Uc (practically identic to the SARD BOARD design). Yesterday I was trying to program them on my friend's computer and I connected the P&amp;amp;E Multilink Cable (USB) to the appropiate Jumper, and got this message on the Hiwave Console: Loading Target ... Windows NT detected. USB HCS08/HCS12 MULTILINK detected - Flash Version 5.49 Frequency change to ~3922304hz. WARNING - Device is secure. Flash is not accessible. Device is 9S08GT60. Mode is In-Circuit Debug. IO registers loaded for MC9S08GT60 from C:\Program Files\Metrowerks\CW08 V3.1\prog\REG\MCU1006.REG Startup command file does not exist. Target Ready IO registers loaded for MC9S08GT60 from C:\Program Files\Metrowerks\CW08 V3.1\prog\REG\MCU1006.REG RESET in&amp;gt; ======================================================== And when I tried programming it, the burner console could not access flash, and could not program the module, because of some "error 11" and did not said what an "error 11" was. I attach the message that normally appears when I connect the SARD: Loading Target ... Windows NT detected. USB HCS08/HCS12 MULTILINK detected - Flash Version 5.49 Frequency change to ~3918336hz. Device is 9S08GT60. Mode is In-Circuit Debug. IO registers loaded for MC9S08GT60 from C:\Program Files\Metrowerks\CW08 V3.1\prog\REG\MCU1006.REG Startup command file does not exist. Target Ready IO registers loaded for MC9S08GT60 from C:\Program Files\Metrowerks\CW08 V3.1\prog\REG\MCU1006.REG RESET in&amp;gt; ================== What can I do to program my Panasonic nodes? &lt;/SPAN&gt;&lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-sad.gif"&gt;&lt;IMG alt=":smileysad:" class="emoticon emoticon-smileysad" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-sad.gif" title="Smiley Sad" /&gt;&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jan 2007 05:38:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/WARNING-Device-is-secure-Flash-is-not-accessible/m-p/141801#M6037</guid>
      <dc:creator>susy_the_crowla</dc:creator>
      <dc:date>2007-01-03T05:38:54Z</dc:date>
    </item>
    <item>
      <title>Re: WARNING - Device is secure. Flash is not accessible</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/WARNING-Device-is-secure-Flash-is-not-accessible/m-p/141802#M6038</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi susy,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Sometimes it says it is secure because it can't talk for some other reason (broken?)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;But if it really is just secured, then use load on the PEDebug menu select your code and burn it in.&lt;/DIV&gt;&lt;DIV&gt;It will do a mass erase first which will get rid of the security.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Perhaps it is secured as additional protection for a bootloader programmed into it???&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Hope this helps&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards&lt;/DIV&gt;&lt;DIV&gt;Peg&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jan 2007 13:59:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/WARNING-Device-is-secure-Flash-is-not-accessible/m-p/141802#M6038</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2007-01-03T13:59:47Z</dc:date>
    </item>
    <item>
      <title>Re: WARNING - Device is secure. Flash is not accessible</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/WARNING-Device-is-secure-Flash-is-not-accessible/m-p/141803#M6039</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thanks Peg!&lt;BR /&gt;&lt;BR /&gt;Now I realized that another way of doing it, is opening the program "Test Tools" with the multilink cable connected, and it detects the restriction, and removes it.&lt;BR /&gt;&lt;BR /&gt;&lt;IMG alt=":smileyvery-happy:" class="emoticon emoticon-smileyvery-happy" id="smileyvery-happy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-very-happy.gif" title="Smiley Very Happy" /&gt; Thank God my nodes now work... And thank you for your help!&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jan 2007 23:26:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/WARNING-Device-is-secure-Flash-is-not-accessible/m-p/141803#M6039</guid>
      <dc:creator>susy_the_crowla</dc:creator>
      <dc:date>2007-01-03T23:26:11Z</dc:date>
    </item>
  </channel>
</rss>