<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: smac use with HCS08QG8 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/smac-use-with-HCS08QG8/m-p/141431#M5937</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello!&lt;BR /&gt;&lt;BR /&gt;Well, what you have to do is:&lt;BR /&gt;&lt;BR /&gt;1. Get the QG8 datasheet, and locate the place where the registers and interruption vectors are, and make a copy of the original folder. You will work on the copy (or the original, whatever, just let one unmodified just in case &lt;IMG alt=":smileywink:" class="emoticon emoticon-smileywink" id="smileywink" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-wink.gif" title="Smiley Wink" /&gt; )&lt;BR /&gt;&lt;BR /&gt;2. Open the file in the beekit project in wich interruption vectors are (don't know the name, but patiently you will find it) and replace the vector addresses in that file, with the addresses on the QG8 datasheet.&lt;BR /&gt;&lt;BR /&gt;3. Do the same with Port Registers, Timer Registers, and any other module.&lt;BR /&gt;&lt;BR /&gt;4. In case your QG8 has less ports or pins in a port or modules than the QB60, delete any references made in the main program for those pins or ports or modules.&lt;BR /&gt;&lt;BR /&gt;5. Compile again, debug, and repeat if needed, until your application works. ¡Enjoy!&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Jan 2007 23:33:22 GMT</pubDate>
    <dc:creator>susy_the_crowla</dc:creator>
    <dc:date>2007-01-03T23:33:22Z</dc:date>
    <item>
      <title>smac use with HCS08QG8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/smac-use-with-HCS08QG8/m-p/141430#M5936</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi, I imported a smac application from the beekit wireless toolbox into code warrior.&amp;nbsp; The problem is the smac application is targeted for the MC9S08QB60 and I have the MC9S08QG8.&amp;nbsp; What libraries need to be added to target the board that I have.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 30 Dec 2006 00:02:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/smac-use-with-HCS08QG8/m-p/141430#M5936</guid>
      <dc:creator>jgod1784</dc:creator>
      <dc:date>2006-12-30T00:02:12Z</dc:date>
    </item>
    <item>
      <title>Re: smac use with HCS08QG8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/smac-use-with-HCS08QG8/m-p/141431#M5937</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello!&lt;BR /&gt;&lt;BR /&gt;Well, what you have to do is:&lt;BR /&gt;&lt;BR /&gt;1. Get the QG8 datasheet, and locate the place where the registers and interruption vectors are, and make a copy of the original folder. You will work on the copy (or the original, whatever, just let one unmodified just in case &lt;IMG alt=":smileywink:" class="emoticon emoticon-smileywink" id="smileywink" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-wink.gif" title="Smiley Wink" /&gt; )&lt;BR /&gt;&lt;BR /&gt;2. Open the file in the beekit project in wich interruption vectors are (don't know the name, but patiently you will find it) and replace the vector addresses in that file, with the addresses on the QG8 datasheet.&lt;BR /&gt;&lt;BR /&gt;3. Do the same with Port Registers, Timer Registers, and any other module.&lt;BR /&gt;&lt;BR /&gt;4. In case your QG8 has less ports or pins in a port or modules than the QB60, delete any references made in the main program for those pins or ports or modules.&lt;BR /&gt;&lt;BR /&gt;5. Compile again, debug, and repeat if needed, until your application works. ¡Enjoy!&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jan 2007 23:33:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/smac-use-with-HCS08QG8/m-p/141431#M5937</guid>
      <dc:creator>susy_the_crowla</dc:creator>
      <dc:date>2007-01-03T23:33:22Z</dc:date>
    </item>
    <item>
      <title>Re: smac use with HCS08QG8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/smac-use-with-HCS08QG8/m-p/141432#M5938</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Ok but Im still a little confused. The target&amp;nbsp;MC1319EVB was set in the BeeKit toolbox and I need to target the P&amp;amp;E multilink to download onto the QG8 board. Do I create a new project targeted for the QG8 and copy the files from the drivers and SMAC folders from the imported project to the new project (demostrated in the AN3381.pdf) and then change the register addresses&amp;nbsp;according to the QG8 data sheet&amp;nbsp;?&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jan 2007 23:37:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/smac-use-with-HCS08QG8/m-p/141432#M5938</guid>
      <dc:creator>jgod1784</dc:creator>
      <dc:date>2007-01-04T23:37:58Z</dc:date>
    </item>
  </channel>
</rss>