<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Beginners question QG4/QG8 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Beginners-question-QG4-QG8/m-p/140804#M5761</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi!&lt;BR /&gt;Many thanks to tonyp and Pingu! Meanwhile I was very busy with debugging the hardware and some software bugs in my firmware, that's the reason why I am answering very late.&lt;BR /&gt;I have done some tests and the memory seems to be there really. As Pingu wrote, the QG4 seem to be QG8 with a failure in flash (or maybe ram) area that is only used by the QG8.&lt;BR /&gt;Many thanks again for your replies!&lt;BR /&gt;Have a nice day!&lt;BR /&gt;Best regards&lt;BR /&gt;Ralph&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Jul 2006 20:01:38 GMT</pubDate>
    <dc:creator>Ralph</dc:creator>
    <dc:date>2006-07-06T20:01:38Z</dc:date>
    <item>
      <title>Beginners question QG4/QG8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Beginners-question-QG4-QG8/m-p/140801#M5758</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am new to HCS08QG8 so the question may be dumb. Some years ago I played around already with 68332 and BD32 (DOS-Debugger), now I want to use the mentioned device and Code Warrior 5.0.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have started with the DEMO9S08QG8 and wrote some Code. Since our distributor had the QG4 on stock and the lower memory will be enough for my application I have ordered the QG4. Since I am a little curious I didn't change the device in CW5.0 and awaited an error because the flash of the QG4 starts at $F000 instead of $E000 of the QG8. But there seems to be no problem. To verify that I've written code with two ascii test strings with the org command to $EA00 and another to $F000. Both are there in the memory window! &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Setting the device to QG4 in CW5.0 results for sure in "00" from $E000 to $EFFF.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Has somebody got an idea why this happens? &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Best Regards &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ralph&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;P.S.: "P&amp;amp;E Multilink/Cyclone Pro" is selected as debugger.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Jun 2006 22:32:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Beginners-question-QG4-QG8/m-p/140801#M5758</guid>
      <dc:creator>Ralph</dc:creator>
      <dc:date>2006-06-23T22:32:46Z</dc:date>
    </item>
    <item>
      <title>Re: Beginners question QG4/QG8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Beginners-question-QG4-QG8/m-p/140802#M5759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Have you tried with another chip (preferrably from a different batch)?&amp;nbsp; Does it still happen?&lt;/P&gt;&lt;P&gt;If only some chips do this, one possibility is that during production (of would-be QG8) some Flash fails the tests while the rest (within the QG4 range) passes.&amp;nbsp; Freescale "baptises" the chip&amp;nbsp;QG4, and you end up with a little "bonus" that you probably shouldn't trust (the extra memory, that is) for production but can be used for playing.&amp;nbsp; They used to do that with HC11s.&amp;nbsp; You ordered a ROM-less part to find either Buffalo or some other firmware in the on-chip ROM.&amp;nbsp; &lt;EM&gt;[This actually saved me once in a production unit, when (for reasons too complicated to mention here) the part switched from expanded to single-chip mode and auto-executed the built-in&amp;nbsp;Buffalo.&amp;nbsp; I used Buffalo to set it back to using expanded mode.]&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Then again, it could be a totally unrelated issue having to do with CW's debugging facilities of which I know nothing about as I don't use it (e.g., a "ghost" image&amp;nbsp;that isn't really in the chip, only on the debugger's window).&lt;/P&gt;&lt;P&gt;Message Edited by tonyp on &lt;SPAN class="date_text"&gt;2006-06-23&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;11:24 PM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 24 Jun 2006 03:20:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Beginners-question-QG4-QG8/m-p/140802#M5759</guid>
      <dc:creator>tonyp</dc:creator>
      <dc:date>2006-06-24T03:20:57Z</dc:date>
    </item>
    <item>
      <title>Re: Beginners question QG4/QG8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Beginners-question-QG4-QG8/m-p/140803#M5760</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;The first description from tonyp&amp;nbsp;is the correct one in this case.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Jun 2006 19:43:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Beginners-question-QG4-QG8/m-p/140803#M5760</guid>
      <dc:creator>Pingu</dc:creator>
      <dc:date>2006-06-29T19:43:10Z</dc:date>
    </item>
    <item>
      <title>Re: Beginners question QG4/QG8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Beginners-question-QG4-QG8/m-p/140804#M5761</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi!&lt;BR /&gt;Many thanks to tonyp and Pingu! Meanwhile I was very busy with debugging the hardware and some software bugs in my firmware, that's the reason why I am answering very late.&lt;BR /&gt;I have done some tests and the memory seems to be there really. As Pingu wrote, the QG4 seem to be QG8 with a failure in flash (or maybe ram) area that is only used by the QG8.&lt;BR /&gt;Many thanks again for your replies!&lt;BR /&gt;Have a nice day!&lt;BR /&gt;Best regards&lt;BR /&gt;Ralph&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jul 2006 20:01:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Beginners-question-QG4-QG8/m-p/140804#M5761</guid>
      <dc:creator>Ralph</dc:creator>
      <dc:date>2006-07-06T20:01:38Z</dc:date>
    </item>
  </channel>
</rss>