<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: QG8 PTB0 looks like PTA4 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/QG8-PTB0-looks-like-PTA4/m-p/140487#M5638</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;What you said was true and I needed to do that, but I could not configure PTB0 as an output.&amp;nbsp;&amp;nbsp; I was able to toggle all of the other pins (exept the for the Debug pins and not PTB0). &amp;nbsp; But then I looked at the Bean output "void PE_low_level_init(void)", and it was not setting PTBDD bit 0 as an output.&amp;nbsp; I changed&amp;nbsp; that and it works!&lt;BR /&gt;&lt;BR /&gt;Thanks for your help&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Jul 2007 01:34:32 GMT</pubDate>
    <dc:creator>blinari</dc:creator>
    <dc:date>2007-07-24T01:34:32Z</dc:date>
    <item>
      <title>QG8 PTB0 looks like PTA4</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/QG8-PTB0-looks-like-PTA4/m-p/140484#M5635</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;P&gt;I am running the DEMO9S08QG8 board&amp;nbsp; I set all my inputs and output the way that I want them using the Processor Expert as a KBI.&amp;nbsp; I set PTB0 to an input (KBI) that is driven by 100 ohm output resistant source and PTB0 looks like PTA4 (the debug data) with a some of the real signal?&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt; If I get rid of the input it look almost the same as PTA4.&amp;nbsp; It looks high impedance between PTA4 and PTB0 like 2Mohm&amp;nbsp; and all the corners are rounded.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do I get PTB0 to not follow PTA4 so I can use PTB0.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jul 2007 02:27:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/QG8-PTB0-looks-like-PTA4/m-p/140484#M5635</guid>
      <dc:creator>blinari</dc:creator>
      <dc:date>2007-07-19T02:27:55Z</dc:date>
    </item>
    <item>
      <title>Re: QG8 PTB0 looks like PTA4</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/QG8-PTB0-looks-like-PTA4/m-p/140485#M5636</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi blinari,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I am not sure if I follow you (pun intended) but here goes:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;PTA4 shares with BKGD on a QG8 so you have to be careful about using both uses of this pin.&lt;/DIV&gt;&lt;DIV&gt;On a DEMOQG8 board this pin is hard-wired into the BDM converter section, so using it for anything else is nigh on impossible with board modifications.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;PTB0 shares with RXD. This pin on the DEMOQG8 board is hardwired to the MAX3218 so the same sort of things apply here.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;PTA0, PTA1, PTA2, PTA3, PTB2, PTB3, PTB4, PTB5, PTB6 and PTB7 are really the only ones freely available for other uses on this demo board. (If you remove the USER EN jumpers.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;PTB0, PTB1 are used for comms and PTA4, PTA5 are used for BDM.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Hope this helps.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Jul 2007 08:16:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/QG8-PTB0-looks-like-PTA4/m-p/140485#M5636</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2007-07-21T08:16:19Z</dc:date>
    </item>
    <item>
      <title>Re: QG8 PTB0 looks like PTA4</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/QG8-PTB0-looks-like-PTA4/m-p/140486#M5637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello blinari,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I read your question again today and I think I mis-interpreted it yesterday.&lt;/DIV&gt;&lt;DIV&gt;I now believe you are saying that PTB0 is tracking the BDM comms on PTA4/BKGD.&lt;/DIV&gt;&lt;DIV&gt;What I said before I still believe is correct but perhaps not so relevant to your problem.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I now think the answer is to remove the jumper between 2 and 3 of COM_EN.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If you want to disable the MAX3218 to free-up PTB0 but still use BKGD you need to place the jumper on COM_EN between 1 and 2.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;COM_EN 2 to 3 connects BKGD to FORCEON/OFF of the MAX3218. So the signal you are seeing on PTB0 is probably the reciever coming in and out of tri-state mode.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 22 Jul 2007 06:10:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/QG8-PTB0-looks-like-PTA4/m-p/140486#M5637</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2007-07-22T06:10:30Z</dc:date>
    </item>
    <item>
      <title>Re: QG8 PTB0 looks like PTA4</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/QG8-PTB0-looks-like-PTA4/m-p/140487#M5638</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;What you said was true and I needed to do that, but I could not configure PTB0 as an output.&amp;nbsp;&amp;nbsp; I was able to toggle all of the other pins (exept the for the Debug pins and not PTB0). &amp;nbsp; But then I looked at the Bean output "void PE_low_level_init(void)", and it was not setting PTBDD bit 0 as an output.&amp;nbsp; I changed&amp;nbsp; that and it works!&lt;BR /&gt;&lt;BR /&gt;Thanks for your help&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jul 2007 01:34:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/QG8-PTB0-looks-like-PTA4/m-p/140487#M5638</guid>
      <dc:creator>blinari</dc:creator>
      <dc:date>2007-07-24T01:34:32Z</dc:date>
    </item>
  </channel>
</rss>