<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Programing &amp;quot;High-end&amp;quot; microcontrolers with USBSPYDER08 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Programing-quot-High-end-quot-microcontrolers-with-USBSPYDER08/m-p/125269#M558</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;yes it can! refer to &amp;nbsp;&lt;A href="http://www.eckhard-gosch.de/en/readarticle.php?article_id=12" rel="nofollow" target="_blank"&gt;http://www.eckhard-gosch.de/en/readarticle.php?article_id=12&lt;/A&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Jul 2007 06:32:16 GMT</pubDate>
    <dc:creator>SBrazz</dc:creator>
    <dc:date>2007-07-20T06:32:16Z</dc:date>
    <item>
      <title>Programing "High-end" microcontrolers with USBSPYDER08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Programing-quot-High-end-quot-microcontrolers-with-USBSPYDER08/m-p/125266#M555</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have bought a USBSPYDER08 kit and I would like to use the BDM interface to program the better microcontrolers (for example AW60 etc.). But in CodeWarrior It's possible to chose QD4, QG4 and QG8 only. So i would like to ask you. It's possible to add another microcotroler or does exist "better" drivers for USBSPYDER08?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank You for Answer&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Mar 2007 00:06:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Programing-quot-High-end-quot-microcontrolers-with-USBSPYDER08/m-p/125266#M555</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2007-03-07T00:06:55Z</dc:date>
    </item>
    <item>
      <title>Re: Programing "High-end" microcontrolers with USBSPYDER08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Programing-quot-High-end-quot-microcontrolers-with-USBSPYDER08/m-p/125267#M556</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi Mica,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I was wondering about this too when I saw it come out.&lt;/DIV&gt;&lt;DIV&gt;I don't have an answer for you but I suspect there is some deliberate "hobbling" going on here in order to protect sales of higher end adapters.&lt;/DIV&gt;&lt;DIV&gt;I would like to know the technical reasons behind this limitation as well. There is very little difference between supporting a QG and a GB or AW.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Mar 2007 15:11:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Programing-quot-High-end-quot-microcontrolers-with-USBSPYDER08/m-p/125267#M556</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2007-03-07T15:11:37Z</dc:date>
    </item>
    <item>
      <title>Re: Programing "High-end" microcontrolers with USBSPYDER08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Programing-quot-High-end-quot-microcontrolers-with-USBSPYDER08/m-p/125268#M557</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi&lt;BR /&gt;that is the fine thing of low cost development systems; when you see your device is to weak for your application you have to switch to a bigger environment. You then not only have to install the software again, your hardware is also obsolete!&lt;BR /&gt;For this reason i prefer a modular design. A long, long time ago i have begun to build up my modular development system. First based on the ECB-Bus (CP/M80, Z80) and later my own "standard". This includes a port connector with the bits always on the same location as well as some power pins for powering the "addons". I am now able to switch between different MPU's by changing the MPU module. That works for the HCS08, HC08 and RS08 family, even the software can be modified thanks to EBS08!&lt;BR /&gt;I am wondering why the whole word is designing EVB's for a single MPU (a lot of repeated work for layouting and testing) with solder pads on it (they are looking ugly after a short time!!), when it could be done much easier.&lt;BR /&gt;&lt;BR /&gt;The first pic is showing a GB32 module with the baseplate and two RS232 converters while testing the software for a milling machine and the second pic is the KAx module with the OSBDM+E and the porttester during EBS08R testing.&lt;BR /&gt;&lt;BR /&gt;Saluti Joerg&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Mar 2007 23:35:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Programing-quot-High-end-quot-microcontrolers-with-USBSPYDER08/m-p/125268#M557</guid>
      <dc:creator>joerg</dc:creator>
      <dc:date>2007-03-07T23:35:16Z</dc:date>
    </item>
    <item>
      <title>Re: Programing "High-end" microcontrolers with USBSPYDER08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Programing-quot-High-end-quot-microcontrolers-with-USBSPYDER08/m-p/125269#M558</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;yes it can! refer to &amp;nbsp;&lt;A href="http://www.eckhard-gosch.de/en/readarticle.php?article_id=12" rel="nofollow" target="_blank"&gt;http://www.eckhard-gosch.de/en/readarticle.php?article_id=12&lt;/A&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jul 2007 06:32:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Programing-quot-High-end-quot-microcontrolers-with-USBSPYDER08/m-p/125269#M558</guid>
      <dc:creator>SBrazz</dc:creator>
      <dc:date>2007-07-20T06:32:16Z</dc:date>
    </item>
  </channel>
</rss>