<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: HC908AP LED driver question</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908AP-LED-driver-question/m-p/139859#M5480</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;&lt;FONT size="2"&gt;Hello Dave,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;The specification you refer to is the port pin sink current (via the N-channel MOSFET).&amp;nbsp; A higher voltage across the LED means a lower voltage at the pin, and therefore less current through the LED.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;The output characteristic of the MOSFET, when conducting, may be represented by a resistance to the negative rail.&amp;nbsp; For 3 volt supply, the calculated resistance value may vary between approximately 130 ohms and 670 ohms (unit-to-unit).&amp;nbsp; A red LED would have a voltage drop in the vicinity of 1.8 volts, so the current through the LED may vary between about 2mA and 9mA, with no external series resistance.&amp;nbsp; If this current is insufficient, or the variation of current is too wide,&amp;nbsp;an external buffer transistor or MOSFET would be necessary (including a resistor in series with the LED).&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;For a 5 volt supply, the internal N-channel variation would be approximately 120 to 330 ohms.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Regards,&lt;BR /&gt;Mac&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Message Edited by bigmac on &lt;SPAN class="date_text"&gt;2006-06-17&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;01:03 AM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Jun 2006 22:00:46 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2006-06-16T22:00:46Z</dc:date>
    <item>
      <title>HC908AP LED driver question</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908AP-LED-driver-question/m-p/139858#M5479</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I'm not understanding the LED driver on port A.&amp;nbsp; Vol = 2V with Vcc = 3V leaves one volt to drive the LED.&amp;nbsp; I don't have any 1 volt LEDs.&amp;nbsp; Is this a pull down pin or a source pin?&amp;nbsp; Anyone using it?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Dave&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Jun 2006 07:48:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908AP-LED-driver-question/m-p/139858#M5479</guid>
      <dc:creator>erokc</dc:creator>
      <dc:date>2006-06-16T07:48:20Z</dc:date>
    </item>
    <item>
      <title>Re: HC908AP LED driver question</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908AP-LED-driver-question/m-p/139859#M5480</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;&lt;FONT size="2"&gt;Hello Dave,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;The specification you refer to is the port pin sink current (via the N-channel MOSFET).&amp;nbsp; A higher voltage across the LED means a lower voltage at the pin, and therefore less current through the LED.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;The output characteristic of the MOSFET, when conducting, may be represented by a resistance to the negative rail.&amp;nbsp; For 3 volt supply, the calculated resistance value may vary between approximately 130 ohms and 670 ohms (unit-to-unit).&amp;nbsp; A red LED would have a voltage drop in the vicinity of 1.8 volts, so the current through the LED may vary between about 2mA and 9mA, with no external series resistance.&amp;nbsp; If this current is insufficient, or the variation of current is too wide,&amp;nbsp;an external buffer transistor or MOSFET would be necessary (including a resistor in series with the LED).&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;For a 5 volt supply, the internal N-channel variation would be approximately 120 to 330 ohms.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Regards,&lt;BR /&gt;Mac&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Message Edited by bigmac on &lt;SPAN class="date_text"&gt;2006-06-17&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;01:03 AM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Jun 2006 22:00:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908AP-LED-driver-question/m-p/139859#M5480</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2006-06-16T22:00:46Z</dc:date>
    </item>
    <item>
      <title>Re: HC908AP LED driver question</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908AP-LED-driver-question/m-p/139860#M5481</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Mac, thanks for the clearification.&amp;nbsp; I could not understand how to apply the driver.&amp;nbsp; Brightness is not an issue for me as this will be used for diagnostics, not normal product indicators.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Dave&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Jun 2006 22:58:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908AP-LED-driver-question/m-p/139860#M5481</guid>
      <dc:creator>erokc</dc:creator>
      <dc:date>2006-06-16T22:58:22Z</dc:date>
    </item>
  </channel>
</rss>