<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: MC1321x RF reference design question</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC1321x-RF-reference-design-question/m-p/139612#M5402</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi, Nevo:&lt;BR /&gt;&lt;BR /&gt;I can't be sure of the original designer's intent, but when I use a zero-ohm resistor, it is either as a jumper, or as a placeholder for a possible future non-zero-ohm resistor.&lt;BR /&gt;&lt;BR /&gt;In this case, it looks like a jumper to select the on-board "F" antenna. To use an external antenna attached to the J100 connector, you would leave R111 out, and include a zero-ohm resistor at R112 (which is shown as "Not Mounted" on the schematic).&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Dec 2006 10:18:01 GMT</pubDate>
    <dc:creator>rocco</dc:creator>
    <dc:date>2006-12-12T10:18:01Z</dc:date>
    <item>
      <title>MC1321x RF reference design question</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC1321x-RF-reference-design-question/m-p/139611#M5401</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&amp;nbsp;all!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I'm reviewing AppNote 3248, "Using the MX1321x Internal Transmit/Receive Switch in a Low-Cost, Single-Port, Two Layer Design."&amp;nbsp; I am not an RF engineer and I'll happily copy a tested design.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I'm curious about a feature of the design. Just before the antenna, the signal is sent through R111, which apparently is a zero ohm resistor.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Now, I'm a digital guy and anything analog is black magic to me. But I've just got to ask: what is the purpose of a zero-ohm resistor?&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Dec 2006 07:56:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC1321x-RF-reference-design-question/m-p/139611#M5401</guid>
      <dc:creator>Nevo</dc:creator>
      <dc:date>2006-12-12T07:56:02Z</dc:date>
    </item>
    <item>
      <title>Re: MC1321x RF reference design question</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC1321x-RF-reference-design-question/m-p/139612#M5402</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi, Nevo:&lt;BR /&gt;&lt;BR /&gt;I can't be sure of the original designer's intent, but when I use a zero-ohm resistor, it is either as a jumper, or as a placeholder for a possible future non-zero-ohm resistor.&lt;BR /&gt;&lt;BR /&gt;In this case, it looks like a jumper to select the on-board "F" antenna. To use an external antenna attached to the J100 connector, you would leave R111 out, and include a zero-ohm resistor at R112 (which is shown as "Not Mounted" on the schematic).&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Dec 2006 10:18:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC1321x-RF-reference-design-question/m-p/139612#M5402</guid>
      <dc:creator>rocco</dc:creator>
      <dc:date>2006-12-12T10:18:01Z</dc:date>
    </item>
    <item>
      <title>Re: MC1321x RF reference design question</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC1321x-RF-reference-design-question/m-p/139613#M5403</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Thanks, Rocco.&amp;nbsp; That makes perfect sense and is pretty much what I'd assumed.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Dec 2006 12:25:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC1321x-RF-reference-design-question/m-p/139613#M5403</guid>
      <dc:creator>Nevo</dc:creator>
      <dc:date>2006-12-12T12:25:55Z</dc:date>
    </item>
  </channel>
</rss>