<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ICG Programming problem in FEI mode for bus frequency in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ICG-Programming-problem-in-FEI-mode-for-bus-frequency/m-p/139545#M5368</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Sorry, I was wrong. I could program ICGC1 and ICGC2 of MCS908GB60 in FEI mode correctly. In fact, I can change the bus frequency "on the fly" and my M69DEMO908GB60 demo board responds accordingly. Thanks.&lt;/P&gt;&lt;P&gt;-priyanto.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Jun 2006 02:59:58 GMT</pubDate>
    <dc:creator>priyanto</dc:creator>
    <dc:date>2006-06-15T02:59:58Z</dc:date>
    <item>
      <title>ICG Programming problem in FEI mode for bus frequency</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ICG-Programming-problem-in-FEI-mode-for-bus-frequency/m-p/139544#M5367</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi All,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;To reduce external component, we are not using external components for system clock generation. So I use FEI mode and followed the&amp;nbsp;example #3&amp;nbsp;on manual p.114 to generate 5.4 MHz bus clock with value of ICGC1 = $28 and ICGC2 = $31. Then I use this bus clock to drive TPM1 timer which I program the bits CLKSB:CLKSA equals to 0:1 (BUSCLK). I want to use TPM1 as base system timer. However, it does not seem the timer is using the value of the programmed bus clock (5.4MHz). FYI, I use the demo board which has 32KHz external crystal, and it seems the timer is still using the external clock. Another interesting point is that if I program using "Device Initialization" wizard on CW for ICGC1 value, it does not take it. Any idea why the programmed ICG values don't take effect? Thanks for any responses.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Rgds,&lt;/DIV&gt;&lt;DIV&gt;-priyanto.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Jun 2006 08:02:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ICG-Programming-problem-in-FEI-mode-for-bus-frequency/m-p/139544#M5367</guid>
      <dc:creator>priyanto</dc:creator>
      <dc:date>2006-06-14T08:02:23Z</dc:date>
    </item>
    <item>
      <title>Re: ICG Programming problem in FEI mode for bus frequency</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ICG-Programming-problem-in-FEI-mode-for-bus-frequency/m-p/139545#M5368</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Sorry, I was wrong. I could program ICGC1 and ICGC2 of MCS908GB60 in FEI mode correctly. In fact, I can change the bus frequency "on the fly" and my M69DEMO908GB60 demo board responds accordingly. Thanks.&lt;/P&gt;&lt;P&gt;-priyanto.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Jun 2006 02:59:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ICG-Programming-problem-in-FEI-mode-for-bus-frequency/m-p/139545#M5368</guid>
      <dc:creator>priyanto</dc:creator>
      <dc:date>2006-06-15T02:59:58Z</dc:date>
    </item>
  </channel>
</rss>