<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Single Board Computer with the HCS08 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Single-Board-Computer-with-the-HCS08/m-p/139508#M5359</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have developed a simple single-board MCU based on the MC9SAW60CFUE&lt;BR /&gt;&lt;BR /&gt;Features:&lt;BR /&gt;&lt;BR /&gt;. Integrated switching supply, 9-20 VAC input&lt;BR /&gt;. AW60 is 5V based&lt;BR /&gt;. 24-key keyboard interface ( 8 KBI x 3 scan, active low )&lt;BR /&gt;. LCD interface&lt;BR /&gt;. RS-485 interface&lt;BR /&gt;. All of the GPIO pins are routed to edge pin connectors&lt;BR /&gt;. BDM Interface&lt;BR /&gt;&lt;BR /&gt;As a fanatic Freescale junkie, and because you have a small company ( we were all small once), I will let you have the schematics, Gerbers, etc. which you will need to construct the board free of charge.&lt;BR /&gt;&lt;BR /&gt;I am in a good mood, and is Xmas anyway - I will even let you have a blank PCB which you can use to construct the MCU.&lt;BR /&gt;&lt;BR /&gt;See pics attached.&lt;BR /&gt;&lt;BR /&gt;Let me know if you want it.&lt;BR /&gt;&lt;BR /&gt;John Ulyate&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/files/community_files/8BITCOMM/3998_1_RIMG0004.jpg" rel="nofollow" target="_self"&gt;RIMG0004.jpg&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/files/community_files/8BITCOMM/3998_2_RIMG0005.jpg" rel="nofollow" target="_self"&gt;RIMG0005.jpg&lt;/A&gt;&lt;/P&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by t.dowe on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-10-20&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;01:37 PM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Dec 2006 01:06:25 GMT</pubDate>
    <dc:creator>Jaux</dc:creator>
    <dc:date>2006-12-15T01:06:25Z</dc:date>
    <item>
      <title>Single Board Computer with the HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Single-Board-Computer-with-the-HCS08/m-p/139506#M5357</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I am need of a single board computer with an HCS08 MCU that is ready to be used in the end application.&amp;nbsp; Are there any companies that produce them?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Dec 2006 06:13:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Single-Board-Computer-with-the-HCS08/m-p/139506#M5357</guid>
      <dc:creator>FC</dc:creator>
      <dc:date>2006-12-11T06:13:45Z</dc:date>
    </item>
    <item>
      <title>Re: Single Board Computer with the HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Single-Board-Computer-with-the-HCS08/m-p/139507#M5358</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello FC.&lt;BR /&gt;I have a small company that produces a board based on the MC9S08GB60 (HCS08). It can be had either "bare-bones" or pre-configured with some buffered I/O. It also has an RS-232 port and on-board regulator, etc.&lt;BR /&gt;Go to &lt;A href="http://gadgetwerksinc.com" target="test_blank"&gt;http://gadgetwerksinc.com&lt;/A&gt; for a picture and details. Freescale forum members get an un-official 20% discount off the list price.&lt;BR /&gt;ron&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Dec 2006 14:22:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Single-Board-Computer-with-the-HCS08/m-p/139507#M5358</guid>
      <dc:creator>glork</dc:creator>
      <dc:date>2006-12-11T14:22:31Z</dc:date>
    </item>
    <item>
      <title>Re: Single Board Computer with the HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Single-Board-Computer-with-the-HCS08/m-p/139508#M5359</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have developed a simple single-board MCU based on the MC9SAW60CFUE&lt;BR /&gt;&lt;BR /&gt;Features:&lt;BR /&gt;&lt;BR /&gt;. Integrated switching supply, 9-20 VAC input&lt;BR /&gt;. AW60 is 5V based&lt;BR /&gt;. 24-key keyboard interface ( 8 KBI x 3 scan, active low )&lt;BR /&gt;. LCD interface&lt;BR /&gt;. RS-485 interface&lt;BR /&gt;. All of the GPIO pins are routed to edge pin connectors&lt;BR /&gt;. BDM Interface&lt;BR /&gt;&lt;BR /&gt;As a fanatic Freescale junkie, and because you have a small company ( we were all small once), I will let you have the schematics, Gerbers, etc. which you will need to construct the board free of charge.&lt;BR /&gt;&lt;BR /&gt;I am in a good mood, and is Xmas anyway - I will even let you have a blank PCB which you can use to construct the MCU.&lt;BR /&gt;&lt;BR /&gt;See pics attached.&lt;BR /&gt;&lt;BR /&gt;Let me know if you want it.&lt;BR /&gt;&lt;BR /&gt;John Ulyate&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/files/community_files/8BITCOMM/3998_1_RIMG0004.jpg" rel="nofollow" target="_self"&gt;RIMG0004.jpg&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/files/community_files/8BITCOMM/3998_2_RIMG0005.jpg" rel="nofollow" target="_self"&gt;RIMG0005.jpg&lt;/A&gt;&lt;/P&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by t.dowe on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-10-20&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;01:37 PM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Dec 2006 01:06:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Single-Board-Computer-with-the-HCS08/m-p/139508#M5359</guid>
      <dc:creator>Jaux</dc:creator>
      <dc:date>2006-12-15T01:06:25Z</dc:date>
    </item>
  </channel>
</rss>