<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: USB Multilink in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125204#M534</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;peg wrote:&lt;BR /&gt;&lt;P&gt;Hello Cmux,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Are you using a P&amp;amp;E Multilink (USB-ML-12)?&lt;/P&gt;&lt;P&gt;Are you using Codewarrior on the PC?&lt;/P&gt;&lt;P&gt;Does the yellow LED light when Multilink is plugged in to PC on its own?&lt;/P&gt;&lt;P&gt;Does the blue LED light when the poawered board is then plugged into the Multilink?&lt;/P&gt;&lt;P&gt;Is the Multilink/PC combination known to function with some other device or is this all new to you?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes I am using P&amp;amp;E Multilink (USB-ML-12)&lt;/P&gt;&lt;P&gt;Yes I am using CodeWarrior on the PC&lt;/P&gt;&lt;P&gt;The blue light glows when the Multilink is plugged into the PC and the yellow light glows when the powered board is connected to it.&lt;/P&gt;&lt;P&gt;The Multilink/PC combination works with S12P and S12XS microcontrollers which I have been programming successfully since a long time.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any ideas why the connection manager for the programmer shows the MCU reset line to be low and why does the programmer pull the reset line low inspite of a pullup?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;--&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cmux&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Oct 2009 11:38:29 GMT</pubDate>
    <dc:creator>Cmux</dc:creator>
    <dc:date>2009-10-02T11:38:29Z</dc:date>
    <item>
      <title>USB Multilink</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125191#M521</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I have a problem when i connect my usb multilink with my µ, the message:&lt;/DIV&gt;&lt;DIV&gt;"Error can not background mode"&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Can you explain me this ?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jul 2006 21:13:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125191#M521</guid>
      <dc:creator>Batscap</dc:creator>
      <dc:date>2006-07-28T21:13:48Z</dc:date>
    </item>
    <item>
      <title>Re: USB Multilink</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125192#M522</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;More information would be very helpful in making us able to help you. A few basic things to check right off the bat:&lt;BR /&gt;&lt;BR /&gt;- Check that your chip is properly powered. (To begin with, just make sure that it's plugged in. Later, if it is still misbehaving, you could also check the power connections going into the mcu with a multimeter to make sure that it isn't a board fab issue)&lt;BR /&gt;&lt;BR /&gt;- Check that the multilink is properly connected, and drivers are installed. When it is connected to the computer and drivers are running, the blue LED should come on. Later, when connected to the chip and the chip is powered, a yellow LED should come on.&lt;BR /&gt;&lt;BR /&gt;- Make sure that you only have one instance of the debugger open at once. The hardware for debugging is locked to the first project that tries to use it, and will refresh for that project. However, if another project is attempting to enter debug, it won't read a multilink pod as being attached.&lt;BR /&gt;&lt;BR /&gt;- If you have access to another multilink pod, try that. If that doesn't work either, then you have largely ruled out the possibility that this is hardware failure on the part of the pod.&lt;BR /&gt;&lt;BR /&gt;Other than that, can you give any more info? The connection manager should come up at the beginning of attempted debugging - does it say anything in red, such as MCU reset line is low or voltage is low?&lt;BR /&gt;&lt;BR /&gt;Good luck, and let us know what you find out.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jul 2006 22:37:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125192#M522</guid>
      <dc:creator>RedMountain</dc:creator>
      <dc:date>2006-07-28T22:37:07Z</dc:date>
    </item>
    <item>
      <title>Re: USB Multilink</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125193#M523</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Also - try not to put the multilink through a USB hub.. I had erratic behavior having my BDM connected through one.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Jul 2006 01:01:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125193#M523</guid>
      <dc:creator>mjcoury</dc:creator>
      <dc:date>2006-07-29T01:01:27Z</dc:date>
    </item>
    <item>
      <title>Re: USB Multilink</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125194#M524</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;On the ICD Connection Manager&lt;/P&gt;&lt;P&gt;CPU : HCS08 Processor autodetected&lt;/P&gt;&lt;P&gt;MCU Reset line : High.&lt;/P&gt;&lt;P&gt;MCU voltage :&amp;nbsp;4.98V.&lt;/P&gt;&lt;P&gt;Note: failure connecting to device power cycle the hcs08 processor (with debug cable attached) and try connecting again.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Jul 2006 16:48:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125194#M524</guid>
      <dc:creator>Batscap</dc:creator>
      <dc:date>2006-07-31T16:48:26Z</dc:date>
    </item>
    <item>
      <title>Re: USB Multilink</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125195#M525</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;FONT face="Arial" size="2"&gt;and :&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Arial" size="2"&gt;Loading Target ...&lt;BR /&gt;Windows NT detected.&lt;BR /&gt;USB HCS08/HCS12 MULTILINK detected - Flash Version 5.28&lt;BR /&gt;Frequency change to ~269184hz.&lt;BR /&gt;USB HCS08/HCS12 MULTILINK detected - Flash Version 5.28&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Arial" size="2"&gt;Error: Can not enter background mode .&lt;BR /&gt;&lt;/FONT&gt;&lt;/DIV&gt;&lt;FONT color="#000000"&gt;&lt;/FONT&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Jul 2006 19:20:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125195#M525</guid>
      <dc:creator>Batscap</dc:creator>
      <dc:date>2006-07-31T19:20:06Z</dc:date>
    </item>
    <item>
      <title>Re: USB Multilink</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125196#M526</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I think the board is trying to tell you that the processor can't enter the background debug mode. Check your documentation and board jumpers to see if the board is configured for debug mode.&lt;BR /&gt;&lt;BR /&gt;---Tom&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Jul 2006 21:25:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125196#M526</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2006-07-31T21:25:45Z</dc:date>
    </item>
    <item>
      <title>Re: USB Multilink</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125197#M527</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;I work with the µ &lt;DIV&gt;&lt;A href="http://forums.freescale.com/" rel="nofollow" target="_blank"&gt;MC9S08AW16&lt;/A&gt;&lt;/DIV&gt;but i don't find this family on the CodeWarrior 5.1 family can you explain me ?&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Jul 2006 22:22:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125197#M527</guid>
      <dc:creator>Batscap</dc:creator>
      <dc:date>2006-07-31T22:22:59Z</dc:date>
    </item>
    <item>
      <title>Re: USB Multilink</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125198#M528</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Yeah, I can't find the MC9S08AW16 as a provided processor setting in Codewarrior either. Which header file are you currently using right now? The header file for the AW32 should be almost, if not exactly, identical.&lt;BR /&gt;&lt;BR /&gt;What are you programming onto the chip and trying to debug? It might be good to try a very simple program that does something like initialize a single port as output and toggle it, just to see if what you are programming is interfering with debugger operation.&lt;BR /&gt;&lt;BR /&gt;Good luck.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Jul 2006 22:43:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125198#M528</guid>
      <dc:creator>RedMountain</dc:creator>
      <dc:date>2006-07-31T22:43:14Z</dc:date>
    </item>
    <item>
      <title>Re: USB Multilink</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125199#M529</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;P&gt;I use the -S08AW16, and I think I had the same problem.&amp;nbsp; Use the -AW32 setting in CodeWarrior, then modify the ROM setting in the project.prm file according to the -AW16's data sheet.&lt;/P&gt;&lt;P&gt;Also, see if the attached helps.&amp;nbsp; Change the filename to *.ppt&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-Tomahawk&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/DIV&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by t.dowe on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-08-31&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;03:31 PM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Aug 2006 22:18:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125199#M529</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2006-08-02T22:18:46Z</dc:date>
    </item>
    <item>
      <title>Re: USB Multilink</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125200#M530</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Or pdf if you don't have powerpoint:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/files/community_files/8BITCOMM/TN247.pdf" rel="nofollow" target="_self"&gt;TN247.pdf&lt;/A&gt;&lt;/P&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by t.dowe on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-08-31&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;03:29 PM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Aug 2006 23:00:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125200#M530</guid>
      <dc:creator>RedMountain</dc:creator>
      <dc:date>2006-08-02T23:00:43Z</dc:date>
    </item>
    <item>
      <title>Re: USB Multilink</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125201#M531</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;You have to use the MCS08AW32xxx and modify the MC9S08AW32.inc file.&lt;/P&gt;&lt;P&gt;ROMStart is at $0c0000&lt;/P&gt;&lt;P&gt;RAMEnd is at $046F&lt;/P&gt;&lt;P&gt;Thats all.&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Truk&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Aug 2006 20:09:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125201#M531</guid>
      <dc:creator>Truk</dc:creator>
      <dc:date>2006-08-03T20:09:11Z</dc:date>
    </item>
    <item>
      <title>Re: USB Multilink</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125202#M532</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have made a very simple board consisting of just MC9S08SG8 with its RESET pin pulled up (10k), BKGD pulled up (10k) and a decoupling capacitor (0.1u) across Vdd and GND. Apart from this there is a BDM header through which I am trying to program the microcontroller. While programming the connection manager tells me that the RESET line is low inspite of the pullup I have connected. Is there something more that I need to add to the programming circuit? Another piece of debugging information is that when I connect the programmer to the BDM header, the RESET voltage falls to 0.65V from 5V.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kindly help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;--&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cmux&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Oct 2009 18:26:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125202#M532</guid>
      <dc:creator>Cmux</dc:creator>
      <dc:date>2009-10-01T18:26:38Z</dc:date>
    </item>
    <item>
      <title>Re: USB Multilink</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125203#M533</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Cmux,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Are you using a P&amp;amp;E Multilink (USB-ML-12)?&lt;/P&gt;&lt;P&gt;Are you using Codewarrior on the PC?&lt;/P&gt;&lt;P&gt;Does the yellow LED light when Multilink is plugged in to PC on its own?&lt;/P&gt;&lt;P&gt;Does the blue LED light when the poawered board is then plugged into the Multilink?&lt;/P&gt;&lt;P&gt;Is the Multilink/PC combination known to function with some other device or is this all new to you?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Oct 2009 06:00:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125203#M533</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2009-10-02T06:00:38Z</dc:date>
    </item>
    <item>
      <title>Re: USB Multilink</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125204#M534</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;peg wrote:&lt;BR /&gt;&lt;P&gt;Hello Cmux,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Are you using a P&amp;amp;E Multilink (USB-ML-12)?&lt;/P&gt;&lt;P&gt;Are you using Codewarrior on the PC?&lt;/P&gt;&lt;P&gt;Does the yellow LED light when Multilink is plugged in to PC on its own?&lt;/P&gt;&lt;P&gt;Does the blue LED light when the poawered board is then plugged into the Multilink?&lt;/P&gt;&lt;P&gt;Is the Multilink/PC combination known to function with some other device or is this all new to you?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes I am using P&amp;amp;E Multilink (USB-ML-12)&lt;/P&gt;&lt;P&gt;Yes I am using CodeWarrior on the PC&lt;/P&gt;&lt;P&gt;The blue light glows when the Multilink is plugged into the PC and the yellow light glows when the powered board is connected to it.&lt;/P&gt;&lt;P&gt;The Multilink/PC combination works with S12P and S12XS microcontrollers which I have been programming successfully since a long time.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any ideas why the connection manager for the programmer shows the MCU reset line to be low and why does the programmer pull the reset line low inspite of a pullup?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;--&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cmux&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Oct 2009 11:38:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125204#M534</guid>
      <dc:creator>Cmux</dc:creator>
      <dc:date>2009-10-02T11:38:29Z</dc:date>
    </item>
    <item>
      <title>Re: USB Multilink</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125205#M535</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Cmux,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Woops, I got my LED colours mixed up in my questions.&lt;/P&gt;&lt;P&gt;This seems strange.&lt;/P&gt;&lt;P&gt;Just to check some more:&lt;/P&gt;&lt;P&gt;You power up the device on its own and the reset pin is at 5 volts.&lt;/P&gt;&lt;P&gt;You connect the Multilink and it pulls the reset permanently low.&lt;/P&gt;&lt;P&gt;Then Codewarrior complains about the reset line being low.&lt;/P&gt;&lt;P&gt;Is this correct?&lt;/P&gt;&lt;P&gt;What if you disconnect the reset line and try to connect like this.&lt;/P&gt;&lt;P&gt;Also test the reset line (both sides of break) while trying this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Oct 2009 13:12:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Multilink/m-p/125205#M535</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2009-10-02T13:12:12Z</dc:date>
    </item>
  </channel>
</rss>