<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Interfacing an mmc/sd memory card to hc08</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Interfacing-an-mmc-sd-memory-card-to-hc08/m-p/138923#M5147</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;Does anyone has an application note or any example in which an hc08ap32 &amp;nbsp;spi port is connected to an mmc/sd memory card.&lt;/DIV&gt;&lt;DIV&gt;Im trying but we have some troubles , the system works well&amp;nbsp;in debug mode, but not alone.The spi signals are ok, and micro works fine.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Also when we connect the micro with the card together it does not work, (the supply pwer goes down)&lt;/DIV&gt;&lt;DIV&gt;but if you connect first the micro and then insert the card it works,&lt;/DIV&gt;&lt;DIV&gt;Any idea will be welcome.&lt;/DIV&gt;&lt;DIV&gt;thanks a lot.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 08 Jun 2006 20:49:38 GMT</pubDate>
    <dc:creator>marbia</dc:creator>
    <dc:date>2006-06-08T20:49:38Z</dc:date>
    <item>
      <title>Interfacing an mmc/sd memory card to hc08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Interfacing-an-mmc-sd-memory-card-to-hc08/m-p/138923#M5147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;Does anyone has an application note or any example in which an hc08ap32 &amp;nbsp;spi port is connected to an mmc/sd memory card.&lt;/DIV&gt;&lt;DIV&gt;Im trying but we have some troubles , the system works well&amp;nbsp;in debug mode, but not alone.The spi signals are ok, and micro works fine.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Also when we connect the micro with the card together it does not work, (the supply pwer goes down)&lt;/DIV&gt;&lt;DIV&gt;but if you connect first the micro and then insert the card it works,&lt;/DIV&gt;&lt;DIV&gt;Any idea will be welcome.&lt;/DIV&gt;&lt;DIV&gt;thanks a lot.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jun 2006 20:49:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Interfacing-an-mmc-sd-memory-card-to-hc08/m-p/138923#M5147</guid>
      <dc:creator>marbia</dc:creator>
      <dc:date>2006-06-08T20:49:38Z</dc:date>
    </item>
    <item>
      <title>Re: Interfacing an mmc/sd memory card to hc08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Interfacing-an-mmc-sd-memory-card-to-hc08/m-p/138924#M5148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;&lt;FONT size="3"&gt;No example, but:&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="3"&gt;I use an MMC (in SPI mode) with a GB60 without any problems.&amp;nbsp; Here's the inter-connection:&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="1"&gt;-------------------------------------------&lt;BR /&gt;&amp;nbsp;9S08GB60 Pins&amp;nbsp;&amp;nbsp; |MMC PIN#| MMC Description&lt;BR /&gt;-----------------+--------+----------------&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="1"&gt;&amp;nbsp;PE2 / SPI SS&amp;nbsp;&amp;nbsp;&amp;nbsp; |&amp;nbsp;&amp;nbsp; 1&amp;nbsp;&amp;nbsp;&amp;nbsp; | Chip Select&lt;BR /&gt;&amp;nbsp;PE4 / SPI MOSI&amp;nbsp;&amp;nbsp;|&amp;nbsp;&amp;nbsp; 2&amp;nbsp;&amp;nbsp;&amp;nbsp; | DataIn&lt;BR /&gt;&amp;nbsp;Vss&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;|&amp;nbsp;&amp;nbsp; 3&amp;nbsp;&amp;nbsp;&amp;nbsp; | GND&lt;BR /&gt;&amp;nbsp;Vdd&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;|&amp;nbsp;&amp;nbsp; 4&amp;nbsp;&amp;nbsp;&amp;nbsp; | +2.7-3.6V&lt;BR /&gt;&amp;nbsp;PE5 / SPI SCLK&amp;nbsp;&amp;nbsp;|&amp;nbsp;&amp;nbsp; 5&amp;nbsp;&amp;nbsp;&amp;nbsp; | CLK&lt;BR /&gt;&amp;nbsp;Vss&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;|&amp;nbsp;&amp;nbsp; 6&amp;nbsp;&amp;nbsp;&amp;nbsp; | GND&lt;BR /&gt;&amp;nbsp;PE3 / SPI MISO&amp;nbsp;&amp;nbsp;|&amp;nbsp;&amp;nbsp; 7&amp;nbsp;&amp;nbsp;&amp;nbsp; | DataOut&lt;BR /&gt;-----------------+--------+----------------&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="3"&gt;AFAIK, most cards work at 3V. Are you running the AP32 at 3V or 5V?&amp;nbsp; If at 5V, maybe your level conversion circuit isn't working as expected.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="3"&gt;About the debug/standalone difference, here's one possibility:&amp;nbsp; Some cards (as the protocol notes I have say) expect an initialization with a slower rate (I think it is about 400KHz), then you can switch to faster SPI rates.&amp;nbsp; So, maybe while in debug (because of the extra overhead or instruction stepping) the rate is within range but gets out of range in standalone mode.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="3"&gt;Hope this helps.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="1"&gt;&lt;FONT face="Arial" size="3"&gt;Now, while we're on the subject I've got a question, too.&amp;nbsp; Anyone know how to address more than 32MB?&amp;nbsp; Haven't been able to find any freely available reference to this yet.&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="3"&gt;TIA&lt;/FONT&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jun 2006 22:44:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Interfacing-an-mmc-sd-memory-card-to-hc08/m-p/138924#M5148</guid>
      <dc:creator>tonyp</dc:creator>
      <dc:date>2006-06-08T22:44:56Z</dc:date>
    </item>
    <item>
      <title>Re: Interfacing an mmc/sd memory card to hc08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Interfacing-an-mmc-sd-memory-card-to-hc08/m-p/138925#M5149</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Thanks&amp;nbsp; for the data.&lt;/DIV&gt;&lt;DIV&gt;Do you have the same problem during init procedure, we are working at 3.3v&lt;/DIV&gt;&lt;DIV&gt;the initialization clock always must to be slow?.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;What do you mean when say 32 Mbytes, only,&lt;/DIV&gt;&lt;DIV&gt;that is FFFF * 200, the capacity to address via spi? I really dont think&amp;nbsp; to this point yet&amp;nbsp;, but it may be a problem.&lt;/DIV&gt;&lt;DIV&gt;Im new to this enviroment but&amp;nbsp; What about multiple block write?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Jun 2006 00:43:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Interfacing-an-mmc-sd-memory-card-to-hc08/m-p/138925#M5149</guid>
      <dc:creator>marbia</dc:creator>
      <dc:date>2006-06-09T00:43:01Z</dc:date>
    </item>
    <item>
      <title>Re: Interfacing an mmc/sd memory card to hc08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Interfacing-an-mmc-sd-memory-card-to-hc08/m-p/138926#M5150</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;With 6 bytes for adressing you shouldnt have any problem to get more than 32 Mega. Are you using fat 12 instead of fat 16 . This could be a limitation.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Jun 2006 19:16:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Interfacing-an-mmc-sd-memory-card-to-hc08/m-p/138926#M5150</guid>
      <dc:creator>marbia</dc:creator>
      <dc:date>2006-06-09T19:16:31Z</dc:date>
    </item>
    <item>
      <title>Re: Interfacing an mmc/sd memory card to hc08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Interfacing-an-mmc-sd-memory-card-to-hc08/m-p/138927#M5151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Does anyone have any source code for reading/writing to a FAT16 filesystem(on a SD card) from a HCS08 (GT/GB series)?&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Aug 2006 23:35:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Interfacing-an-mmc-sd-memory-card-to-hc08/m-p/138927#M5151</guid>
      <dc:creator>kbu</dc:creator>
      <dc:date>2006-08-03T23:35:18Z</dc:date>
    </item>
  </channel>
</rss>