<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Baud Rate and the MC9S080G8 uCtrl</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Baud-Rate-and-the-MC9S080G8-uCtrl/m-p/138452#M4983</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hi Brian,&lt;/P&gt;&lt;P&gt;First I will presume you mean QG8,&lt;/P&gt;&lt;P&gt;Answer is 8MHz.&lt;/P&gt;&lt;P&gt;a.) Statement is WRONG!&lt;/P&gt;&lt;P&gt;b.) Statement is correct.&lt;/P&gt;&lt;P&gt;c.) Drawing is correct. The 2^n divider is controlled by BDIV which has a reset default of 01 which means /2.&lt;/P&gt;&lt;P&gt;Regards David&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Jun 2006 05:36:37 GMT</pubDate>
    <dc:creator>peg</dc:creator>
    <dc:date>2006-06-07T05:36:37Z</dc:date>
    <item>
      <title>Baud Rate and the MC9S080G8 uCtrl</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Baud-Rate-and-the-MC9S080G8-uCtrl/m-p/138451#M4982</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Im using the internal 16MHZ osc with the default ICS settings.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="text-decoration: underline;"&gt;My question is:&lt;/SPAN&gt; &lt;EM&gt;&lt;STRONG&gt;"What speed does the BUSS run @ when using the Default 16Mhz clock?"&lt;/STRONG&gt;&lt;/EM&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;When looking thru the datasheet of the subject controller it shows three different things:&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="color: #ff0000;"&gt;a)&lt;/SPAN&gt; The internal frequency settings is nominally 16Mhz and will provide a 4Mhz BUSS out of a RESET.&amp;nbsp; (section 2.2.2, Oscilator section of datasheet)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="color: #ff0000;"&gt;b)&lt;/SPAN&gt; The BUSS frequency will be 1/2 of the ICSOUT frequency (section 10.1, of datasheet)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="color: #ff0000;"&gt;c)&lt;/SPAN&gt; The diagram shown in Figure 10.2 shows the ICSOUT signal being fed ny a 2^n divider, not a divide by two.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Can anyone help clear up my discrepencies,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks&lt;/DIV&gt;&lt;DIV&gt;Brian&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Jun 2006 22:06:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Baud-Rate-and-the-MC9S080G8-uCtrl/m-p/138451#M4982</guid>
      <dc:creator>Cennedie</dc:creator>
      <dc:date>2006-06-06T22:06:59Z</dc:date>
    </item>
    <item>
      <title>Re: Baud Rate and the MC9S080G8 uCtrl</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Baud-Rate-and-the-MC9S080G8-uCtrl/m-p/138452#M4983</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hi Brian,&lt;/P&gt;&lt;P&gt;First I will presume you mean QG8,&lt;/P&gt;&lt;P&gt;Answer is 8MHz.&lt;/P&gt;&lt;P&gt;a.) Statement is WRONG!&lt;/P&gt;&lt;P&gt;b.) Statement is correct.&lt;/P&gt;&lt;P&gt;c.) Drawing is correct. The 2^n divider is controlled by BDIV which has a reset default of 01 which means /2.&lt;/P&gt;&lt;P&gt;Regards David&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jun 2006 05:36:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Baud-Rate-and-the-MC9S080G8-uCtrl/m-p/138452#M4983</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2006-06-07T05:36:37Z</dc:date>
    </item>
    <item>
      <title>Re: Baud Rate and the MC9S080G8 uCtrl</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Baud-Rate-and-the-MC9S080G8-uCtrl/m-p/138453#M4984</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Passed onto Datasheet owner&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jun 2006 15:04:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Baud-Rate-and-the-MC9S080G8-uCtrl/m-p/138453#M4984</guid>
      <dc:creator>Alban</dc:creator>
      <dc:date>2006-06-07T15:04:59Z</dc:date>
    </item>
    <item>
      <title>Re: Baud Rate and the MC9S080G8 uCtrl</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Baud-Rate-and-the-MC9S080G8-uCtrl/m-p/138454#M4985</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hi Brian,&lt;/P&gt;&lt;P&gt;My first response is WRONG!&lt;/P&gt;&lt;P&gt;The sections of the manual you refer to are ALL CORRECT!&lt;/P&gt;&lt;P&gt;The answer is 4MHz&lt;/P&gt;&lt;P&gt;For an explanation refer to Figure 10.2.&lt;/P&gt;&lt;P&gt;Start at the internal reference clock in the middle.&lt;BR /&gt;It runs at nominally 16MHz.&lt;BR /&gt;To IREFS.&lt;BR /&gt;IREFS defaults to 1 which selects internal rather than external clock.&lt;BR /&gt;Then through programmable divider controlled by RDIV.&lt;BR /&gt;RDIV defaults to 000 which is divide by 1. (16MHz)&lt;BR /&gt;Into the FLL.&lt;BR /&gt;CLKS defaults to 00 which selects the output of the FLL&lt;BR /&gt;then to another programmable divider controlled by BDIV.&lt;BR /&gt;BDIV defaults to 01 which is divide by 2. (8MHz)&lt;BR /&gt;Now the signal is called ICSOUT.&lt;BR /&gt;This is then divided by 2 to produce BUSCLK.(4MHz). (as noted in OP's b) section 10.1)&lt;/P&gt;&lt;P&gt;Sorry if I have lead anyone astray.&lt;/P&gt;&lt;P&gt;Alban, quick get that note to the datasheet owner back before he thinks we are all illiterate, especially me, then you and the 53 people that read my incorrect response without comment. &lt;IMG alt=":smileyvery-happy:" class="emoticon emoticon-smileyvery-happy" id="smileyvery-happy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-very-happy.gif" title="Smiley Very Happy" /&gt;&lt;/P&gt;&lt;P&gt;Regards David&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Message Edited by peg on &lt;SPAN class="date_text"&gt;2006-06-08&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;09:39 PM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jun 2006 18:36:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Baud-Rate-and-the-MC9S080G8-uCtrl/m-p/138454#M4985</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2006-06-08T18:36:47Z</dc:date>
    </item>
  </channel>
</rss>