<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 908LJ12 - frequency meter in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/908LJ12-frequency-meter/m-p/138374#M4951</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hi Hasan,&lt;BR /&gt;&lt;BR /&gt;If the LJ12 is indeed a member of the HC08 family (I did not verify) and you are running it at 5 volts, then the resolution of the timer is 125 nanoseconds with the maximum bus clock of 8Mhz. But this is not the full story.&lt;BR /&gt;&lt;BR /&gt;To use it as a frequency counter, you will need to service an interrupt per cycle, and that will take over 2 microseconds minimum for each cycle. With background processing, you might be able to measure as fast as 400khz. It may work well for audio.&lt;BR /&gt;&lt;BR /&gt;When I measure frequency, I use a high-speed, pipelined counter in and FPGA, that I then control with the output-compare function of the timer. But I have never needed to measure faster than a few tens of megahertz.&lt;BR /&gt;&lt;BR /&gt;HTH&lt;BR /&gt;&lt;BR /&gt;--&lt;BR /&gt;Alban Edit: Part number must be shown in subject line&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by Alban on &lt;SPAN class="date_text"&gt;2007-06-27&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;02:15 AM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Jun 2007 02:43:42 GMT</pubDate>
    <dc:creator>rocco</dc:creator>
    <dc:date>2007-06-27T02:43:42Z</dc:date>
    <item>
      <title>908LJ12 - frequency meter</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/908LJ12-frequency-meter/m-p/138373#M4950</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;Hi;&lt;/DIV&gt;&lt;DIV&gt;i wanna make a freq. counter, i have been searched for the resolution of the capture module in the datasheet of 908LJ12 controller, but unfortunately i didn't find it's resolution, for example say&amp;nbsp;PIC controllers Capture module with 12.5 nsec.&lt;/DIV&gt;&lt;DIV&gt;i need to know what's the resolution of the 908LJ12 controller;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;regards&lt;/DIV&gt;&lt;DIV&gt;Hasan&lt;BR /&gt;&lt;BR /&gt;--&lt;BR /&gt;Alban Edit: Part number must be shown in subject line&lt;BR /&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Message Edited by Alban on &lt;/SPAN&gt;&lt;SPAN class="date_text"&gt;2007-06-27&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;02:15 AM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jun 2007 00:48:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/908LJ12-frequency-meter/m-p/138373#M4950</guid>
      <dc:creator>mohammed</dc:creator>
      <dc:date>2007-06-27T00:48:46Z</dc:date>
    </item>
    <item>
      <title>Re: 908LJ12 - frequency meter</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/908LJ12-frequency-meter/m-p/138374#M4951</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hi Hasan,&lt;BR /&gt;&lt;BR /&gt;If the LJ12 is indeed a member of the HC08 family (I did not verify) and you are running it at 5 volts, then the resolution of the timer is 125 nanoseconds with the maximum bus clock of 8Mhz. But this is not the full story.&lt;BR /&gt;&lt;BR /&gt;To use it as a frequency counter, you will need to service an interrupt per cycle, and that will take over 2 microseconds minimum for each cycle. With background processing, you might be able to measure as fast as 400khz. It may work well for audio.&lt;BR /&gt;&lt;BR /&gt;When I measure frequency, I use a high-speed, pipelined counter in and FPGA, that I then control with the output-compare function of the timer. But I have never needed to measure faster than a few tens of megahertz.&lt;BR /&gt;&lt;BR /&gt;HTH&lt;BR /&gt;&lt;BR /&gt;--&lt;BR /&gt;Alban Edit: Part number must be shown in subject line&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by Alban on &lt;SPAN class="date_text"&gt;2007-06-27&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;02:15 AM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jun 2007 02:43:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/908LJ12-frequency-meter/m-p/138374#M4951</guid>
      <dc:creator>rocco</dc:creator>
      <dc:date>2007-06-27T02:43:42Z</dc:date>
    </item>
  </channel>
</rss>