<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC9S08GB60 Internal Number in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08GB60-Internal-Number/m-p/125041#M487</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;No,&lt;BR /&gt;There is no serial number you can read.&lt;BR /&gt;However, some programmer are able to create one when the software is put into Flash in the programming house.&lt;BR /&gt;Cheers,&lt;BR /&gt;Alban.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Jul 2006 03:30:00 GMT</pubDate>
    <dc:creator>Alban</dc:creator>
    <dc:date>2006-07-27T03:30:00Z</dc:date>
    <item>
      <title>MC9S08GB60 Internal Number</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08GB60-Internal-Number/m-p/125040#M486</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Is there an internal unique number that is recorded in the MC9S08GB60 that I can read using C that would be unique with each CPU?&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jul 2006 01:05:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08GB60-Internal-Number/m-p/125040#M486</guid>
      <dc:creator>billp</dc:creator>
      <dc:date>2006-07-27T01:05:43Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08GB60 Internal Number</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08GB60-Internal-Number/m-p/125041#M487</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;No,&lt;BR /&gt;There is no serial number you can read.&lt;BR /&gt;However, some programmer are able to create one when the software is put into Flash in the programming house.&lt;BR /&gt;Cheers,&lt;BR /&gt;Alban.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jul 2006 03:30:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08GB60-Internal-Number/m-p/125041#M487</guid>
      <dc:creator>Alban</dc:creator>
      <dc:date>2006-07-27T03:30:00Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08GB60 Internal Number</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08GB60-Internal-Number/m-p/125042#M488</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;&lt;FONT size="2"&gt;Hello,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;P&amp;amp;E have a "Serialize" utility available from their web site.&amp;nbsp; This might do what you you require.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Regards,&lt;BR /&gt;Mac&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jul 2006 04:50:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08GB60-Internal-Number/m-p/125042#M488</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2006-07-27T04:50:08Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08GB60 Internal Number</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08GB60-Internal-Number/m-p/125043#M489</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;If you have need of a peripheral, see if you can get a unique number from that.&lt;BR /&gt;&lt;BR /&gt;I have a small weather device that I used a DS18S20 temerature sensor part on, and it's 1-wire address is perfect for providing a serial number on the fly for the entire unit. Hey, if you gotta have the part anyway, choose it wisely!&lt;BR /&gt;&lt;BR /&gt;The only caveat is if you change that part... I've had 2 units where I had to change that part. One shorted out and the other was physically broken off the unit. (It sticks out to have the best response time to temperature changes.) I had to make allowances in my tracking software to be able to change that number 'on the fly' for repairs.&lt;BR /&gt;&lt;BR /&gt;Mike&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jul 2006 21:50:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08GB60-Internal-Number/m-p/125043#M489</guid>
      <dc:creator>mke_et</dc:creator>
      <dc:date>2006-07-27T21:50:23Z</dc:date>
    </item>
  </channel>
</rss>