<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: HC908GP __isflag_carry()</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908GP-isflag-carry/m-p/137512#M4709</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Yeah,&amp;nbsp;I got the part about looking at it - I assumed that turning off optimizations was the desired setting, so I figured having it "checked" was right...&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I'm not all _that_ young...&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks to all for the help.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Carlos&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Nov 2006 05:10:17 GMT</pubDate>
    <dc:creator>CJH</dc:creator>
    <dc:date>2006-11-23T05:10:17Z</dc:date>
    <item>
      <title>HC908GP __isflag_carry()</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908GP-isflag-carry/m-p/137504#M4701</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I'm trying to check the carry bit using __isflag_carry() but keep getting the linker error&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;L1822: Symbol __isflag_carry in file ....c.o is undefined&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;According to the manual file,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;"To avoid using HLI for this purpose, the Compiler offers a set of intrinsic functions. The code of these functions is inlined. The processor flags listed in &lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=mk%3A%40MSITStore%3AC%3A%2FProgram%2520Files%2FFreescale%2FCodeWarrior%2520for%2520HC08%2520V5.1%2FHelp%2FCompiler_HC08.chm%3A%3A%2FHC08_Compiler-11-11.html%23wp967220" rel="nofollow" target="_blank"&gt;Table 8.3&lt;/A&gt; are read by the associated intrinsic function. "&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Since it's supposed to be intrinsic, there does not appear to be a .h file to declare it.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;What am I missing?&amp;nbsp; (CW V5.7.0 Build 2015, HC908GP)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Nov 2006 06:26:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908GP-isflag-carry/m-p/137504#M4701</guid>
      <dc:creator>CJH</dc:creator>
      <dc:date>2006-11-22T06:26:57Z</dc:date>
    </item>
    <item>
      <title>Re: HC908GP __isflag_carry()</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908GP-isflag-carry/m-p/137505#M4702</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;The following sample builds/runs fine for me (default options)&lt;BR /&gt;&lt;BR /&gt;Daniel&lt;BR /&gt;&lt;BR /&gt;&lt;PRE&gt;
#include &amp;lt;hidef.h&amp;gt;
#include "derivative.h"

void Err() { for (;;) { /* wait here */ } }

char __isflag_carry(void);

char fun(unsigned char a) {
  __asm ADD #1;
  return __isflag_carry();
}
void main() {
  if (fun(1) != 0) {
    Err();
  }
  if (fun(255) != 1) {
    Err();
  }

  for(;;) {
    __RESET_WATCHDOG(); /* feeds the dog */
  }
}
&lt;/PRE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;PRE&gt;
    9:    __asm ADD #1;
  0000 ab01     [2]             ADD   #1
   10:    return __isflag_carry();
  0002 2502     [3]             BCS   L6 ;abs = 0006
  0004 4f       [1]             CLRA 
  0005 81       [4]             RTS  
  0006          [5]     L6:    
  0006 a601     [2]             LDA   #1
   11:  }
  0008 81       [4]             RTS  
   12:  void main() {
&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Nov 2006 00:58:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908GP-isflag-carry/m-p/137505#M4702</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2006-11-23T00:58:56Z</dc:date>
    </item>
    <item>
      <title>Re: HC908GP __isflag_carry()</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908GP-isflag-carry/m-p/137506#M4703</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Check your compiler option "Disable optimizations".&lt;BR /&gt;Al&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Nov 2006 01:13:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908GP-isflag-carry/m-p/137506#M4703</guid>
      <dc:creator>Geezer</dc:creator>
      <dc:date>2006-11-23T01:13:06Z</dc:date>
    </item>
    <item>
      <title>Re: HC908GP __isflag_carry()</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908GP-isflag-carry/m-p/137507#M4704</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Strange - I copied your code into CW and compiled and I get:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;12:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __asm ADD #1;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;0000 ab01&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; [2]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADD&amp;nbsp;&amp;nbsp; #1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;13:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return __isflag_carry();&lt;BR /&gt;&amp;nbsp;0002 cd0000&amp;nbsp;&amp;nbsp; [5]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; JSR&amp;nbsp;&amp;nbsp; __isflag_carry&lt;BR /&gt;&amp;nbsp;&amp;nbsp;14:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp;0005 81&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; [4]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; RTS&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;15:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;16:&amp;nbsp; void main() {&lt;BR /&gt;&lt;/DIV&gt;&lt;DIV&gt;Which of course results in the __isflag_carry undefined message from the linker...&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;What version of CW are you running?&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Nov 2006 02:07:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908GP-isflag-carry/m-p/137507#M4704</guid>
      <dc:creator>CJH</dc:creator>
      <dc:date>2006-11-23T02:07:20Z</dc:date>
    </item>
    <item>
      <title>Re: HC908GP __isflag_carry()</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908GP-isflag-carry/m-p/137508#M4705</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I do have "disable optimizations" checked in the compiler options tab.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Nov 2006 02:08:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908GP-isflag-carry/m-p/137508#M4705</guid>
      <dc:creator>CJH</dc:creator>
      <dc:date>2006-11-23T02:08:11Z</dc:date>
    </item>
    <item>
      <title>Re: HC908GP __isflag_carry()</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908GP-isflag-carry/m-p/137509#M4706</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I see, it's a silly behavior of the -ont option.&lt;BR /&gt;If you disable the complete tree optimizer, then the intrinsics are not recognized :smileysad:&lt;BR /&gt;2 solutions:&lt;BR /&gt;- only disable the treeopt suboptimization you really do not want. So instead of -ont, use -ont=ab.......&lt;BR /&gt;- define the __isflag_carry function in another module.&lt;BR /&gt;As the function is only called with disabled optimizations, it wont affect the release build. And the debug build will just call it.&lt;BR /&gt;&lt;BR /&gt;Daniel&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Nov 2006 04:21:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908GP-isflag-carry/m-p/137509#M4706</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2006-11-23T04:21:04Z</dc:date>
    </item>
    <item>
      <title>Re: HC908GP __isflag_carry()</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908GP-isflag-carry/m-p/137510#M4707</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;CJH:&lt;BR /&gt;&lt;BR /&gt;For younger generations checking something means clicking on a little square icon.&lt;BR /&gt;&lt;BR /&gt;Sigh.Poor modern English on my part... when I said to "check" an item I meant it in the older sense of "go look at it".&lt;BR /&gt;&lt;BR /&gt;Al&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Nov 2006 04:39:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908GP-isflag-carry/m-p/137510#M4707</guid>
      <dc:creator>Geezer</dc:creator>
      <dc:date>2006-11-23T04:39:11Z</dc:date>
    </item>
    <item>
      <title>Re: HC908GP __isflag_carry()</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908GP-isflag-carry/m-p/137511#M4708</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Man, I would never have figured that out - disabling optimizations disables intrinsics too!&amp;nbsp; Certainly not obvious to me, and I don't think a very desirable behavior...&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thank you!&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Nov 2006 05:07:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908GP-isflag-carry/m-p/137511#M4708</guid>
      <dc:creator>CJH</dc:creator>
      <dc:date>2006-11-23T05:07:57Z</dc:date>
    </item>
    <item>
      <title>Re: HC908GP __isflag_carry()</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908GP-isflag-carry/m-p/137512#M4709</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Yeah,&amp;nbsp;I got the part about looking at it - I assumed that turning off optimizations was the desired setting, so I figured having it "checked" was right...&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I'm not all _that_ young...&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks to all for the help.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Carlos&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Nov 2006 05:10:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908GP-isflag-carry/m-p/137512#M4709</guid>
      <dc:creator>CJH</dc:creator>
      <dc:date>2006-11-23T05:10:17Z</dc:date>
    </item>
    <item>
      <title>Re: HC908GP __isflag_carry()</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908GP-isflag-carry/m-p/137513#M4710</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;As a matter of curiosity, do both&amp;nbsp;the two different compiled versions produce the&amp;nbsp;intended result?&amp;nbsp; It appears to me that one version may make a macro substitution, and the other version makes a sub-routine call, with either version&amp;nbsp;giving&amp;nbsp;correct operation.&amp;nbsp; Does it have something to do with the compiler optimising for speed, or code compactness&lt;/FONT&gt;&lt;FONT size="2"&gt;?&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Just a thought.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Nov 2006 09:34:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908GP-isflag-carry/m-p/137513#M4710</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2006-11-23T09:34:40Z</dc:date>
    </item>
    <item>
      <title>Re: HC908GP __isflag_carry()</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908GP-isflag-carry/m-p/137514#M4711</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Mac,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The main problem I was having is that it's NOT defined anywhere else - there is no such subroutine, so the version compiled with a subroutine call produces an error in linking since the linker doesn't find that subroutine anywhere.&amp;nbsp; So no, they don't produce equivalent results, at least not in my opinion...&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Carlos&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Nov 2006 20:49:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HC908GP-isflag-carry/m-p/137514#M4711</guid>
      <dc:creator>CJH</dc:creator>
      <dc:date>2006-11-27T20:49:18Z</dc:date>
    </item>
  </channel>
</rss>