<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Software Toll for Reading and Setting ENBDM in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Software-Toll-for-Reading-and-Setting-ENBDM/m-p/137103#M4607</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Hi Pegasus,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I think you are correct, I think that when the BDM pod is connected it likes to set this bit so it can be in control. I don't think there is a way to directly control or read the BDSCR register from Codewarrior or P&amp;amp;E software.&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;There are dedicated BDM commands for this (READ_STATUS and WRITE_CONTROL).&lt;/DIV&gt;&lt;DIV&gt;But the software does it all for you automatically.&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Gabriel Dubatti's BDMLoader can but it uses its own pod which is a problem for you with your built in pod.&lt;/DIV&gt;&lt;DIV&gt;You can drive BDMLoader from a terminal where you have full access to the raw commands.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I presume you are powering the board via the USB cable?&lt;/DIV&gt;&lt;DIV&gt;Have you tried to go to STOP1 after a power on reset without any software running? This way ENBDM should still be a 0 (unless the hardware does it on its own???)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards&lt;/DIV&gt;&lt;DIV&gt;David&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;Message Edited by peg on &lt;SPAN class="date_text"&gt;2006-11-20&lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;07:41 AM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 20 Nov 2006 05:36:12 GMT</pubDate>
    <dc:creator>peg</dc:creator>
    <dc:date>2006-11-20T05:36:12Z</dc:date>
    <item>
      <title>Software Toll for Reading and Setting ENBDM</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Software-Toll-for-Reading-and-Setting-ENBDM/m-p/137102#M4606</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I'm trying to put&amp;nbsp; DEMO9S08QG8E (demo board for MS9S08QG8) into STOP 1 mode. But when exiting the STOP Mode I receive&amp;nbsp;the message "exiting stop 3 mode". I suspect that ENBDM is set.&lt;/DIV&gt;&lt;DIV&gt;I'm connected to the board using USB. The baord include P&amp;amp;E USB-DBC controller.&lt;/DIV&gt;&lt;DIV&gt;I couldn't find how the read and set ENBDM (Actually BDSCR) using codeWarrier 5.0. Can someone help in explaining how to use CodeWarrier, or recommend a software tool for reading and setting BDSCR?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Pegasus&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Nov 2006 01:10:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Software-Toll-for-Reading-and-Setting-ENBDM/m-p/137102#M4606</guid>
      <dc:creator>Pegasus</dc:creator>
      <dc:date>2006-11-18T01:10:22Z</dc:date>
    </item>
    <item>
      <title>Re: Software Toll for Reading and Setting ENBDM</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Software-Toll-for-Reading-and-Setting-ENBDM/m-p/137103#M4607</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Hi Pegasus,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I think you are correct, I think that when the BDM pod is connected it likes to set this bit so it can be in control. I don't think there is a way to directly control or read the BDSCR register from Codewarrior or P&amp;amp;E software.&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;There are dedicated BDM commands for this (READ_STATUS and WRITE_CONTROL).&lt;/DIV&gt;&lt;DIV&gt;But the software does it all for you automatically.&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Gabriel Dubatti's BDMLoader can but it uses its own pod which is a problem for you with your built in pod.&lt;/DIV&gt;&lt;DIV&gt;You can drive BDMLoader from a terminal where you have full access to the raw commands.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I presume you are powering the board via the USB cable?&lt;/DIV&gt;&lt;DIV&gt;Have you tried to go to STOP1 after a power on reset without any software running? This way ENBDM should still be a 0 (unless the hardware does it on its own???)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards&lt;/DIV&gt;&lt;DIV&gt;David&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;Message Edited by peg on &lt;SPAN class="date_text"&gt;2006-11-20&lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;07:41 AM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Nov 2006 05:36:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Software-Toll-for-Reading-and-Setting-ENBDM/m-p/137103#M4607</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2006-11-20T05:36:12Z</dc:date>
    </item>
  </channel>
</rss>