<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Vector interrupt in MC68HC908GZ60</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Vector-interrupt-in-MC68HC908GZ60/m-p/136875#M4503</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The interrupt vector numbers are just the word number counting down from FFFF. The reset vector is FFFE:FFFF and is 0 and so on. If you refer to the datasheet you can use the IF numbers in the table for the Interrupt status register and add one to these values.&lt;/P&gt;&lt;P&gt;Regards David&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 May 2006 17:47:52 GMT</pubDate>
    <dc:creator>peg</dc:creator>
    <dc:date>2006-05-24T17:47:52Z</dc:date>
    <item>
      <title>Vector interrupt in MC68HC908GZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Vector-interrupt-in-MC68HC908GZ60/m-p/136874#M4502</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi everybody,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;How do I can know the default vector for interrupt (for MC68HC908GZ60) such as: TBM, TIM1 overflow ... in MC68HC908GZ60. For example, vector for TBM is 17. What's about TIM1 overflow, ...?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks alot&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Best regards&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 May 2006 17:26:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Vector-interrupt-in-MC68HC908GZ60/m-p/136874#M4502</guid>
      <dc:creator>baonguyen</dc:creator>
      <dc:date>2006-05-24T17:26:18Z</dc:date>
    </item>
    <item>
      <title>Re: Vector interrupt in MC68HC908GZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Vector-interrupt-in-MC68HC908GZ60/m-p/136875#M4503</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The interrupt vector numbers are just the word number counting down from FFFF. The reset vector is FFFE:FFFF and is 0 and so on. If you refer to the datasheet you can use the IF numbers in the table for the Interrupt status register and add one to these values.&lt;/P&gt;&lt;P&gt;Regards David&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 May 2006 17:47:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Vector-interrupt-in-MC68HC908GZ60/m-p/136875#M4503</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2006-05-24T17:47:52Z</dc:date>
    </item>
  </channel>
</rss>