<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Any sample code for S08QG8 to use SCI &amp; SPI port?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Any-sample-code-for-S08QG8-to-use-SCI-SPI-port/m-p/136412#M4329</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;&lt;FONT size="2"&gt;Hello TonyLin,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;The SPI code, and therefore the SCI-to-SPI bridge will be dependent on whether the SPI facility is a master or a slave.&amp;nbsp; If SCI receive traffic exceeds the transmit traffic, I would tend to&amp;nbsp;choose a SPI master.&amp;nbsp; If the SCI transmit traffic is greater, the SPI would operate as a slave.&amp;nbsp; It&amp;nbsp;will also depend on whether the other end of the SPI link is master or slave.&amp;nbsp; If the other end is existing equipment, you will also need to match the SPI parameters CPHA and CPOL.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;The slave SPI would generally be interrupt driven, whereas the master operation might be polled.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Regards,&lt;BR /&gt;Mac&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 May 2006 19:03:45 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2006-05-18T19:03:45Z</dc:date>
    <item>
      <title>Any sample code for S08QG8 to use SCI &amp; SPI port?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Any-sample-code-for-S08QG8-to-use-SCI-SPI-port/m-p/136408#M4325</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi, I would like to make S08QG8 working as an UART-SPI interface, so that I can communicate from PC to SPI devices. Is there any sample code for this application available?&lt;/DIV&gt;&lt;DIV&gt;Thanks a lot!&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 May 2006 10:14:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Any-sample-code-for-S08QG8-to-use-SCI-SPI-port/m-p/136408#M4325</guid>
      <dc:creator>TonyLin</dc:creator>
      <dc:date>2006-05-18T10:14:39Z</dc:date>
    </item>
    <item>
      <title>Re: Any sample code for S08QG8 to use SCI &amp; SPI port?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Any-sample-code-for-S08QG8-to-use-SCI-SPI-port/m-p/136409#M4326</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;have you read this ?&lt;/DIV&gt;&lt;DIV&gt;&lt;A href="http://www.freescale.com/files/microcontrollers/doc/user_guide/HCS08QRUG.pdf" rel="nofollow" target="_blank"&gt;http://www.freescale.com/files/microcontrollers/doc/user_guide/HCS08QRUG.pdf&lt;/A&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;you can download the code too at the product page.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Eckhard&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 May 2006 14:23:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Any-sample-code-for-S08QG8-to-use-SCI-SPI-port/m-p/136409#M4326</guid>
      <dc:creator>eckhard</dc:creator>
      <dc:date>2006-05-18T14:23:15Z</dc:date>
    </item>
    <item>
      <title>Re: Any sample code for S08QG8 to use SCI &amp; SPI port?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Any-sample-code-for-S08QG8-to-use-SCI-SPI-port/m-p/136410#M4327</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;ya, I have read it. However, it provides codes for SCI and SPI individually. What I need it is actually a bridge from SCI-to-SPI.&lt;/DIV&gt;&lt;DIV&gt;Thanks anyway.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 May 2006 14:55:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Any-sample-code-for-S08QG8-to-use-SCI-SPI-port/m-p/136410#M4327</guid>
      <dc:creator>TonyLin</dc:creator>
      <dc:date>2006-05-18T14:55:52Z</dc:date>
    </item>
    <item>
      <title>Re: Any sample code for S08QG8 to use SCI &amp; SPI port?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Any-sample-code-for-S08QG8-to-use-SCI-SPI-port/m-p/136411#M4328</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;In the document, I saw there was a sample project named SCI.mcp. But I can find it inside the HCS08QRUGSW.zip.&lt;/DIV&gt;&lt;DIV&gt;Do you have any idea where I can find it? Thanks!&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 May 2006 15:13:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Any-sample-code-for-S08QG8-to-use-SCI-SPI-port/m-p/136411#M4328</guid>
      <dc:creator>TonyLin</dc:creator>
      <dc:date>2006-05-18T15:13:11Z</dc:date>
    </item>
    <item>
      <title>Re: Any sample code for S08QG8 to use SCI &amp; SPI port?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Any-sample-code-for-S08QG8-to-use-SCI-SPI-port/m-p/136412#M4329</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;&lt;FONT size="2"&gt;Hello TonyLin,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;The SPI code, and therefore the SCI-to-SPI bridge will be dependent on whether the SPI facility is a master or a slave.&amp;nbsp; If SCI receive traffic exceeds the transmit traffic, I would tend to&amp;nbsp;choose a SPI master.&amp;nbsp; If the SCI transmit traffic is greater, the SPI would operate as a slave.&amp;nbsp; It&amp;nbsp;will also depend on whether the other end of the SPI link is master or slave.&amp;nbsp; If the other end is existing equipment, you will also need to match the SPI parameters CPHA and CPOL.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;The slave SPI would generally be interrupt driven, whereas the master operation might be polled.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Regards,&lt;BR /&gt;Mac&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 May 2006 19:03:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Any-sample-code-for-S08QG8-to-use-SCI-SPI-port/m-p/136412#M4329</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2006-05-18T19:03:45Z</dc:date>
    </item>
  </channel>
</rss>