<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックTimer Link for MSCAN on GZ16</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Timer-Link-for-MSCAN-on-GZ16/m-p/124799#M430</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Has anyone had any trouble with the Timer link for the MSCAN module on the GZ16.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am setting up Timer 2 Channel 0 as an input capture timer and setting the TLNKEN bit in CMCR0. I have checked that it is definatly set using debug later on in my code. The capture registers remain at 0 even though I am receiving valid CAN packets.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The Timer is still receiving its signal from the port pin instead of the MSCAN module. If I wiggle the port pin the timer will capture, but no captures take place on Reception of a CAN packet.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there sometihng I am missing?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I know the Timer is running and Capture mode is enabled but I cannot get it to capture on MSCAN reception instead of port pin rising edge.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Does anything else need to be done besides setting TLNKEN in CMCR0?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any advice would be greatly appreicated&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Paul&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Jul 2006 16:25:27 GMT</pubDate>
    <dc:creator>PaulPorter</dc:creator>
    <dc:date>2006-07-25T16:25:27Z</dc:date>
    <item>
      <title>Timer Link for MSCAN on GZ16</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Timer-Link-for-MSCAN-on-GZ16/m-p/124799#M430</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Has anyone had any trouble with the Timer link for the MSCAN module on the GZ16.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am setting up Timer 2 Channel 0 as an input capture timer and setting the TLNKEN bit in CMCR0. I have checked that it is definatly set using debug later on in my code. The capture registers remain at 0 even though I am receiving valid CAN packets.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The Timer is still receiving its signal from the port pin instead of the MSCAN module. If I wiggle the port pin the timer will capture, but no captures take place on Reception of a CAN packet.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there sometihng I am missing?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I know the Timer is running and Capture mode is enabled but I cannot get it to capture on MSCAN reception instead of port pin rising edge.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Does anything else need to be done besides setting TLNKEN in CMCR0?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any advice would be greatly appreicated&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Paul&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Jul 2006 16:25:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Timer-Link-for-MSCAN-on-GZ16/m-p/124799#M430</guid>
      <dc:creator>PaulPorter</dc:creator>
      <dc:date>2006-07-25T16:25:27Z</dc:date>
    </item>
    <item>
      <title>Re: Timer Link for MSCAN on GZ16</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Timer-Link-for-MSCAN-on-GZ16/m-p/124800#M431</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Paul -&lt;/P&gt;&lt;P&gt;I know that this is a late response, but a colleague just saw this post and recognized the problem.&lt;/P&gt;&lt;P&gt;There is a mistake in the documentation. The Timer Link is actually associated with Timer 1, Channel 0.&lt;/P&gt;&lt;P&gt;- Rocky&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Aug 2006 02:36:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Timer-Link-for-MSCAN-on-GZ16/m-p/124800#M431</guid>
      <dc:creator>RockyRoad</dc:creator>
      <dc:date>2006-08-16T02:36:57Z</dc:date>
    </item>
  </channel>
</rss>