<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SO8QG8 3.3volt interface to 5v logic  (eg LCD)  ? in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SO8QG8-3-3volt-interface-to-5v-logic-eg-LCD/m-p/136056#M4204</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Many thanks, Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Glenn&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 Nov 2006 12:10:46 GMT</pubDate>
    <dc:creator>glennp</dc:creator>
    <dc:date>2006-11-10T12:10:46Z</dc:date>
    <item>
      <title>SO8QG8 3.3volt interface to 5v logic  (eg LCD)  ?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SO8QG8-3-3volt-interface-to-5v-logic-eg-LCD/m-p/136054#M4202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi&lt;/DIV&gt;&lt;DIV&gt;I have never used 3.3v&amp;nbsp;uP chips before and was wondering what is the preffered method of interfacing the 3.3v SO8QG8 parts to an LCD module for example that runs on 5v supply.?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;At this stage I would like to connect my DEMO QG8 board to an LCD.&amp;nbsp; Software is not a problem, just the physical interface.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Glenn&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Nov 2006 07:35:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/SO8QG8-3-3volt-interface-to-5v-logic-eg-LCD/m-p/136054#M4202</guid>
      <dc:creator>glennp</dc:creator>
      <dc:date>2006-11-10T07:35:19Z</dc:date>
    </item>
    <item>
      <title>Re: SO8QG8 3.3volt interface to 5v logic  (eg LCD)  ?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SO8QG8-3-3volt-interface-to-5v-logic-eg-LCD/m-p/136055#M4203</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello Glenn,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;For a 5 volt LCD module, you might consider using a buffer from the 74HCT logic family, (and power this from the same supply as the LCD).&amp;nbsp; The inputs to these devices are TTL compatible, and should work with a 3.3 volt logic swing.&amp;nbsp; If you need to convert any 5 volt output levels down to 3.3 volts, simply use a resistive&amp;nbsp;voltage divider.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Nov 2006 11:07:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/SO8QG8-3-3volt-interface-to-5v-logic-eg-LCD/m-p/136055#M4203</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2006-11-10T11:07:22Z</dc:date>
    </item>
    <item>
      <title>Re: SO8QG8 3.3volt interface to 5v logic  (eg LCD)  ?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SO8QG8-3-3volt-interface-to-5v-logic-eg-LCD/m-p/136056#M4204</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Many thanks, Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Glenn&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Nov 2006 12:10:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/SO8QG8-3-3volt-interface-to-5v-logic-eg-LCD/m-p/136056#M4204</guid>
      <dc:creator>glennp</dc:creator>
      <dc:date>2006-11-10T12:10:46Z</dc:date>
    </item>
    <item>
      <title>Re: SO8QG8 3.3volt interface to 5v logic  (eg LCD)  ?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SO8QG8-3-3volt-interface-to-5v-logic-eg-LCD/m-p/136057#M4205</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;The eval board we bought uses a 74HCT244 as the level booster. Our in-house design, which works just fine, omits it. Our LCD (a 5V part) is configured as WRITE-ONLY, and driven directly from PORTA of a GT16A. Keeps on ticking, a 3.3 swing is fine with **most** TTL. However my lawyer says I should say: the LCD manufacturer's specs always rule.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Nov 2006 22:58:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/SO8QG8-3-3volt-interface-to-5v-logic-eg-LCD/m-p/136057#M4205</guid>
      <dc:creator>Geezer</dc:creator>
      <dc:date>2006-11-10T22:58:45Z</dc:date>
    </item>
    <item>
      <title>Re: SO8QG8 3.3volt interface to 5v logic  (eg LCD)  ?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SO8QG8-3-3volt-interface-to-5v-logic-eg-LCD/m-p/136058#M4206</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I have used the 9S08QG8 connected directly to 5V LCD module (write only mode). The LCD modules I use have the spec of VinH 2.2Vmin,&amp;nbsp;&amp;nbsp; VinL 0.6Vmax . It works just great for me.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Nov 2006 08:00:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/SO8QG8-3-3volt-interface-to-5v-logic-eg-LCD/m-p/136058#M4206</guid>
      <dc:creator>paul</dc:creator>
      <dc:date>2006-11-11T08:00:22Z</dc:date>
    </item>
    <item>
      <title>Re: SO8QG8 3.3volt interface to 5v logic  (eg LCD)  ?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SO8QG8-3-3volt-interface-to-5v-logic-eg-LCD/m-p/136059#M4207</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello Glenn,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;I stand corrected.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;As others have pointed out, the HD44780 device (and similar clones), used&amp;nbsp;within the alphanumeric LCD&amp;nbsp;modules, have TTL input logic thresholds.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Nov 2006 10:49:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/SO8QG8-3-3volt-interface-to-5v-logic-eg-LCD/m-p/136059#M4207</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2006-11-11T10:49:06Z</dc:date>
    </item>
    <item>
      <title>Re: SO8QG8 3.3volt interface to 5v logic  (eg LCD)  ?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SO8QG8-3-3volt-interface-to-5v-logic-eg-LCD/m-p/136060#M4208</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;ADI (Analog Devices) makes a cool bi-directional level translator that does not need direction control signals.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The ADG3308 can handle any voltages between 1.2V and 5.5V.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Two notes of caution:&lt;/DIV&gt;&lt;DIV&gt;1) note that the Y side voltage must always be equal or greater than the A side.&lt;/DIV&gt;&lt;DIV&gt;2) if any of the lines are shared by other pins (like a bus), care needs to be taken to avoid bus contention since all lines are always connected.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;BadDad&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Nov 2006 22:08:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/SO8QG8-3-3volt-interface-to-5v-logic-eg-LCD/m-p/136060#M4208</guid>
      <dc:creator>baddad</dc:creator>
      <dc:date>2006-11-16T22:08:19Z</dc:date>
    </item>
  </channel>
</rss>