<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC13213 single-port, internal T/R switch - does it work? in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13213-single-port-internal-T-R-switch-does-it-work/m-p/135921#M4158</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi snickels,&lt;BR /&gt;I have implemented a custom board using a single port configuration and it's work.&lt;BR /&gt;The only change I have made is to set CT_Bias_en bit and RF_Switch_Mode bit for enable single port operation.&lt;BR /&gt;If you are using MAC codebase you must change these bits in MC1319xHandler.c file.&lt;BR /&gt;&lt;BR /&gt;Sorry for my english&lt;SPAN&gt;&lt;IMG alt=":smileytongue:" class="emoticon emoticon-smileytongue" id="smileytongue" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-tongue.gif" title="Smiley Tongue" /&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Spell&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 Jun 2007 20:07:12 GMT</pubDate>
    <dc:creator>Spell</dc:creator>
    <dc:date>2007-06-07T20:07:12Z</dc:date>
    <item>
      <title>MC13213 single-port, internal T/R switch - does it work?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13213-single-port-internal-T-R-switch-does-it-work/m-p/135920#M4157</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;DIV&gt;Anyone successfully implement the single-port, internal T/R switch for the MC13213 as described in AN3248?&amp;nbsp; I saw a related post "BeeKit User Defined Target Question", but the discussion seemed to wander.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;My code, based on the WirelessUart example (in BeeKit), works on the MC13213SRB, but it won't run on my custom board - uses the single-port RF with internal&amp;nbsp;T/R switch&amp;nbsp;design.&amp;nbsp; I have modified the MC21XSRB.c file (per AN3248)&amp;nbsp;so that register 0x07 is loaded with 0x5C00 instead.&amp;nbsp; This should be the only change.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I don't have a spectrum analyzer to test if RF is being emitted.&amp;nbsp;&amp;nbsp;My circuit isn't exactly as described in the app. note.&amp;nbsp; It&amp;nbsp;has a single 6.8nH inductor across the RF lines to the left of the balun, and then an 8.2nH inductor on the right side.&amp;nbsp; I've attached the schematic.&amp;nbsp; It's based on some other reference design (someone else created board for me).&amp;nbsp; The actual part on the board is "PC13213", so perhaps this pre-production part had an issue?&amp;nbsp; I have looked at the CT_BIAS pin using a scope&amp;nbsp;and it is correctly goes to VDDA during transmit.&amp;nbsp; I see some pulses on the RFIN_P and RFIN_M pins at the time of the transmit.&amp;nbsp; For kicks I placed the scope on the othe side of the balun, but didn't see anything.&amp;nbsp; There's no mention of RF problems in the errata.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;All of Freescale's development boards for the MC1321X&amp;nbsp;use differential output, so I would like a little proof that it works&amp;nbsp;on&amp;nbsp;real hardware.&amp;nbsp;&amp;nbsp;My next step is to hotwire it to exactly match AN3248.&amp;nbsp; That'll involve some microscope work so it'd be good to hear "it worked for me" before I go through the effort.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jun 2007 03:26:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13213-single-port-internal-T-R-switch-does-it-work/m-p/135920#M4157</guid>
      <dc:creator>snickels</dc:creator>
      <dc:date>2007-06-06T03:26:04Z</dc:date>
    </item>
    <item>
      <title>Re: MC13213 single-port, internal T/R switch - does it work?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13213-single-port-internal-T-R-switch-does-it-work/m-p/135921#M4158</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi snickels,&lt;BR /&gt;I have implemented a custom board using a single port configuration and it's work.&lt;BR /&gt;The only change I have made is to set CT_Bias_en bit and RF_Switch_Mode bit for enable single port operation.&lt;BR /&gt;If you are using MAC codebase you must change these bits in MC1319xHandler.c file.&lt;BR /&gt;&lt;BR /&gt;Sorry for my english&lt;SPAN&gt;&lt;IMG alt=":smileytongue:" class="emoticon emoticon-smileytongue" id="smileytongue" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-tongue.gif" title="Smiley Tongue" /&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Spell&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jun 2007 20:07:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13213-single-port-internal-T-R-switch-does-it-work/m-p/135921#M4158</guid>
      <dc:creator>Spell</dc:creator>
      <dc:date>2007-06-07T20:07:12Z</dc:date>
    </item>
    <item>
      <title>Re: MC13213 single-port, internal T/R switch - does it work?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13213-single-port-internal-T-R-switch-does-it-work/m-p/135922#M4159</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi,&lt;BR /&gt;I cannot proof you if your design will work. But I know that only change You have to do in the source code when using SMAC is in the RadioInit() function where You have to rewrite: SPIDrvWrite(0x07,0x4C00) to SPIDrvWrite(0x07,0x5C00). And as target board I chose MC1321XNCB.&lt;BR /&gt;&lt;BR /&gt;I am currently working with PAN4555 which uses singleport design. And it works perfectly.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jun 2007 19:24:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13213-single-port-internal-T-R-switch-does-it-work/m-p/135922#M4159</guid>
      <dc:creator>honzin</dc:creator>
      <dc:date>2007-06-11T19:24:03Z</dc:date>
    </item>
    <item>
      <title>Re: MC13213 single-port, internal T/R switch - does it work?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13213-single-port-internal-T-R-switch-does-it-work/m-p/135923#M4160</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Sounds like it might be easier to pick up the PAN4555.&amp;nbsp; In small qty, it is less than $20 at Digi-Key.&amp;nbsp; Then you don't need to worry about the spectrum analyzer and such.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Also, I heard that Panasonic is going to come out with a PAN4555ETU version of this module real soon.&amp;nbsp; This is the PAN4555 on a daughter board, so it is supposed to be easy to implement in the design process.&amp;nbsp; I'll take a look at it when it becomes available though.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Aug 2007 11:59:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13213-single-port-internal-T-R-switch-does-it-work/m-p/135923#M4160</guid>
      <dc:creator>Icono</dc:creator>
      <dc:date>2007-08-01T11:59:08Z</dc:date>
    </item>
  </channel>
</rss>