<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: help: low power microcontroller chosen in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/help-low-power-microcontroller-chosen/m-p/124687#M409</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;If you want to use a Freescale 8-bitter then you will need to use an external RTC say from Maxim/Dallas. Could interface using SPI or I2C.&lt;/P&gt;&lt;P&gt;Some application specific ones that are fairly big have an RTC but none of the general purpose ones do.&lt;/P&gt;&lt;P&gt;A QG8 might fit the bill, but only 16 pin (See under HCS08 menu, top left).&lt;/P&gt;&lt;P&gt;Regards David&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 23 Jul 2006 05:55:39 GMT</pubDate>
    <dc:creator>peg</dc:creator>
    <dc:date>2006-07-23T05:55:39Z</dc:date>
    <item>
      <title>help: low power microcontroller chosen</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/help-low-power-microcontroller-chosen/m-p/124686#M408</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;could you advise me about a 8 bit low power consumption microcontroller.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;These are the other characteristics:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;2 kB/4kB flash&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;real time clock&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;20 pin o similar...&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jul 2006 15:27:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/help-low-power-microcontroller-chosen/m-p/124686#M408</guid>
      <dc:creator>gzeds</dc:creator>
      <dc:date>2006-07-21T15:27:32Z</dc:date>
    </item>
    <item>
      <title>Re: help: low power microcontroller chosen</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/help-low-power-microcontroller-chosen/m-p/124687#M409</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;If you want to use a Freescale 8-bitter then you will need to use an external RTC say from Maxim/Dallas. Could interface using SPI or I2C.&lt;/P&gt;&lt;P&gt;Some application specific ones that are fairly big have an RTC but none of the general purpose ones do.&lt;/P&gt;&lt;P&gt;A QG8 might fit the bill, but only 16 pin (See under HCS08 menu, top left).&lt;/P&gt;&lt;P&gt;Regards David&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 23 Jul 2006 05:55:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/help-low-power-microcontroller-chosen/m-p/124687#M409</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2006-07-23T05:55:39Z</dc:date>
    </item>
  </channel>
</rss>