<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: Mc13213 write/read eeprom</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Mc13213-write-read-eeprom/m-p/135450#M4019</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;program eeprom haha.&lt;BR /&gt;there are a few tips, when i did a search most of what came up was busted junk code. when i re invented the wheel i submitted some more busted junk code. you can look for it. the how to for flash read/write should be in a seperate section as reference material or in the product spec itself but is not and causes countless confusion, a bad for freescale. my usage of _assy code is cleaner that what i have seen but i can only verify it works for me, good luck.&lt;BR /&gt;&lt;BR /&gt;few tips:&lt;BR /&gt;-the routine that writes to eeprom needs to be in ram. people usally write in in assy but it dosnt have to be. now think about this, if the processor state machine is handling the flash write the internal bus structure is tied up and cant access flash program memory to support flash emulation. put the emulation code in ram.&lt;BR /&gt;-my processor is a mc9s08rd32dwe, and it could would be different on alot of processors, what is your processor? i dont even know if mine is close to yours&lt;BR /&gt;-the process to write even one byte to flash is:&lt;BR /&gt;0)you will need to set the flash timing in relation to the processor clock, do this up front in initiliaztion.&lt;BR /&gt;1)determine the 512 page where the byte is located in flsh and write the whole thingy to ram&lt;BR /&gt;2)modify the page in ram&lt;BR /&gt;3)erase that page in flash&lt;BR /&gt;4)wrtie from ram to flash the modifyed data&lt;BR /&gt;5)you might want to verify at this point flash = ram for that page&lt;BR /&gt;6)before while writting flash you might want to look for low battery&lt;BR /&gt;7)disable irq while writting&lt;BR /&gt;8)general note, the assy program has details that freescale outlined in the manual about cking for errors and things&lt;BR /&gt;&lt;BR /&gt;//sample code:&lt;BR /&gt;//excerpt form initilization&lt;BR /&gt;// ** Flash Init&lt;BR /&gt;if(FSTAT &amp;amp; 0x10) FSTAT &amp;amp;= 0x10; //reset flash error if any, then set flash clock devider&lt;BR /&gt;FCDIV = 0x27; //for 8mhz per freescale datasheet p50 table 4-6&lt;BR /&gt;&lt;BR /&gt;//excerpt form varriables.c&lt;BR /&gt;//code example flash memory page erase &amp;amp; byte write&lt;BR /&gt;// FlashRamRoutine.Adr = 0xE001;&lt;BR /&gt;// FlashRamRoutine.Data = 0xFF;&lt;BR /&gt;// FlashRamRoutine.Command = 0x40;&lt;BR /&gt;// _asm jsr FlashRamRoutine.Start;&lt;BR /&gt;// FlashRamRoutine.Adr = 0xE000;//byte write&lt;BR /&gt;// FlashRamRoutine.Data = 0xBB;&lt;BR /&gt;// FlashRamRoutine.Command = 0x20;&lt;BR /&gt;// _asm jsr FlashRamRoutine.Start;&lt;BR /&gt;#pragma DATA_SEG _RAMROUTINE&lt;BR /&gt;struct flashramroutine FlashRamRoutine = {&lt;BR /&gt;{0xc6,0x18,0x25,0xa5,0x10,0x27,0x07,0x45,//start instruction bytes&lt;BR /&gt;0x18,0x25,0xf6,0xaa,0x10,0xf7,0x32,&lt;BR /&gt;0x08,0x43, //address of unsigned int address&lt;BR /&gt;0xc6, //instruction byte&lt;BR /&gt;0x08,0x45, //address of unsigned char data&lt;BR /&gt;0xf7,0xa6}, //instruction bytes&lt;BR /&gt;{0x00}, //unsigned char command&lt;BR /&gt;{0x45,0x18,0x25,0xe7,0x01,0xf6,0xaa,0x80,//final instruction bytes&lt;BR /&gt;0xf7,0x9d,0x9d,0x9d,0x9d,0xc6,0x18,0x25,&lt;BR /&gt;0xc6,0x18,0x25,0xa5,0x40,0x27,0xf9,0x81},&lt;BR /&gt;0,0};//value of uint address, uchar data&lt;BR /&gt;#pragma DATA_SEG DEFAULT&lt;BR /&gt;&lt;BR /&gt;//excerpt form varriables.h&lt;BR /&gt;#pragma DATA_SEG _RAMROUTINE&lt;BR /&gt;extern struct flashramroutine {&lt;BR /&gt;const unsigned char Start[22];&lt;BR /&gt;unsigned char Command;&lt;BR /&gt;const unsigned char End[24];&lt;BR /&gt;unsigned int Adr;&lt;BR /&gt;unsigned char Data;&lt;BR /&gt;} FlashRamRoutine;&lt;BR /&gt;#pragma DATA_SEG DEFAULT&lt;BR /&gt;&lt;BR /&gt;//in my *.prn linker command file&lt;BR /&gt;SEGMENTS&lt;BR /&gt;RAMROUTINE= READ_WRITE 0x0814 TO 0x0845;&lt;BR /&gt;END&lt;BR /&gt;PLACEMENT&lt;BR /&gt;_RAMROUTINE INTO RAMROUTINE;&lt;BR /&gt;END&lt;BR /&gt;&lt;BR /&gt;//usage&lt;BR /&gt;//copy whole flash page to ram&lt;BR /&gt;for(i=0x1FF; i+1; i-- ) PatchRAM[i] = *((unsigned char*)((patch.adr &amp;amp; 0xFE00) + i));&lt;BR /&gt;&lt;BR /&gt;//after doing this code modifies copied ram version with new data and re-writes back&lt;BR /&gt;&lt;BR /&gt;//copy modified ram page to flash&lt;BR /&gt;FlashRamRoutine.Adr = patch.adr-1; //erase whole flash page&lt;BR /&gt;FlashRamRoutine.Command = 0x40;&lt;BR /&gt;_asm jsr FlashRamRoutine.Start;&lt;BR /&gt;FlashRamRoutine.Command = 0x20; //write whole page to flash from ram&lt;BR /&gt;for(i=0; i0x200; i++){&lt;BR /&gt;FlashRamRoutine.Adr = (FlashRamRoutine.Adr &amp;amp; 0xFE00) + i;&lt;BR /&gt;FlashRamRoutine.Data = PatchRAM[i];&lt;BR /&gt;_asm jsr FlashRamRoutine.Start; }&lt;P&gt;Message Edited by jah on &lt;SPAN class="date_text"&gt;2006-11-06&lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;10:23 AM&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Message Edited by jah on &lt;SPAN class="date_text"&gt;2006-11-06&lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;10:27 AM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Nov 2006 00:18:40 GMT</pubDate>
    <dc:creator>jah</dc:creator>
    <dc:date>2006-11-07T00:18:40Z</dc:date>
    <item>
      <title>Mc13213 write/read eeprom</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Mc13213-write-read-eeprom/m-p/135449#M4018</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;i have some problem for programming eeprom in my mc13213.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;i have a 13213SDK board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;the question is: exist any exsample for this board??&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thank you&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;max&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Nov 2006 19:35:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Mc13213-write-read-eeprom/m-p/135449#M4018</guid>
      <dc:creator>kimegliodime</dc:creator>
      <dc:date>2006-11-06T19:35:42Z</dc:date>
    </item>
    <item>
      <title>Re: Mc13213 write/read eeprom</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Mc13213-write-read-eeprom/m-p/135450#M4019</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;program eeprom haha.&lt;BR /&gt;there are a few tips, when i did a search most of what came up was busted junk code. when i re invented the wheel i submitted some more busted junk code. you can look for it. the how to for flash read/write should be in a seperate section as reference material or in the product spec itself but is not and causes countless confusion, a bad for freescale. my usage of _assy code is cleaner that what i have seen but i can only verify it works for me, good luck.&lt;BR /&gt;&lt;BR /&gt;few tips:&lt;BR /&gt;-the routine that writes to eeprom needs to be in ram. people usally write in in assy but it dosnt have to be. now think about this, if the processor state machine is handling the flash write the internal bus structure is tied up and cant access flash program memory to support flash emulation. put the emulation code in ram.&lt;BR /&gt;-my processor is a mc9s08rd32dwe, and it could would be different on alot of processors, what is your processor? i dont even know if mine is close to yours&lt;BR /&gt;-the process to write even one byte to flash is:&lt;BR /&gt;0)you will need to set the flash timing in relation to the processor clock, do this up front in initiliaztion.&lt;BR /&gt;1)determine the 512 page where the byte is located in flsh and write the whole thingy to ram&lt;BR /&gt;2)modify the page in ram&lt;BR /&gt;3)erase that page in flash&lt;BR /&gt;4)wrtie from ram to flash the modifyed data&lt;BR /&gt;5)you might want to verify at this point flash = ram for that page&lt;BR /&gt;6)before while writting flash you might want to look for low battery&lt;BR /&gt;7)disable irq while writting&lt;BR /&gt;8)general note, the assy program has details that freescale outlined in the manual about cking for errors and things&lt;BR /&gt;&lt;BR /&gt;//sample code:&lt;BR /&gt;//excerpt form initilization&lt;BR /&gt;// ** Flash Init&lt;BR /&gt;if(FSTAT &amp;amp; 0x10) FSTAT &amp;amp;= 0x10; //reset flash error if any, then set flash clock devider&lt;BR /&gt;FCDIV = 0x27; //for 8mhz per freescale datasheet p50 table 4-6&lt;BR /&gt;&lt;BR /&gt;//excerpt form varriables.c&lt;BR /&gt;//code example flash memory page erase &amp;amp; byte write&lt;BR /&gt;// FlashRamRoutine.Adr = 0xE001;&lt;BR /&gt;// FlashRamRoutine.Data = 0xFF;&lt;BR /&gt;// FlashRamRoutine.Command = 0x40;&lt;BR /&gt;// _asm jsr FlashRamRoutine.Start;&lt;BR /&gt;// FlashRamRoutine.Adr = 0xE000;//byte write&lt;BR /&gt;// FlashRamRoutine.Data = 0xBB;&lt;BR /&gt;// FlashRamRoutine.Command = 0x20;&lt;BR /&gt;// _asm jsr FlashRamRoutine.Start;&lt;BR /&gt;#pragma DATA_SEG _RAMROUTINE&lt;BR /&gt;struct flashramroutine FlashRamRoutine = {&lt;BR /&gt;{0xc6,0x18,0x25,0xa5,0x10,0x27,0x07,0x45,//start instruction bytes&lt;BR /&gt;0x18,0x25,0xf6,0xaa,0x10,0xf7,0x32,&lt;BR /&gt;0x08,0x43, //address of unsigned int address&lt;BR /&gt;0xc6, //instruction byte&lt;BR /&gt;0x08,0x45, //address of unsigned char data&lt;BR /&gt;0xf7,0xa6}, //instruction bytes&lt;BR /&gt;{0x00}, //unsigned char command&lt;BR /&gt;{0x45,0x18,0x25,0xe7,0x01,0xf6,0xaa,0x80,//final instruction bytes&lt;BR /&gt;0xf7,0x9d,0x9d,0x9d,0x9d,0xc6,0x18,0x25,&lt;BR /&gt;0xc6,0x18,0x25,0xa5,0x40,0x27,0xf9,0x81},&lt;BR /&gt;0,0};//value of uint address, uchar data&lt;BR /&gt;#pragma DATA_SEG DEFAULT&lt;BR /&gt;&lt;BR /&gt;//excerpt form varriables.h&lt;BR /&gt;#pragma DATA_SEG _RAMROUTINE&lt;BR /&gt;extern struct flashramroutine {&lt;BR /&gt;const unsigned char Start[22];&lt;BR /&gt;unsigned char Command;&lt;BR /&gt;const unsigned char End[24];&lt;BR /&gt;unsigned int Adr;&lt;BR /&gt;unsigned char Data;&lt;BR /&gt;} FlashRamRoutine;&lt;BR /&gt;#pragma DATA_SEG DEFAULT&lt;BR /&gt;&lt;BR /&gt;//in my *.prn linker command file&lt;BR /&gt;SEGMENTS&lt;BR /&gt;RAMROUTINE= READ_WRITE 0x0814 TO 0x0845;&lt;BR /&gt;END&lt;BR /&gt;PLACEMENT&lt;BR /&gt;_RAMROUTINE INTO RAMROUTINE;&lt;BR /&gt;END&lt;BR /&gt;&lt;BR /&gt;//usage&lt;BR /&gt;//copy whole flash page to ram&lt;BR /&gt;for(i=0x1FF; i+1; i-- ) PatchRAM[i] = *((unsigned char*)((patch.adr &amp;amp; 0xFE00) + i));&lt;BR /&gt;&lt;BR /&gt;//after doing this code modifies copied ram version with new data and re-writes back&lt;BR /&gt;&lt;BR /&gt;//copy modified ram page to flash&lt;BR /&gt;FlashRamRoutine.Adr = patch.adr-1; //erase whole flash page&lt;BR /&gt;FlashRamRoutine.Command = 0x40;&lt;BR /&gt;_asm jsr FlashRamRoutine.Start;&lt;BR /&gt;FlashRamRoutine.Command = 0x20; //write whole page to flash from ram&lt;BR /&gt;for(i=0; i0x200; i++){&lt;BR /&gt;FlashRamRoutine.Adr = (FlashRamRoutine.Adr &amp;amp; 0xFE00) + i;&lt;BR /&gt;FlashRamRoutine.Data = PatchRAM[i];&lt;BR /&gt;_asm jsr FlashRamRoutine.Start; }&lt;P&gt;Message Edited by jah on &lt;SPAN class="date_text"&gt;2006-11-06&lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;10:23 AM&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Message Edited by jah on &lt;SPAN class="date_text"&gt;2006-11-06&lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;10:27 AM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Nov 2006 00:18:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Mc13213-write-read-eeprom/m-p/135450#M4019</guid>
      <dc:creator>jah</dc:creator>
      <dc:date>2006-11-07T00:18:40Z</dc:date>
    </item>
  </channel>
</rss>