<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックProblem with HCS08AW60 in 3.3v system</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-with-HCS08AW60-in-3-3v-system/m-p/134968#M3899</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am operating an AW60 in a 3.3v system.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;By default on power-on reset the LVD system in enabled to reset the uP when the voltage drops below the lower LVD threshold (2.56v). On two occasions I have found that the system is being held in reset because the threshold has been changed to the upper level(4.4v) relevant for a 5v system. I have proved this by increasing the supply voltage to around 5v and the system starts, lower it back to 3.3 and the uP is held in reset without performing a POR.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have not actively changed the LVWV bit in SPMSC2 to a "1". The bit changing to a "1" in a 3.3v system is fatal!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My I don't think my code is crashing and it is highly unlikely to be setting this bit, or is there a problem with the part itself.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I would prefer that the threshold selection bit was set in flash at programming time!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I look forward to your comments.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Phil Green&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 31 Oct 2006 18:09:06 GMT</pubDate>
    <dc:creator>PhilG</dc:creator>
    <dc:date>2006-10-31T18:09:06Z</dc:date>
    <item>
      <title>Problem with HCS08AW60 in 3.3v system</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-with-HCS08AW60-in-3-3v-system/m-p/134968#M3899</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am operating an AW60 in a 3.3v system.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;By default on power-on reset the LVD system in enabled to reset the uP when the voltage drops below the lower LVD threshold (2.56v). On two occasions I have found that the system is being held in reset because the threshold has been changed to the upper level(4.4v) relevant for a 5v system. I have proved this by increasing the supply voltage to around 5v and the system starts, lower it back to 3.3 and the uP is held in reset without performing a POR.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have not actively changed the LVWV bit in SPMSC2 to a "1". The bit changing to a "1" in a 3.3v system is fatal!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My I don't think my code is crashing and it is highly unlikely to be setting this bit, or is there a problem with the part itself.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I would prefer that the threshold selection bit was set in flash at programming time!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I look forward to your comments.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Phil Green&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Oct 2006 18:09:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-with-HCS08AW60-in-3-3v-system/m-p/134968#M3899</guid>
      <dc:creator>PhilG</dc:creator>
      <dc:date>2006-10-31T18:09:06Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with HCS08AW60 in 3.3v system</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-with-HCS08AW60-in-3-3v-system/m-p/134969#M3900</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;reference: mc9s08rd32dwe&lt;BR /&gt;&lt;BR /&gt;on the above processor we may be experiencing some die mis-functions in voltage detection. i have not looked into this other than deleting the lo voltage detection except during flash a flash write.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Nov 2006 00:36:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-with-HCS08AW60-in-3-3v-system/m-p/134969#M3900</guid>
      <dc:creator>jah</dc:creator>
      <dc:date>2006-11-07T00:36:50Z</dc:date>
    </item>
  </channel>
</rss>