<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: [WDCKIT]WirelessUART with 230400 baud? in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/WDCKIT-WirelessUART-with-230400-baud/m-p/134704#M3792</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Eso,&lt;BR /&gt;I spent more time to develop the project wireless uart.&lt;BR /&gt;I started from Wireless Uart from BeeKit, then I removed ACK code for the packet, I make a circular buffer for SCI.&lt;BR /&gt;If you need help I'm glad to answer you.&lt;BR /&gt;&lt;BR /&gt;Stevasway&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Nov 2006 17:47:57 GMT</pubDate>
    <dc:creator>stevasway</dc:creator>
    <dc:date>2006-11-02T17:47:57Z</dc:date>
    <item>
      <title>[WDCKIT]WirelessUART with 230400 baud?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/WDCKIT-WirelessUART-with-230400-baud/m-p/134701#M3789</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello @ all,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I´m using the WDCKIT(13192-SARD -- MC9S08GT60). First of all, I would say, that i never used CodeWarrior and Freescale products. So I´m completely new here.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I need a wireless UART Cable replacement for a student project. The "Test-Tool" installation includes a demo-programm called "Wireless-Uart-Cable-Replacement" witch allows simple data transfer. It has a preset datarate of 19.200 baud. Is there any way to set it up to 230.400? Can i get a source file of "EVK_Wireless_UART_w_Embedded_Bootloader_V202_13192_SARD_EVB.s19"?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks and regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Eso&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Oct 2006 23:37:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/WDCKIT-WirelessUART-with-230400-baud/m-p/134701#M3789</guid>
      <dc:creator>Eso</dc:creator>
      <dc:date>2006-10-30T23:37:57Z</dc:date>
    </item>
    <item>
      <title>Re: [WDCKIT]WirelessUART with 230400 baud?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/WDCKIT-WirelessUART-with-230400-baud/m-p/134702#M3790</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Eso,&lt;BR /&gt;I tried the WirelessUart Project Demo, but sincerely is far from a cable replacement. If you try to download a file by Hyperterm you see how good is that project.&lt;BR /&gt;Terrible!&lt;BR /&gt;&lt;BR /&gt;So, I had to realize a new prj that runs correctly.&lt;BR /&gt;&lt;BR /&gt;Good Luck&lt;BR /&gt;Stevasway&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Oct 2006 01:01:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/WDCKIT-WirelessUART-with-230400-baud/m-p/134702#M3790</guid>
      <dc:creator>stevasway</dc:creator>
      <dc:date>2006-10-31T01:01:24Z</dc:date>
    </item>
    <item>
      <title>Re: [WDCKIT]WirelessUART with 230400 baud?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/WDCKIT-WirelessUART-with-230400-baud/m-p/134703#M3791</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi stevasway,&lt;BR /&gt;&lt;BR /&gt;thanks for your fast answer. Can you maybe send me your project. It would be a great help 4 me. My email is Esos.musik@gmx.at.&lt;BR /&gt;&lt;BR /&gt;regards&lt;BR /&gt;Eso&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Oct 2006 23:02:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/WDCKIT-WirelessUART-with-230400-baud/m-p/134703#M3791</guid>
      <dc:creator>Eso</dc:creator>
      <dc:date>2006-10-31T23:02:31Z</dc:date>
    </item>
    <item>
      <title>Re: [WDCKIT]WirelessUART with 230400 baud?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/WDCKIT-WirelessUART-with-230400-baud/m-p/134704#M3792</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Eso,&lt;BR /&gt;I spent more time to develop the project wireless uart.&lt;BR /&gt;I started from Wireless Uart from BeeKit, then I removed ACK code for the packet, I make a circular buffer for SCI.&lt;BR /&gt;If you need help I'm glad to answer you.&lt;BR /&gt;&lt;BR /&gt;Stevasway&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Nov 2006 17:47:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/WDCKIT-WirelessUART-with-230400-baud/m-p/134704#M3792</guid>
      <dc:creator>stevasway</dc:creator>
      <dc:date>2006-11-02T17:47:57Z</dc:date>
    </item>
    <item>
      <title>Re: [WDCKIT]WirelessUART with 230400 baud?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/WDCKIT-WirelessUART-with-230400-baud/m-p/134705#M3793</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;hi Stevasway,&lt;BR /&gt;&lt;BR /&gt;where can i get the source file? I have only the compiled file. Before im going to start with that, i have to know if its possible to run that system with 230400 baud. If someone knows that, plz answer.&lt;BR /&gt;&lt;BR /&gt;thx&lt;BR /&gt;&lt;BR /&gt;Eso&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Nov 2006 16:26:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/WDCKIT-WirelessUART-with-230400-baud/m-p/134705#M3793</guid>
      <dc:creator>Eso</dc:creator>
      <dc:date>2006-11-06T16:26:59Z</dc:date>
    </item>
    <item>
      <title>Re: [WDCKIT]WirelessUART with 230400 baud?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/WDCKIT-WirelessUART-with-230400-baud/m-p/134706#M3794</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Ok You have to download the BeeKit&lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://www.freescale.com/webapp/Download?colCode=BEEKITDOWNLOADPACKAGE.ZIP&amp;amp;prodCode=BEEKIT_WIRELESS_CONNECTIVITY_TOOLKIT&amp;amp;nodeId=012795pnQYXdNP9930&amp;amp;location=psp" target="test_blank"&gt;https://www.freescale.com/webapp/Download?colCode=BEEKITDOWNLOADPACKAGE.ZIP&amp;amp;prodCode=BEEKIT_WIRELESS_CONNECTIVITY_TOOLKIT&amp;amp;nodeId=012795pnQYXdNP9930&amp;amp;location=psp&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;then you'll see a project named WirelessUART.&lt;BR /&gt;&lt;BR /&gt;I guess it's possible to go to 230400 baud, depens on IGC settings.&lt;BR /&gt;&lt;BR /&gt;Bye&lt;BR /&gt;Stevasway&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Nov 2006 17:01:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/WDCKIT-WirelessUART-with-230400-baud/m-p/134706#M3794</guid>
      <dc:creator>stevasway</dc:creator>
      <dc:date>2006-11-06T17:01:34Z</dc:date>
    </item>
    <item>
      <title>Re: [WDCKIT]WirelessUART with 230400 baud?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/WDCKIT-WirelessUART-with-230400-baud/m-p/134707#M3795</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;thx,&lt;BR /&gt;&lt;BR /&gt;if have any question i will ask you. &lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Nov 2006 19:01:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/WDCKIT-WirelessUART-with-230400-baud/m-p/134707#M3795</guid>
      <dc:creator>Eso</dc:creator>
      <dc:date>2006-11-06T19:01:23Z</dc:date>
    </item>
  </channel>
</rss>