<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic where is the mc9s08aw16.h? in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/where-is-the-mc9s08aw16-h/m-p/134315#M3670</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;now i am working on a project using mc9s08aw16,but i can't find the header file for it in codewarrior,and i searched&amp;nbsp;the codewarrior updates,still i can't find it,why?there are mc9s08aw32 and mc9s08aw48 and mc9s08aw60 header files in the web,please tell me the reason.&amp;nbsp;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Oct 2006 21:36:24 GMT</pubDate>
    <dc:creator>allegropro</dc:creator>
    <dc:date>2006-10-25T21:36:24Z</dc:date>
    <item>
      <title>where is the mc9s08aw16.h?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/where-is-the-mc9s08aw16-h/m-p/134315#M3670</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;now i am working on a project using mc9s08aw16,but i can't find the header file for it in codewarrior,and i searched&amp;nbsp;the codewarrior updates,still i can't find it,why?there are mc9s08aw32 and mc9s08aw48 and mc9s08aw60 header files in the web,please tell me the reason.&amp;nbsp;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Oct 2006 21:36:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/where-is-the-mc9s08aw16-h/m-p/134315#M3670</guid>
      <dc:creator>allegropro</dc:creator>
      <dc:date>2006-10-25T21:36:24Z</dc:date>
    </item>
    <item>
      <title>Re: where is the mc9s08aw16.h?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/where-is-the-mc9s08aw16-h/m-p/134316#M3671</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Since the differences between the header files for the other devices is minimal, you should be able to create your own header file for the AW16.&amp;nbsp; Copy and rename one of the existing files.&amp;nbsp; I would&amp;nbsp;suspect that the only edit required would be to replace the&amp;nbsp;lines -&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Courier New" size="2"&gt;#ifndef _MC9S08AW60_H&lt;BR /&gt;#define _MC9S08AW60_H&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;with the following -&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;FONT face="Courier New"&gt;#ifndef _MC9S08AW16_H&lt;BR /&gt;#define _MC9S08AW16_H&lt;BR /&gt;&lt;/FONT&gt;&lt;BR /&gt;This are&amp;nbsp;the only difference&amp;nbsp;between the other header files.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Oct 2006 23:59:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/where-is-the-mc9s08aw16-h/m-p/134316#M3671</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2006-10-25T23:59:18Z</dc:date>
    </item>
    <item>
      <title>Re: where is the mc9s08aw16.h?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/where-is-the-mc9s08aw16-h/m-p/134317#M3672</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Just a side note.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;CodeWarrior HC08 V5.1 comes with a header file mc9s08aw16a.h for HCS08AW16.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;CrasyCat&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Oct 2006 21:14:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/where-is-the-mc9s08aw16-h/m-p/134317#M3672</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2006-10-26T21:14:46Z</dc:date>
    </item>
    <item>
      <title>Re: where is the mc9s08aw16.h?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/where-is-the-mc9s08aw16-h/m-p/134318#M3673</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;&lt;BLOCKQUOTE&gt;&lt;DIV&gt;&lt;HR /&gt;CrasyCat wrote:&lt;BR /&gt;&lt;DIV&gt;Just a side note.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;CodeWarrior HC08 V5.1 comes with a header file mc9s08aw16a.h for HCS08AW16.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;CrasyCat&lt;/DIV&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;BR /&gt;&lt;DIV&gt;Funny, my CW5.1 didn't &lt;IMG alt=":smileysad:" class="emoticon emoticon-smileysad" id="smileysad" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-sad.gif" title="Smiley Sad" /&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Nov 2006 04:12:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/where-is-the-mc9s08aw16-h/m-p/134318#M3673</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2006-11-21T04:12:25Z</dc:date>
    </item>
  </channel>
</rss>