<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: connecting ZSTAR via serial</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/connecting-ZSTAR-via-serial/m-p/134231#M3663</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Dears,&lt;BR /&gt;&lt;BR /&gt;since the ZSTAR uses serial communication emulation over USB, the actual baudrate is only limited by the speed of USB stick/USB bus/driver chain. No serial parameter is taken into account, simply all settings are ignored.&lt;BR /&gt;&lt;BR /&gt;Once the RD3152MMA7260Q_SW.exe GUI works, the same COM port number can be used to grab the data over HyperTerminal or any other application that is able to talk to serial port.&lt;BR /&gt;&lt;BR /&gt;BTW, new firmware for Sensor and USB stick plus the new GUI is being developped and soon will be available to replace current firmware.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Pavel Lajsner (ZSTAR co-developper)&lt;BR /&gt;Freescale Czech Republic&lt;BR /&gt;&lt;BR /&gt;Message Edited by ok2ucx on &lt;SPAN class="date_text"&gt;2007-09-21&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;09:07 PM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 22 Sep 2007 02:06:47 GMT</pubDate>
    <dc:creator>ok2ucx</dc:creator>
    <dc:date>2007-09-22T02:06:47Z</dc:date>
    <item>
      <title>connecting ZSTAR via serial</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/connecting-ZSTAR-via-serial/m-p/134229#M3661</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;SPAN&gt;Folks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've just got a ZSTAR kit for evaluation, everything works fine with included demo.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;But I cant get anything via hyper-terminal through COM port. I tried serveral setting parameters and&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;still dont working at all.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Since I want grab information for the sensor directly, is anyone successful on this yet ? Otherwise there's&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;some documents that I was missing.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for your help&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ed&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 19 May 2007 08:41:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/connecting-ZSTAR-via-serial/m-p/134229#M3661</guid>
      <dc:creator>edwardc</dc:creator>
      <dc:date>2007-05-19T08:41:35Z</dc:date>
    </item>
    <item>
      <title>Re: connecting ZSTAR via serial</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/connecting-ZSTAR-via-serial/m-p/134230#M3662</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;It works fine. The documentation for the serial protocol is ZSTARRM.pdf.&lt;BR /&gt;&lt;BR /&gt;serial parameter (e.g.):&lt;BR /&gt;baud rate 9600&lt;BR /&gt;data 8bit&lt;BR /&gt;stop 1bit&lt;BR /&gt;&lt;BR /&gt;you can optimize speed, on my pc it even works with 115200.&lt;BR /&gt;&lt;BR /&gt;Bye,&lt;BR /&gt;Martin&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 May 2007 14:16:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/connecting-ZSTAR-via-serial/m-p/134230#M3662</guid>
      <dc:creator>mjo</dc:creator>
      <dc:date>2007-05-23T14:16:40Z</dc:date>
    </item>
    <item>
      <title>Re: connecting ZSTAR via serial</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/connecting-ZSTAR-via-serial/m-p/134231#M3663</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Dears,&lt;BR /&gt;&lt;BR /&gt;since the ZSTAR uses serial communication emulation over USB, the actual baudrate is only limited by the speed of USB stick/USB bus/driver chain. No serial parameter is taken into account, simply all settings are ignored.&lt;BR /&gt;&lt;BR /&gt;Once the RD3152MMA7260Q_SW.exe GUI works, the same COM port number can be used to grab the data over HyperTerminal or any other application that is able to talk to serial port.&lt;BR /&gt;&lt;BR /&gt;BTW, new firmware for Sensor and USB stick plus the new GUI is being developped and soon will be available to replace current firmware.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Pavel Lajsner (ZSTAR co-developper)&lt;BR /&gt;Freescale Czech Republic&lt;BR /&gt;&lt;BR /&gt;Message Edited by ok2ucx on &lt;SPAN class="date_text"&gt;2007-09-21&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;09:07 PM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 22 Sep 2007 02:06:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/connecting-ZSTAR-via-serial/m-p/134231#M3663</guid>
      <dc:creator>ok2ucx</dc:creator>
      <dc:date>2007-09-22T02:06:47Z</dc:date>
    </item>
  </channel>
</rss>