<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: question about QT4 flash using ...</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/question-about-QT4-flash-using/m-p/134002#M3602</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;&lt;FONT size="2"&gt;Hello Dany,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;I have attached a file that provides a simple&amp;nbsp;&lt;/FONT&gt;&lt;FONT size="2"&gt;sub-routine&amp;nbsp;that erases the first page (64 bytes) of&amp;nbsp; flash memory, and programs the data into the first 32 byte block.&amp;nbsp; This should be satisfactory provided the stored data doesn't have to be re-written too often.&amp;nbsp; If more frequent re-writes are required, the more complex method of AN2346&amp;nbsp;might be used.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;For the simple case, no special measures are required to read the programmed flash bytes.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Regards,&lt;BR /&gt;Mac&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;BR /&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 May 2006 03:10:27 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2006-05-04T03:10:27Z</dc:date>
    <item>
      <title>question about QT4 flash using ...</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/question-about-QT4-flash-using/m-p/134000#M3600</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I have to write and read a couple of bytes in the flash area while QT4 MCU is running my code.&lt;/DIV&gt;&lt;DIV&gt;Does anybody knows about any "AN" I can get with an assembler example of this?&lt;/DIV&gt;&lt;DIV&gt;Thank you!&lt;/DIV&gt;&lt;DIV&gt;Dany&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Apr 2006 19:57:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/question-about-QT4-flash-using/m-p/134000#M3600</guid>
      <dc:creator>DanyPier</dc:creator>
      <dc:date>2006-04-28T19:57:04Z</dc:date>
    </item>
    <item>
      <title>Re: question about QT4 flash using ...</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/question-about-QT4-flash-using/m-p/134001#M3601</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;How about AN1831?&lt;/P&gt;&lt;P&gt;Peg&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Apr 2006 20:15:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/question-about-QT4-flash-using/m-p/134001#M3601</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2006-04-28T20:15:40Z</dc:date>
    </item>
    <item>
      <title>Re: question about QT4 flash using ...</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/question-about-QT4-flash-using/m-p/134002#M3602</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;&lt;FONT size="2"&gt;Hello Dany,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;I have attached a file that provides a simple&amp;nbsp;&lt;/FONT&gt;&lt;FONT size="2"&gt;sub-routine&amp;nbsp;that erases the first page (64 bytes) of&amp;nbsp; flash memory, and programs the data into the first 32 byte block.&amp;nbsp; This should be satisfactory provided the stored data doesn't have to be re-written too often.&amp;nbsp; If more frequent re-writes are required, the more complex method of AN2346&amp;nbsp;might be used.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;For the simple case, no special measures are required to read the programmed flash bytes.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Regards,&lt;BR /&gt;Mac&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;BR /&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 May 2006 03:10:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/question-about-QT4-flash-using/m-p/134002#M3602</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2006-05-04T03:10:27Z</dc:date>
    </item>
  </channel>
</rss>