<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Help: MMDS05 fail to load firmware</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-MMDS05-fail-to-load-firmware/m-p/133969#M3581</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi, Simon:&lt;BR /&gt;&lt;BR /&gt;Is your target powered up and is it's clock running?&lt;BR /&gt;&lt;BR /&gt;The clock in my system is configured to run from the target, which I believe is the default. If the target is not providing a clock to the processor, my system hangs at the "Loading Firmware" message.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Oct 2006 12:09:46 GMT</pubDate>
    <dc:creator>rocco</dc:creator>
    <dc:date>2006-10-23T12:09:46Z</dc:date>
    <item>
      <title>Help: MMDS05 fail to load firmware</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-MMDS05-fail-to-load-firmware/m-p/133968#M3580</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I am using the MMDS05 and M68EM08 series emulator modules, but now when I try to load ZAP MMDS 6808, it always fails to load firmware, I mean it always reports "loading firmware"? Is there any possible root cause that I can try to fix?&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Oct 2006 10:26:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-MMDS05-fail-to-load-firmware/m-p/133968#M3580</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2006-10-23T10:26:09Z</dc:date>
    </item>
    <item>
      <title>Re: Help: MMDS05 fail to load firmware</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-MMDS05-fail-to-load-firmware/m-p/133969#M3581</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi, Simon:&lt;BR /&gt;&lt;BR /&gt;Is your target powered up and is it's clock running?&lt;BR /&gt;&lt;BR /&gt;The clock in my system is configured to run from the target, which I believe is the default. If the target is not providing a clock to the processor, my system hangs at the "Loading Firmware" message.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Oct 2006 12:09:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-MMDS05-fail-to-load-firmware/m-p/133969#M3581</guid>
      <dc:creator>rocco</dc:creator>
      <dc:date>2006-10-23T12:09:46Z</dc:date>
    </item>
    <item>
      <title>Re: Help: MMDS05 fail to load firmware</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-MMDS05-fail-to-load-firmware/m-p/133970#M3582</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi, rocco:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I replaced the target&amp;nbsp;MCU and it work now. I think maybe the target&amp;nbsp;has some problem.&lt;/DIV&gt;&lt;DIV&gt;Thanks for your advice.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Oct 2006 16:12:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-MMDS05-fail-to-load-firmware/m-p/133970#M3582</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2006-10-24T16:12:08Z</dc:date>
    </item>
  </channel>
</rss>