<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 9S08AW16 vs 9S08GT16 ? in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08AW16-vs-9S08GT16/m-p/133368#M3364</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I'm working on a project using 9S08QG8....... I'm almost out of flash so I have to move up to 16K flash device.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I see that the 9S08AW16 and 9S08GT16 have pretty much the same features (although the 08AW will work @ 5V), can anyone recommend which device I should move to?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I've noticed that&amp;nbsp;no-one has stock of the&amp;nbsp;GT16. Is this a common problem?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Any direction would be appreciated.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Oct 2006 20:18:10 GMT</pubDate>
    <dc:creator>paul</dc:creator>
    <dc:date>2006-10-17T20:18:10Z</dc:date>
    <item>
      <title>9S08AW16 vs 9S08GT16 ?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08AW16-vs-9S08GT16/m-p/133368#M3364</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I'm working on a project using 9S08QG8....... I'm almost out of flash so I have to move up to 16K flash device.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I see that the 9S08AW16 and 9S08GT16 have pretty much the same features (although the 08AW will work @ 5V), can anyone recommend which device I should move to?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I've noticed that&amp;nbsp;no-one has stock of the&amp;nbsp;GT16. Is this a common problem?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Any direction would be appreciated.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Oct 2006 20:18:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08AW16-vs-9S08GT16/m-p/133368#M3364</guid>
      <dc:creator>paul</dc:creator>
      <dc:date>2006-10-17T20:18:10Z</dc:date>
    </item>
    <item>
      <title>Re: 9S08AW16 vs 9S08GT16 ?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08AW16-vs-9S08GT16/m-p/133369#M3365</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;I'm not too sure about the availability part of your question, but I would check with your local Avnet person.&amp;nbsp; Both devices are fairly new, so they should be around for quite awhile.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;As far as the differences, it really comes down to what you really need:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;5V I/O or more than 8 ADC channels&amp;nbsp;-&amp;gt; use the AW&lt;/DIV&gt;&lt;DIV&gt;down to 1.8V, lower power&amp;nbsp;-&amp;gt; use the GT (or GTA for more RAM)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The other consideration is the prototype build.&amp;nbsp; If you need to&amp;nbsp;build it yourself, then the GT is available in a DIP package.&amp;nbsp; The AW is QFP(tough, but can be done by hand)&amp;nbsp;or QFN(good luck with this one).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Just my couple pennies worth.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Brian&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Oct 2006 22:18:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08AW16-vs-9S08GT16/m-p/133369#M3365</guid>
      <dc:creator>baddad</dc:creator>
      <dc:date>2006-10-17T22:18:16Z</dc:date>
    </item>
  </channel>
</rss>