<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックMC13213 SRD and NCB Hardware Design Error??</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13213-SRD-and-NCB-Hardware-Design-Error/m-p/133308#M3342</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;SPAN&gt;The schematics for the SRD and NCB boards show some signals from Port C connected to IC 104 which is an Atmel AT25HP512. I believe that this is a 65K x 8 bit EEPROM with a serial SPI interface. Unfortunately, Port C isn't the SPI. Unless I'm missing something, I don't see how this chip can ever be driven by the MC13213. Also, you can't simply re-wire the EEPROM to the SPI signals on the MC13213 because they are reserved for use by the wireless transceiver internal to the SOC.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does anyone else have any ideas?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Chuck Matthews&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 10 May 2007 05:07:55 GMT</pubDate>
    <dc:creator>fgs_chuck</dc:creator>
    <dc:date>2007-05-10T05:07:55Z</dc:date>
    <item>
      <title>MC13213 SRD and NCB Hardware Design Error??</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13213-SRD-and-NCB-Hardware-Design-Error/m-p/133308#M3342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;SPAN&gt;The schematics for the SRD and NCB boards show some signals from Port C connected to IC 104 which is an Atmel AT25HP512. I believe that this is a 65K x 8 bit EEPROM with a serial SPI interface. Unfortunately, Port C isn't the SPI. Unless I'm missing something, I don't see how this chip can ever be driven by the MC13213. Also, you can't simply re-wire the EEPROM to the SPI signals on the MC13213 because they are reserved for use by the wireless transceiver internal to the SOC.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does anyone else have any ideas?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Chuck Matthews&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 May 2007 05:07:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13213-SRD-and-NCB-Hardware-Design-Error/m-p/133308#M3342</guid>
      <dc:creator>fgs_chuck</dc:creator>
      <dc:date>2007-05-10T05:07:55Z</dc:date>
    </item>
    <item>
      <title>Re: MC13213 SRD and NCB Hardware Design Error??</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13213-SRD-and-NCB-Hardware-Design-Error/m-p/133309#M3343</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Bit-banged SPI?&lt;/DIV&gt;&lt;DIV&gt;It's pretty simple to do.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 May 2007 06:47:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13213-SRD-and-NCB-Hardware-Design-Error/m-p/133309#M3343</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2007-05-10T06:47:44Z</dc:date>
    </item>
    <item>
      <title>Re: MC13213 SRD and NCB Hardware Design Error??</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13213-SRD-and-NCB-Hardware-Design-Error/m-p/133310#M3344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hmm, didn't think of that. Has anyone seen any occurrence of this in any of the examples from Freescale? Perhaps in a template that the ZigBee BeeKit produces?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Chuck&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 May 2007 19:52:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13213-SRD-and-NCB-Hardware-Design-Error/m-p/133310#M3344</guid>
      <dc:creator>fgs_chuck</dc:creator>
      <dc:date>2007-05-10T19:52:27Z</dc:date>
    </item>
    <item>
      <title>Re: MC13213 SRD and NCB Hardware Design Error??</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13213-SRD-and-NCB-Hardware-Design-Error/m-p/133311#M3345</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello Chuck,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I think the SPI is only for the internal connection between the MCU and the modem.&lt;/DIV&gt;&lt;DIV&gt;There is no SPI connection outside. You have to implement the sw SPI routines.&lt;/DIV&gt;&lt;DIV&gt;We design our own devices using external FLASH via SPI, and I had to code this feature.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Peter&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Oct 2007 22:21:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13213-SRD-and-NCB-Hardware-Design-Error/m-p/133311#M3345</guid>
      <dc:creator>FPatrick</dc:creator>
      <dc:date>2007-10-11T22:21:27Z</dc:date>
    </item>
  </channel>
</rss>