<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: regarding low power management</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/regarding-low-power-management/m-p/133297#M3341</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi&lt;BR /&gt;I'm trying to use SMAC with low power, but I found problems. Infact in my opinion there are some problems when I use RTI and STOP3 mode, I used an example appeared in SMAC4.1a ver called SimpleNetwork but after a while this example crash.&lt;BR /&gt;How do you use the low power features?&lt;BR /&gt;&lt;BR /&gt;Thx&lt;BR /&gt;Stevasway&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Oct 2006 14:29:41 GMT</pubDate>
    <dc:creator>stevasway</dc:creator>
    <dc:date>2006-10-24T14:29:41Z</dc:date>
    <item>
      <title>regarding low power management</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/regarding-low-power-management/m-p/133292#M3336</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Can any one provide source code for Low power management of mc9s08gt/gb60&lt;/DIV&gt;&lt;DIV&gt;board. I am facing problems when entering and exiting from low power modes.&lt;/DIV&gt;&lt;DIV&gt;Its urgent.plaese reply as early as possible.&lt;/DIV&gt;&lt;DIV&gt;Thank you .&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Apr 2006 19:13:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/regarding-low-power-management/m-p/133292#M3336</guid>
      <dc:creator>rao</dc:creator>
      <dc:date>2006-04-21T19:13:23Z</dc:date>
    </item>
    <item>
      <title>Re: regarding low power management</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/regarding-low-power-management/m-p/133293#M3337</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi:&lt;BR /&gt;&lt;BR /&gt;It would be helpful if you explain what kind of problems you're facing: not coming out of low power, which mode has problems, data corruption, etc.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;&lt;BR /&gt;Alex&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Apr 2006 20:45:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/regarding-low-power-management/m-p/133293#M3337</guid>
      <dc:creator>alex_spotw</dc:creator>
      <dc:date>2006-04-21T20:45:02Z</dc:date>
    </item>
    <item>
      <title>Re: regarding low power management</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/regarding-low-power-management/m-p/133294#M3338</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;RTI clock not responding in stop3&lt;/P&gt;&lt;P&gt;And radio not getting wake up in doze mode.&lt;/P&gt;&lt;P&gt;How u measured power across the resistors provided on the board.&lt;/P&gt;&lt;P&gt;please reply asap.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 22 Apr 2006 11:06:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/regarding-low-power-management/m-p/133294#M3338</guid>
      <dc:creator>rao</dc:creator>
      <dc:date>2006-04-22T11:06:37Z</dc:date>
    </item>
    <item>
      <title>Re: regarding low power management</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/regarding-low-power-management/m-p/133295#M3339</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi:&lt;BR /&gt;&lt;BR /&gt;As the datasheet says:&lt;BR /&gt;&lt;BR /&gt;&lt;B&gt;In run and wait modes, only the external clock can be used as the RTI's clock source. In stop2 mode, only&lt;BR /&gt;the internal RTI clock can be used. In stop3, either the external clock or internal RTI clock can be used.&lt;BR /&gt;&lt;BR /&gt;When using the external oscillator in stop3 mode, it must be enabled in stop (OSCSTEN = 1) and&lt;BR /&gt;configured for low bandwidth operation (RANGE = 0).&lt;BR /&gt;&lt;BR /&gt;&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;Do you use the External or the Internal OSC in Mode 3?&lt;BR /&gt;&lt;BR /&gt;Why do you want to measure the power over resistors? Which resistors and which board?&lt;BR /&gt;&lt;BR /&gt;Let us know!&lt;BR /&gt;&lt;BR /&gt;Alex&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Apr 2006 00:46:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/regarding-low-power-management/m-p/133295#M3339</guid>
      <dc:creator>alex_spotw</dc:creator>
      <dc:date>2006-04-25T00:46:30Z</dc:date>
    </item>
    <item>
      <title>Re: regarding low power management</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/regarding-low-power-management/m-p/133296#M3340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;I ma also facing problem with RTI in low power management. I have wirtten test code to put Radio (MC13192) in Hibernate mode and then I am putting radio into Stop 3 mode. I am trying to use RTI with its intenal clock. But CPU is not coming out off stop 3 mode after time out. My ISR is not getting executed.&lt;/DIV&gt;&lt;DIV&gt;As far As RTI ISR is concern, its worknig fine in normal mode (with ext clock source).&lt;/DIV&gt;&lt;DIV&gt;MCU is responding ti KBI interrupt in stop mode.&lt;/DIV&gt;&lt;DIV&gt;But I am facing some problem with RTI in stop mode. I don't know what kind of problem, but trying to find out.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 18 Jun 2006 23:50:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/regarding-low-power-management/m-p/133296#M3340</guid>
      <dc:creator>SST</dc:creator>
      <dc:date>2006-06-18T23:50:41Z</dc:date>
    </item>
    <item>
      <title>Re: regarding low power management</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/regarding-low-power-management/m-p/133297#M3341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi&lt;BR /&gt;I'm trying to use SMAC with low power, but I found problems. Infact in my opinion there are some problems when I use RTI and STOP3 mode, I used an example appeared in SMAC4.1a ver called SimpleNetwork but after a while this example crash.&lt;BR /&gt;How do you use the low power features?&lt;BR /&gt;&lt;BR /&gt;Thx&lt;BR /&gt;Stevasway&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Oct 2006 14:29:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/regarding-low-power-management/m-p/133297#M3341</guid>
      <dc:creator>stevasway</dc:creator>
      <dc:date>2006-10-24T14:29:41Z</dc:date>
    </item>
  </channel>
</rss>