<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Wire GR8 For Real World Use? in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Wire-GR8-For-Real-World-Use/m-p/132945#M3226</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Mac,&lt;BR /&gt;&lt;BR /&gt;Thanks so much for your speedy response! I will implement these changes immedietly! I don't think the chip is damaged from the SCI already, b/c I can put it back into monitor mode and it works fine, but we'll see!&lt;BR /&gt;&lt;BR /&gt;Thank You!&lt;BR /&gt;-Avery&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Oct 2006 12:57:18 GMT</pubDate>
    <dc:creator>AveryZ</dc:creator>
    <dc:date>2006-10-12T12:57:18Z</dc:date>
    <item>
      <title>Wire GR8 For Real World Use?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Wire-GR8-For-Real-World-Use/m-p/132943#M3224</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a GR8 that I built a programmer for, loaded with code, and now I am ready to move it into its actual real home. I am having trouble figuring out how to wire it so that when it recieves voltage/turns on, it just jumps right into the program code thats on it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Forgetting about where I/O is wired, I connected Vdd and Vss, Vdda and Vssa, and Vdda/ref and Vssa/ref to ground and voltage respectively. I have also connected OSC1 to my crystal which is 9.8304. Is there anythign else that should be wired?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Also I am communicating with the PC over SCI, and I have the two wires plugged directly into their respective ports on the chip, should they be going through a MAX232?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks Guys!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-Avery&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Oct 2006 07:56:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Wire-GR8-For-Real-World-Use/m-p/132943#M3224</guid>
      <dc:creator>AveryZ</dc:creator>
      <dc:date>2006-10-12T07:56:42Z</dc:date>
    </item>
    <item>
      <title>Re: Wire GR8 For Real World Use?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Wire-GR8-For-Real-World-Use/m-p/132944#M3225</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello Avery,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;BR /&gt;&lt;/DIV&gt;&lt;BLOCKQUOTE&gt;&lt;DIV&gt;&lt;FONT size="1"&gt;&lt;/FONT&gt;&lt;HR /&gt;&lt;FONT size="1"&gt;Avery Z wrote:&lt;BR /&gt;&lt;BR /&gt;... &amp;nbsp;I connected Vdd and Vss, Vdda and Vssa, and Vdda/ref and Vssa/ref to ground and voltage respectively. I have also connected OSC1 to my crystal which is 9.8304. Is there anythign else that should be wired?&lt;BR /&gt;&lt;/FONT&gt;&lt;HR /&gt;&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Did you provide separate de-coupling capacitors at each of the supply connection points, as specified in the data sheet?&amp;nbsp; Did you connect the crystal as a Pierce oscillator configuration, as shown in Fig. 28 of the data sheet?&amp;nbsp; This involves connections to both OSC1 and OSC2.&amp;nbsp; For a 9.8304 MHz crystal, the resistor Rs can usually be omitted, and make C2 a fixed capacitor of the same value as C1.&amp;nbsp; What component values do you currently use.&lt;/FONT&gt;&lt;/DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;/DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;DIV&gt;&lt;BR /&gt;&lt;/DIV&gt;&lt;BLOCKQUOTE&gt;&lt;DIV&gt;&lt;FONT size="1"&gt;&lt;/FONT&gt;&lt;HR /&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="1"&gt;Avery Z wrote:&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="1"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="1"&gt;Also I am communicating with the PC over SCI, and I have the two wires plugged directly into their respective ports on the chip, should they be going through a MAX232?&lt;BR /&gt;&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="1"&gt;&lt;/FONT&gt;&lt;HR /&gt;&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Very definitely.&amp;nbsp; You may have already damaged the chip!&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Oct 2006 10:04:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Wire-GR8-For-Real-World-Use/m-p/132944#M3225</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2006-10-12T10:04:02Z</dc:date>
    </item>
    <item>
      <title>Re: Wire GR8 For Real World Use?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Wire-GR8-For-Real-World-Use/m-p/132945#M3226</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Mac,&lt;BR /&gt;&lt;BR /&gt;Thanks so much for your speedy response! I will implement these changes immedietly! I don't think the chip is damaged from the SCI already, b/c I can put it back into monitor mode and it works fine, but we'll see!&lt;BR /&gt;&lt;BR /&gt;Thank You!&lt;BR /&gt;-Avery&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Oct 2006 12:57:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Wire-GR8-For-Real-World-Use/m-p/132945#M3226</guid>
      <dc:creator>AveryZ</dc:creator>
      <dc:date>2006-10-12T12:57:18Z</dc:date>
    </item>
  </channel>
</rss>