<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: HC08AP32A in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC08AP32A/m-p/132556#M3088</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I currently have the board set-up with an 8-Mhz Ceramic Resonator (3-lead with built in 20 pF by-pass capactors) and 10M bypass resistor. I have tried all combination, 1Mhz Resistor, 4Mhz Resonator, 8Mhz crystal. I even have an FAE from Freescale create a small program based upon my schematic just to blink a led design with an 8Mhz crystal and no-phase loop loop. Same results. This board works fine with an external oscillator.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 15 Apr 2006 10:11:34 GMT</pubDate>
    <dc:creator>byteybird1</dc:creator>
    <dc:date>2006-04-15T10:11:34Z</dc:date>
    <item>
      <title>HC08AP32A</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC08AP32A/m-p/132554#M3086</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;I'm using the A version of this part because it accepts a crystal from 1 to 8Mhz, whereasa the "non A" accepts a 32KHz crystal.&amp;nbsp;&amp;nbsp;&amp;nbsp;I'm having a problem where the 8 MHz crystal is not oscillationg (I'm using 20 pF on each leg to ground).&amp;nbsp; &amp;nbsp;I build 6-boards. the first two I put together (using samples from freescale) work.&amp;nbsp; The other 4-boards (micros were purchased) only 1 boards is oscillationg.&amp;nbsp; The other 3, the circuit is not working.&amp;nbsp; I am not using the phase lock loop.&amp;nbsp; I also tried a 4 and an 8 Mhz resonator.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I&amp;nbsp; replaced the micro on one of the boards and still the crystal is not oscillating.&amp;nbsp; The boards work find if I used an external oscillator.&amp;nbsp; This should be the simplest part of the total design.&amp;nbsp; Could the parts be mismarked and I actually received the "Non A" device.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Any suggestion would be greatly appreciated.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Apr 2006 02:39:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HC08AP32A/m-p/132554#M3086</guid>
      <dc:creator>byteybird</dc:creator>
      <dc:date>2006-04-15T02:39:15Z</dc:date>
    </item>
    <item>
      <title>Re: HC08AP32A</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC08AP32A/m-p/132555#M3087</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hi byteybird,&lt;/P&gt;&lt;P&gt;I presume you have 1 10Meg or so parallel resistor and NO series resistor (as you might with a 32kHz xtal).&lt;/P&gt;&lt;P&gt;Have you tried a "good" xtal in a "bad" board. I have seen quite a few "dud" crystals.&lt;/P&gt;&lt;P&gt;BR Peg&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Apr 2006 08:22:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HC08AP32A/m-p/132555#M3087</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2006-04-15T08:22:00Z</dc:date>
    </item>
    <item>
      <title>Re: HC08AP32A</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC08AP32A/m-p/132556#M3088</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I currently have the board set-up with an 8-Mhz Ceramic Resonator (3-lead with built in 20 pF by-pass capactors) and 10M bypass resistor. I have tried all combination, 1Mhz Resistor, 4Mhz Resonator, 8Mhz crystal. I even have an FAE from Freescale create a small program based upon my schematic just to blink a led design with an 8Mhz crystal and no-phase loop loop. Same results. This board works fine with an external oscillator.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Apr 2006 10:11:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HC08AP32A/m-p/132556#M3088</guid>
      <dc:creator>byteybird1</dc:creator>
      <dc:date>2006-04-15T10:11:34Z</dc:date>
    </item>
  </channel>
</rss>