<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: about 908AP32 AD</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/about-908AP32-AD/m-p/132332#M3012</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thanks.&lt;/P&gt;&lt;P&gt;appreciate your response.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Apr 2006 13:09:54 GMT</pubDate>
    <dc:creator>lijiandong</dc:creator>
    <dc:date>2006-04-13T13:09:54Z</dc:date>
    <item>
      <title>about 908AP32 AD</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/about-908AP32-AD/m-p/132330#M3010</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Now&amp;nbsp; a project&amp;nbsp;need 1V-2V&amp;nbsp; voltage AD samples, i use 908AP32 ,my question is whether&amp;nbsp;may &amp;nbsp;I&amp;nbsp;connect the Vrefh port to 2V and Vrefl port to 1V for sampling? if&amp;nbsp;Yes ,&amp;nbsp;Whether the the&amp;nbsp; resolution in 1V-2V increases because the span becomes samll, if not, how to solve it?thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Apr 2006 12:20:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/about-908AP32-AD/m-p/132330#M3010</guid>
      <dc:creator>lijiandong</dc:creator>
      <dc:date>2006-04-13T12:20:13Z</dc:date>
    </item>
    <item>
      <title>Re: about 908AP32 AD</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/about-908AP32-AD/m-p/132331#M3011</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi, lijiandong:&lt;BR /&gt;&lt;BR /&gt;The AP32 is a 5 volt part, and the Vrefl and Vrefh pins need to be at the same voltage as the rest of the chip (don't ask me why; it just does).&lt;BR /&gt;&lt;BR /&gt;The good news is that the ADC has 10 bits of resolution, rather then the 8 bits of many HC08 ADCs. If your reference voltage is precisely at 5 volts, 1 volt will convert to 205 and 2 volts will convert to 410, giving you 205 steps. You will have just under 5 millivolts (actually 4.88 millivolts) per step.&lt;BR /&gt;&lt;BR /&gt;If that isn't enough resolution, you will need to use an external ADC.&lt;P&gt;Message Edited by rocco on &lt;SPAN class="date_text"&gt;04-12-2006&lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;11:00 PM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Apr 2006 12:58:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/about-908AP32-AD/m-p/132331#M3011</guid>
      <dc:creator>rocco</dc:creator>
      <dc:date>2006-04-13T12:58:29Z</dc:date>
    </item>
    <item>
      <title>Re: about 908AP32 AD</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/about-908AP32-AD/m-p/132332#M3012</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thanks.&lt;/P&gt;&lt;P&gt;appreciate your response.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Apr 2006 13:09:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/about-908AP32-AD/m-p/132332#M3012</guid>
      <dc:creator>lijiandong</dc:creator>
      <dc:date>2006-04-13T13:09:54Z</dc:date>
    </item>
    <item>
      <title>Re: about 908AP32 AD</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/about-908AP32-AD/m-p/132333#M3013</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;If you're already going to be adding external parts, it would probably be easier to amplify the signal by 5 and add -1 volts with an opamp and a few resistors.&amp;nbsp; Then you could use the full range and precision of the ADC and not have to write any software to interface the external ADC.&amp;nbsp; And if you use an external ADC, you still won't get to use its full range anyway.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Apr 2006 23:50:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/about-908AP32-AD/m-p/132333#M3013</guid>
      <dc:creator>rhinoceroshead</dc:creator>
      <dc:date>2006-04-19T23:50:15Z</dc:date>
    </item>
  </channel>
</rss>