<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Keyboard interrupt</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Keyboard-interrupt/m-p/132129#M2934</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi Ernest,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;You can see two problems from the supplied waveform.&lt;/DIV&gt;&lt;DIV&gt;1. Sometimes it fails to respond.&lt;/DIV&gt;&lt;DIV&gt;2. Sometimes it apparently responds to both edges/levels.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;This is because you have select level sensitivity instead of edge (leave KBIMOD at 0)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If you want it to toggle at each edge you would have to flip the polarity in the ISR, but watch the pullup/downs.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;You should also look at it with a faster timebase and the problem may be more apparent.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 30 Apr 2007 11:30:55 GMT</pubDate>
    <dc:creator>peg</dc:creator>
    <dc:date>2007-04-30T11:30:55Z</dc:date>
    <item>
      <title>Keyboard interrupt</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Keyboard-interrupt/m-p/132128#M2933</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I have been tring to get the keyboard interrupt to work on MC9S08QG8. I have simplifed the code to the following to try and find the problem.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;SPAN class="msg_source_code"&gt;&lt;SPAN class="text_smallest"&gt;Code:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;PRE&gt;void main(void) {&amp;nbsp;&amp;nbsp; SOPT1_COPE = 0;&amp;nbsp; //diable COP&amp;nbsp;&amp;nbsp; // KBI Set Up foe SW1&amp;nbsp;&amp;nbsp; KBIPE_KBIPE1 =1;&amp;nbsp;&amp;nbsp; /* Enable Keyboard Pin */&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; KBISC_KBIE = 1;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Enable Keyboard Interrupts */&amp;nbsp;&amp;nbsp; KBISC_KBACK = 1;&amp;nbsp;&amp;nbsp; /* Clear Pending Keyboard Interrupts */&amp;nbsp;&amp;nbsp; PTAPE_PTAPE1 = 1;&amp;nbsp;&amp;nbsp; /* Enable Pullup for Keyboard pin */&amp;nbsp;&amp;nbsp; KBISC_KBIMOD = 1;&amp;nbsp;&amp;nbsp; PTBDD_PTBDD1 = 1;&amp;nbsp; //A1&amp;nbsp;&amp;nbsp; EnableInterrupts;&amp;nbsp;&amp;nbsp;&amp;nbsp; for(;;)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Loop Forever&amp;nbsp; {&amp;nbsp; }}//*******************************************// KBI ISR&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // interuptinterrupt 18 void&amp;nbsp;&amp;nbsp; KBI_ISR(void) {&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PTBD_PTBD1 = ~PTAD_PTAD1;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* toggle Port */&amp;nbsp; KBISC_KBACK = 1;&lt;/PRE&gt;&lt;PRE&gt;}&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The&amp;nbsp;waveform from a light gate is input to the keyboard interupt pin and i expect the output pin&amp;nbsp;to toggle on change. However, altough it does most of the time many interupts are missed. Below are the input and output waveforms. I have zoomed in on input waveform and it appears to be clean. Any suggestions greatly appreciated.&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.formulastudent.strath.ac.uk/scope.bmp" rel="nofollow noopener noreferrer" target="_blank"&gt;&lt;IMG src="http://www.formulastudent.strath.ac.uk/scope.bmp" /&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Many Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Apr 2007 10:17:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Keyboard-interrupt/m-p/132128#M2933</guid>
      <dc:creator>ernestsnaith</dc:creator>
      <dc:date>2007-04-30T10:17:09Z</dc:date>
    </item>
    <item>
      <title>Re: Keyboard interrupt</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Keyboard-interrupt/m-p/132129#M2934</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi Ernest,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;You can see two problems from the supplied waveform.&lt;/DIV&gt;&lt;DIV&gt;1. Sometimes it fails to respond.&lt;/DIV&gt;&lt;DIV&gt;2. Sometimes it apparently responds to both edges/levels.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;This is because you have select level sensitivity instead of edge (leave KBIMOD at 0)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If you want it to toggle at each edge you would have to flip the polarity in the ISR, but watch the pullup/downs.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;You should also look at it with a faster timebase and the problem may be more apparent.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Apr 2007 11:30:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Keyboard-interrupt/m-p/132129#M2934</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2007-04-30T11:30:55Z</dc:date>
    </item>
  </channel>
</rss>