<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Lowest Power Consumption</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Lowest-Power-Consumption/m-p/132045#M2912</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I finally got back to this problem. I just cannot get my MC13213 to get into low power consumption STOP2 mode.&lt;BR /&gt;the lowest power it seems to consume is around 900uA.&lt;BR /&gt;&lt;BR /&gt;My most of the IO pins on the board are floating (but I've set them all to outputs), its a direct feed from a 3.3V battery. nothing else on the board except for the TX/RX circuit (LC/baluns etc)&lt;BR /&gt;I'm using SMAC4.2 and have incorporated some of the functions from PWRLib into it.&lt;BR /&gt;&lt;BR /&gt;my code is basically this :&lt;BR /&gt;&lt;BR /&gt;case DEEP_SLEEP_STATE:&lt;BR /&gt;&lt;BR /&gt;UseMcuClock(); // switch to the internal clock&lt;BR /&gt;//Observations: I see clock speed drop to ~4Mhz in the debugger&lt;BR /&gt;&lt;BR /&gt;// set clockspeed to 2Mhz&lt;BR /&gt;PWRLib_ICG_Divider_Setup( N8, R2); //ICGC2 = ((07) | (N4) | (03) | (R0));&lt;BR /&gt;PWRLib_ICG_Mode( LOW_CLOCK); //ICGC1 = ((Clock6) | (05) | (Mode3) | (02));&lt;BR /&gt;//Observations: I see clock speed drop to ~2Mhz in the debugger&lt;BR /&gt;&lt;BR /&gt;SRTISC=0x00; //Disable wake up timer.&lt;BR /&gt;SPMSC1=0x00; // disable LVD&lt;BR /&gt;SPMSC2=0x00; // set PPDF flag to 0&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;MC13192ContReset(); // Place the MC13192 into Reset mode&lt;BR /&gt;//POTENTIAL PROBLEM: the SMAC function seems to set IRQPE = 0 (AN2493 seems to suggest setting it to 1)&lt;BR /&gt;&lt;BR /&gt;// set IRQPE to 1&lt;BR /&gt;IRQSC = 0x1E;&lt;BR /&gt;&lt;BR /&gt;//set all IO pins to outputs&lt;BR /&gt;(e.g. #define mPWRLib_SETUP_PORT_{ALL} PTADD = 0x00;\&lt;BR /&gt;PTAPE = 0x00;\&lt;BR /&gt;PTADD = 0xff; )&lt;BR /&gt;&lt;BR /&gt;PWRLib_SetMCUIOForPowerSavingMode();&lt;BR /&gt;&lt;BR /&gt;PWRLib_RTIClockStart( cPWR_RTITickTime, DozeDuration);&lt;BR /&gt;while ( PWRLib_RTIClockCheck() &amp;gt; 0)&lt;BR /&gt;{&lt;BR /&gt;SPMSC2 |= 0x03; // Sets PDC and PPDC bits for Stop2 mode&lt;BR /&gt;__asm STOP;&lt;BR /&gt;//OBSERVATIONS: Current consumption is around 900uA.&lt;BR /&gt;}&lt;BR /&gt;PWRLib_RTIClockStop();&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;RadioInit();&lt;BR /&gt;AppInit();&lt;BR /&gt;&lt;BR /&gt;// Restart to external clock appx. 10.8mS&lt;BR /&gt;MC13192Restart(); // Bring the MC13192 into the desired Idle condition.&lt;BR /&gt;MC13192Init();&lt;BR /&gt;&lt;BR /&gt;MLMESetChannelRequest(2);&lt;BR /&gt;MLMESetMC13192ClockRate(0); // Set initial Clk speed&lt;BR /&gt;UseExternalClock(); // switch clock sources from mcu to MC1319x CLKO&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;gi8AppStatus = TRANSMIT_DATA;&lt;BR /&gt;&lt;BR /&gt;break;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Any idea whats going on?&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Oct 2006 04:40:34 GMT</pubDate>
    <dc:creator>kbu</dc:creator>
    <dc:date>2006-10-25T04:40:34Z</dc:date>
    <item>
      <title>Lowest Power Consumption</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Lowest-Power-Consumption/m-p/132036#M2903</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;HI,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a GT60 and MC13192 on a module. I've been able to get the micro to get into Stop2 with a 1sec RTI, I'm having trouble getting it to consume close to the power consumption listed in the datasheets.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Here's the setup :&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The MCU is set to 2Mhz internal clock.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Radio is reset.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1.024 sec RTI initialized. (10 second wake up times before doing a transmit on the radio)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;all i/o pins on all ports set to 0x00.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LVD disabled.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;MCU enters Stop2 mode.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;According to AN2493 (GT60 Low power modes), while in stop2 with RTI enabled the system should draw close to 890nA.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;However with my setup, the board seems to be drawing around .4 mA (fluctuates between .428mA and .438mA) . There are no other components on the board, and I'm guessing even with other quiescent current losses I should get a number closer to whats stated in the datasheet.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Has anyone gotten close to this number with their circuits. Any advice?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Apr 2006 02:08:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Lowest-Power-Consumption/m-p/132036#M2903</guid>
      <dc:creator>kbu</dc:creator>
      <dc:date>2006-04-11T02:08:26Z</dc:date>
    </item>
    <item>
      <title>Re: Lowest Power Consumption</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Lowest-Power-Consumption/m-p/132037#M2904</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;HI:&lt;BR /&gt;&lt;BR /&gt;What are you using to measure the current? It the instrument precise enough to give a close measurement to nA?&lt;BR /&gt;&lt;BR /&gt;Waht else do you have in your hardware that might be consuming power? (external memory, devices, the power supply, etc?&lt;BR /&gt;&lt;BR /&gt;Let us know!&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;&lt;BR /&gt;Alex&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Apr 2006 02:12:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Lowest-Power-Consumption/m-p/132037#M2904</guid>
      <dc:creator>alex_spotw</dc:creator>
      <dc:date>2006-04-11T02:12:19Z</dc:date>
    </item>
    <item>
      <title>Re: Lowest Power Consumption</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Lowest-Power-Consumption/m-p/132038#M2905</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I'm using a scope to measure between the legs of a 100 ohm in series with the power supply.&lt;BR /&gt;&lt;BR /&gt;No other devices, this is a zigbee module so only those two components.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Apr 2006 02:18:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Lowest-Power-Consumption/m-p/132038#M2905</guid>
      <dc:creator>kbu</dc:creator>
      <dc:date>2006-04-11T02:18:48Z</dc:date>
    </item>
    <item>
      <title>Re: Lowest Power Consumption</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Lowest-Power-Consumption/m-p/132039#M2906</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;&lt;FONT size="2"&gt;Hello kbu,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;The current you are measuring seems to be roughly that for idle mode of the MC13192, rather than one of the other lower power modes (with SPI inactive).&amp;nbsp; Is this a possibility?&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Any floating unused inputs on the MCU &lt;U&gt;without&lt;/U&gt; pullups enabled?&amp;nbsp; Any unused inputs on the MCU shorted to ground, and &lt;U&gt;with&lt;/U&gt; pullups enabled?&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Regards,&lt;BR /&gt;Mac&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Message Edited by bigmac on &lt;SPAN class="date_text"&gt;04-11-2006&lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;12:55 PM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Apr 2006 09:49:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Lowest-Power-Consumption/m-p/132039#M2906</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2006-04-11T09:49:05Z</dc:date>
    </item>
    <item>
      <title>Re: Lowest Power Consumption</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Lowest-Power-Consumption/m-p/132040#M2907</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;Perhaps you measure your current BEFORE the power regulator, and your current is its consumption...&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Apr 2006 14:49:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Lowest-Power-Consumption/m-p/132040#M2907</guid>
      <dc:creator>yb</dc:creator>
      <dc:date>2006-04-11T14:49:49Z</dc:date>
    </item>
    <item>
      <title>Re: Lowest Power Consumption</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Lowest-Power-Consumption/m-p/132041#M2908</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Mac:&lt;BR /&gt;You're right, I'm not sure which stop mode the micro is going into..&lt;BR /&gt;I tried putting the micro to stop1 but I can tell from seeing the current usage that its not going there, because the RTI is still running. Similarly I'm not sure if infact its going into Stop2 when I ask it to go there.&lt;BR /&gt;&lt;BR /&gt;Many floating pins on the board, a few connected to leds and buttons.. I've done a pullupenable on all of pins (irrespective) and set their data direction to in and set their states to low. But I get the same current profile.&lt;BR /&gt;&lt;BR /&gt;So I guess the question is, how can I tell which stop mode the mcu went into for real.&lt;BR /&gt;&lt;BR /&gt;yb:&lt;BR /&gt;the circuit doesn't have a regulator, just a direct 3.3V battery or power supply source.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Apr 2006 23:10:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Lowest-Power-Consumption/m-p/132041#M2908</guid>
      <dc:creator>kbu</dc:creator>
      <dc:date>2006-04-11T23:10:12Z</dc:date>
    </item>
    <item>
      <title>Re: Lowest Power Consumption</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Lowest-Power-Consumption/m-p/132042#M2909</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Do you have the PDC and PPDC bits set to 1 in the "System Power Management Status &amp;amp; Ctrl Reg 2" (SPMSC2 bits 0:1)? These need to be set for STOP2 mode.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Apr 2006 04:05:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Lowest-Power-Consumption/m-p/132042#M2909</guid>
      <dc:creator>paul</dc:creator>
      <dc:date>2006-04-12T04:05:24Z</dc:date>
    </item>
    <item>
      <title>Re: Lowest Power Consumption</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Lowest-Power-Consumption/m-p/132043#M2910</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Yep those bits are set.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Apr 2006 20:28:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Lowest-Power-Consumption/m-p/132043#M2910</guid>
      <dc:creator>kbu</dc:creator>
      <dc:date>2006-04-12T20:28:28Z</dc:date>
    </item>
    <item>
      <title>Re: Lowest Power Consumption</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Lowest-Power-Consumption/m-p/132044#M2911</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hai,&lt;/P&gt;&lt;P&gt;I am using stop3 and RAdio off .but i am facing problems regarding EXIT from it.&lt;/P&gt;&lt;P&gt;Can u help me please.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Apr 2006 19:16:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Lowest-Power-Consumption/m-p/132044#M2911</guid>
      <dc:creator>rao</dc:creator>
      <dc:date>2006-04-21T19:16:00Z</dc:date>
    </item>
    <item>
      <title>Re: Lowest Power Consumption</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Lowest-Power-Consumption/m-p/132045#M2912</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I finally got back to this problem. I just cannot get my MC13213 to get into low power consumption STOP2 mode.&lt;BR /&gt;the lowest power it seems to consume is around 900uA.&lt;BR /&gt;&lt;BR /&gt;My most of the IO pins on the board are floating (but I've set them all to outputs), its a direct feed from a 3.3V battery. nothing else on the board except for the TX/RX circuit (LC/baluns etc)&lt;BR /&gt;I'm using SMAC4.2 and have incorporated some of the functions from PWRLib into it.&lt;BR /&gt;&lt;BR /&gt;my code is basically this :&lt;BR /&gt;&lt;BR /&gt;case DEEP_SLEEP_STATE:&lt;BR /&gt;&lt;BR /&gt;UseMcuClock(); // switch to the internal clock&lt;BR /&gt;//Observations: I see clock speed drop to ~4Mhz in the debugger&lt;BR /&gt;&lt;BR /&gt;// set clockspeed to 2Mhz&lt;BR /&gt;PWRLib_ICG_Divider_Setup( N8, R2); //ICGC2 = ((07) | (N4) | (03) | (R0));&lt;BR /&gt;PWRLib_ICG_Mode( LOW_CLOCK); //ICGC1 = ((Clock6) | (05) | (Mode3) | (02));&lt;BR /&gt;//Observations: I see clock speed drop to ~2Mhz in the debugger&lt;BR /&gt;&lt;BR /&gt;SRTISC=0x00; //Disable wake up timer.&lt;BR /&gt;SPMSC1=0x00; // disable LVD&lt;BR /&gt;SPMSC2=0x00; // set PPDF flag to 0&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;MC13192ContReset(); // Place the MC13192 into Reset mode&lt;BR /&gt;//POTENTIAL PROBLEM: the SMAC function seems to set IRQPE = 0 (AN2493 seems to suggest setting it to 1)&lt;BR /&gt;&lt;BR /&gt;// set IRQPE to 1&lt;BR /&gt;IRQSC = 0x1E;&lt;BR /&gt;&lt;BR /&gt;//set all IO pins to outputs&lt;BR /&gt;(e.g. #define mPWRLib_SETUP_PORT_{ALL} PTADD = 0x00;\&lt;BR /&gt;PTAPE = 0x00;\&lt;BR /&gt;PTADD = 0xff; )&lt;BR /&gt;&lt;BR /&gt;PWRLib_SetMCUIOForPowerSavingMode();&lt;BR /&gt;&lt;BR /&gt;PWRLib_RTIClockStart( cPWR_RTITickTime, DozeDuration);&lt;BR /&gt;while ( PWRLib_RTIClockCheck() &amp;gt; 0)&lt;BR /&gt;{&lt;BR /&gt;SPMSC2 |= 0x03; // Sets PDC and PPDC bits for Stop2 mode&lt;BR /&gt;__asm STOP;&lt;BR /&gt;//OBSERVATIONS: Current consumption is around 900uA.&lt;BR /&gt;}&lt;BR /&gt;PWRLib_RTIClockStop();&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;RadioInit();&lt;BR /&gt;AppInit();&lt;BR /&gt;&lt;BR /&gt;// Restart to external clock appx. 10.8mS&lt;BR /&gt;MC13192Restart(); // Bring the MC13192 into the desired Idle condition.&lt;BR /&gt;MC13192Init();&lt;BR /&gt;&lt;BR /&gt;MLMESetChannelRequest(2);&lt;BR /&gt;MLMESetMC13192ClockRate(0); // Set initial Clk speed&lt;BR /&gt;UseExternalClock(); // switch clock sources from mcu to MC1319x CLKO&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;gi8AppStatus = TRANSMIT_DATA;&lt;BR /&gt;&lt;BR /&gt;break;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Any idea whats going on?&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Oct 2006 04:40:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Lowest-Power-Consumption/m-p/132045#M2912</guid>
      <dc:creator>kbu</dc:creator>
      <dc:date>2006-10-25T04:40:34Z</dc:date>
    </item>
  </channel>
</rss>