<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Need to program MC68HC908AS32ACFN - Desperately need help! in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Need-to-program-MC68HC908AS32ACFN-Desperately-need-help/m-p/131702#M2812</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hi Mike:&lt;BR /&gt;&lt;BR /&gt;Would a programming adapter help?&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=M68CPA08QF324448&amp;amp;parentCode=68HC08AS32A&amp;amp;nodeId=016246844976632420" rel="nofollow" target="_blank"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=M68CPA08QF324448&amp;amp;parentCode=68HC08AS32A&amp;amp;nodeId=016246844976632420&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Apr 2007 05:27:42 GMT</pubDate>
    <dc:creator>rocco</dc:creator>
    <dc:date>2007-04-25T05:27:42Z</dc:date>
    <item>
      <title>Need to program MC68HC908AS32ACFN - Desperately need help!</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Need-to-program-MC68HC908AS32ACFN-Desperately-need-help/m-p/131701#M2811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;&lt;P&gt;&lt;SPAN style="font-family: Helvetica; font-size: 1;"&gt;I have a bunch of MC68HC908AS32ACFN MCU's I need to program for a product line we have acquired. I'm very late on the project. This is new to me. I'm more of a programmer than an electrician. I have the latest Codewarrior for the HC08. I just need to get the code on the chips. I have a P&amp;amp;E 68HC08&amp;nbsp;MONO8 device, but thats only half the solution. I've tried to wire it to a chip socket... but not doing to well. Is there a 52-pin PLCC adapter that will accept the above MCU and a MONO8 header? Or a complete all-in-one board setup? Almost everything I see out there are for 64-pin QFP versions.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Helvetica; font-size: 1;"&gt;Thank you,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Helvetica; font-size: 1;"&gt;Mike&lt;/SPAN&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Apr 2007 04:58:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Need-to-program-MC68HC908AS32ACFN-Desperately-need-help/m-p/131701#M2811</guid>
      <dc:creator>mikev</dc:creator>
      <dc:date>2007-04-25T04:58:49Z</dc:date>
    </item>
    <item>
      <title>Re: Need to program MC68HC908AS32ACFN - Desperately need help!</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Need-to-program-MC68HC908AS32ACFN-Desperately-need-help/m-p/131702#M2812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hi Mike:&lt;BR /&gt;&lt;BR /&gt;Would a programming adapter help?&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=M68CPA08QF324448&amp;amp;parentCode=68HC08AS32A&amp;amp;nodeId=016246844976632420" rel="nofollow" target="_blank"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=M68CPA08QF324448&amp;amp;parentCode=68HC08AS32A&amp;amp;nodeId=016246844976632420&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Apr 2007 05:27:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Need-to-program-MC68HC908AS32ACFN-Desperately-need-help/m-p/131702#M2812</guid>
      <dc:creator>rocco</dc:creator>
      <dc:date>2007-04-25T05:27:42Z</dc:date>
    </item>
    <item>
      <title>Re: Need to program MC68HC908AS32ACFN - Desperately need help!</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Need-to-program-MC68HC908AS32ACFN-Desperately-need-help/m-p/131703#M2813</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello Mike,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;According to the MON08 Multilink manual, the following connections to the MON08 16-pin header are required for programming the HC908AS -&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Pin 2 = Gnd (Vss)&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Pin 4 = Reset&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Pin 6 = IRQ (Vtst)&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Pin 10 = PTA0&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Pin 12 = PTC0&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Pin 13 = Osc1&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Pin 14 = PTC1&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Pin 15 = Vout (Vdd)&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Pin 16 = PTC3&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;All other pins on the header are not connected.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;You will need to identify the pins on the PLCC52 that correspond to these connections, and connect accordingly.&amp;nbsp; I would use a through-hole type PLCC socket for more convenient point-to-point hand wiring.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;I assume you need to program the devices separately, rather than in situ on the board.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;Message Edited by bigmac on &lt;SPAN class="date_text"&gt;2007-04-25&lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;01:25 PM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Apr 2007 10:19:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Need-to-program-MC68HC908AS32ACFN-Desperately-need-help/m-p/131703#M2813</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2007-04-25T10:19:42Z</dc:date>
    </item>
  </channel>
</rss>