<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SMAC 4.1 installation in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SMAC-4-1-installation/m-p/131519#M2787</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi,&lt;BR /&gt;why do you want to re-compile the SMAC?&lt;BR /&gt;&lt;BR /&gt;It's better to use a demo project (like SimpleNetwork) which uses the lib, so you have less problems.&lt;BR /&gt;&lt;BR /&gt;I used the SMAC4.1 in a project and it's ok. There are any particular problems about installing SMAC.&lt;BR /&gt;&lt;BR /&gt;Try to modify for your purposes the existing projects.&lt;BR /&gt;&lt;BR /&gt;Bye&lt;BR /&gt;Stevasway&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Apr 2006 14:51:43 GMT</pubDate>
    <dc:creator>stevasway</dc:creator>
    <dc:date>2006-04-06T14:51:43Z</dc:date>
    <item>
      <title>SMAC 4.1 installation</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SMAC-4-1-installation/m-p/131518#M2786</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I use codewarrior SE which is a limited version and a MCS08GT60.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to use smac 4.1 for zigbee's communication and I have some problems. When I want to compile smac, an error message appear and tell the size of file simple_phy is too high.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Then when I want to include smac to my projet there ara others problems : the file number is limited at 32. If I don't include all files, I have several problem of linker at the compilation.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can you tell me how I can install and use SMAC 4.1&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Apr 2006 22:37:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/SMAC-4-1-installation/m-p/131518#M2786</guid>
      <dc:creator>martyseb63</dc:creator>
      <dc:date>2006-04-05T22:37:46Z</dc:date>
    </item>
    <item>
      <title>Re: SMAC 4.1 installation</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SMAC-4-1-installation/m-p/131519#M2787</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi,&lt;BR /&gt;why do you want to re-compile the SMAC?&lt;BR /&gt;&lt;BR /&gt;It's better to use a demo project (like SimpleNetwork) which uses the lib, so you have less problems.&lt;BR /&gt;&lt;BR /&gt;I used the SMAC4.1 in a project and it's ok. There are any particular problems about installing SMAC.&lt;BR /&gt;&lt;BR /&gt;Try to modify for your purposes the existing projects.&lt;BR /&gt;&lt;BR /&gt;Bye&lt;BR /&gt;Stevasway&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Apr 2006 14:51:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/SMAC-4-1-installation/m-p/131519#M2787</guid>
      <dc:creator>stevasway</dc:creator>
      <dc:date>2006-04-06T14:51:43Z</dc:date>
    </item>
    <item>
      <title>Re: SMAC 4.1 installation</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SMAC-4-1-installation/m-p/131520#M2788</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I strongly recommend you to get the latest SMAC codebase from BeeKit installer: &lt;A href="http://www.freescale.com/webapp/sps/site/overview.jsp?code=ZIGBEE"&gt;www.freescale.com/zigbee&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SMAC you have is very old.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 May 2013 17:26:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/SMAC-4-1-installation/m-p/131520#M2788</guid>
      <dc:creator>AlanCollins</dc:creator>
      <dc:date>2013-05-30T17:26:58Z</dc:date>
    </item>
  </channel>
</rss>