<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: ZigBee/SMAC - Doubt  about gMacRxOnWhenIdle_c</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ZigBee-SMAC-Doubt-about-gMacRxOnWhenIdle-c/m-p/131408#M2745</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There are no states for RxOnWhenIdle. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If TRUE, the device goes to RX mode when Idle.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If FALSE, the device use polling to retrieve messages from its parent. It can sleep when idle... &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;some of the internal code would validate this setting by using a simply if (RxOnWhenIdle)... So if you have a value = 4, it will work in some cases, but if there is a code that uses the if (TRUE == RxOnWhenIdle), then your code won't function correctly. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recommend you to use TRUE and FALSE values.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Apr 2014 05:36:51 GMT</pubDate>
    <dc:creator>AlanCollins</dc:creator>
    <dc:date>2014-04-15T05:36:51Z</dc:date>
    <item>
      <title>ZigBee/SMAC - Doubt  about gMacRxOnWhenIdle_c</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ZigBee-SMAC-Doubt-about-gMacRxOnWhenIdle-c/m-p/131406#M2743</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;SPAN&gt;Hello!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a doubt about the values that this attribute (gMacRxOnWhenIdle_c) can take.&amp;nbsp; The documentation says that it can be TRUE or FALSE but in my application it is 4.&amp;nbsp; Does it have a special meaning?&amp;nbsp; I mean, can the antenna be in more than two states?&amp;nbsp; Or does this mean just TRUE?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;--&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Alban Edit: title too vague renamed&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;P&gt;Message Edited by Alban on &lt;SPAN class="date_text"&gt;2007-04-20&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;05:52 PM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Apr 2007 22:36:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ZigBee-SMAC-Doubt-about-gMacRxOnWhenIdle-c/m-p/131406#M2743</guid>
      <dc:creator>UC3MZigbeeGroup</dc:creator>
      <dc:date>2007-04-20T22:36:28Z</dc:date>
    </item>
    <item>
      <title>Re: ZigBee/SMAC - Doubt  about gMacRxOnWhenIdle_c</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ZigBee-SMAC-Doubt-about-gMacRxOnWhenIdle-c/m-p/131407#M2744</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;P&gt;&lt;FONT size="2"&gt;Hi,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Please use the standard values (TRUE/FALSE). The others are used internally for the beacon tree feature.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;I hope this helps.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Nina&lt;/FONT&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Apr 2007 23:41:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ZigBee-SMAC-Doubt-about-gMacRxOnWhenIdle-c/m-p/131407#M2744</guid>
      <dc:creator>NLFSJ</dc:creator>
      <dc:date>2007-04-30T23:41:29Z</dc:date>
    </item>
    <item>
      <title>Re: ZigBee/SMAC - Doubt  about gMacRxOnWhenIdle_c</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ZigBee-SMAC-Doubt-about-gMacRxOnWhenIdle-c/m-p/131408#M2745</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There are no states for RxOnWhenIdle. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If TRUE, the device goes to RX mode when Idle.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If FALSE, the device use polling to retrieve messages from its parent. It can sleep when idle... &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;some of the internal code would validate this setting by using a simply if (RxOnWhenIdle)... So if you have a value = 4, it will work in some cases, but if there is a code that uses the if (TRUE == RxOnWhenIdle), then your code won't function correctly. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recommend you to use TRUE and FALSE values.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Apr 2014 05:36:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ZigBee-SMAC-Doubt-about-gMacRxOnWhenIdle-c/m-p/131408#M2745</guid>
      <dc:creator>AlanCollins</dc:creator>
      <dc:date>2014-04-15T05:36:51Z</dc:date>
    </item>
  </channel>
</rss>