<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Problem on switching FEI or FEE mode into FBE mode in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-on-switching-FEI-or-FEE-mode-into-FBE-mode/m-p/130976#M2606</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I'm working on the project that uses battery-operated PCB deploying freescale MC9S08GT60.&lt;/DIV&gt;&lt;DIV&gt;To save power in the normal mode, the PCB uses 32K external crystal oscillator in the FBE&lt;/DIV&gt;&lt;DIV&gt;(FLL Bypassed External) mode.&amp;nbsp; However, during power on or reset, I use internal oscillator&lt;/DIV&gt;&lt;DIV&gt;in the FEI (FLL Engaged Internal) at 5.5MHz. The problem is that I still cannot switch the mode&lt;/DIV&gt;&lt;DIV&gt;from FEI to FBE in low frequency. It always ended up with 4.4 MHz clock.&lt;/DIV&gt;&lt;DIV&gt;Another approach, during power on or reset, I use FEE (FLL Engaged External) at 4.5 MHz&lt;/DIV&gt;&lt;DIV&gt;using external oscillator. It can switch to FBE at 48KHz, but it does not work reliably during&lt;/DIV&gt;&lt;DIV&gt;reset operation. Many times I have to hit the reset switch several times,or it does not work at all.&lt;/DIV&gt;&lt;DIV&gt;Can anybody&amp;nbsp; have good advice or solution? I would appreciate if I can get the sample code.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks.&lt;/DIV&gt;&lt;DIV&gt;-Priyanto.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 Sep 2006 04:25:35 GMT</pubDate>
    <dc:creator>priyanto</dc:creator>
    <dc:date>2006-09-22T04:25:35Z</dc:date>
    <item>
      <title>Problem on switching FEI or FEE mode into FBE mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-on-switching-FEI-or-FEE-mode-into-FBE-mode/m-p/130976#M2606</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I'm working on the project that uses battery-operated PCB deploying freescale MC9S08GT60.&lt;/DIV&gt;&lt;DIV&gt;To save power in the normal mode, the PCB uses 32K external crystal oscillator in the FBE&lt;/DIV&gt;&lt;DIV&gt;(FLL Bypassed External) mode.&amp;nbsp; However, during power on or reset, I use internal oscillator&lt;/DIV&gt;&lt;DIV&gt;in the FEI (FLL Engaged Internal) at 5.5MHz. The problem is that I still cannot switch the mode&lt;/DIV&gt;&lt;DIV&gt;from FEI to FBE in low frequency. It always ended up with 4.4 MHz clock.&lt;/DIV&gt;&lt;DIV&gt;Another approach, during power on or reset, I use FEE (FLL Engaged External) at 4.5 MHz&lt;/DIV&gt;&lt;DIV&gt;using external oscillator. It can switch to FBE at 48KHz, but it does not work reliably during&lt;/DIV&gt;&lt;DIV&gt;reset operation. Many times I have to hit the reset switch several times,or it does not work at all.&lt;/DIV&gt;&lt;DIV&gt;Can anybody&amp;nbsp; have good advice or solution? I would appreciate if I can get the sample code.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks.&lt;/DIV&gt;&lt;DIV&gt;-Priyanto.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Sep 2006 04:25:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-on-switching-FEI-or-FEE-mode-into-FBE-mode/m-p/130976#M2606</guid>
      <dc:creator>priyanto</dc:creator>
      <dc:date>2006-09-22T04:25:35Z</dc:date>
    </item>
  </channel>
</rss>