<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックIs Zigbee compatible with Bluetooth?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Is-Zigbee-compatible-with-Bluetooth/m-p/130572#M2503</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;may i know if it is possible to establish a connection with Zigbee on the transmission side and bluetooth as the receiver?&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Sep 2006 22:31:36 GMT</pubDate>
    <dc:creator>leecw</dc:creator>
    <dc:date>2006-09-18T22:31:36Z</dc:date>
    <item>
      <title>Is Zigbee compatible with Bluetooth?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Is-Zigbee-compatible-with-Bluetooth/m-p/130572#M2503</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;may i know if it is possible to establish a connection with Zigbee on the transmission side and bluetooth as the receiver?&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Sep 2006 22:31:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Is-Zigbee-compatible-with-Bluetooth/m-p/130572#M2503</guid>
      <dc:creator>leecw</dc:creator>
      <dc:date>2006-09-18T22:31:36Z</dc:date>
    </item>
    <item>
      <title>Re: Is Zigbee compatible with Bluetooth?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Is-Zigbee-compatible-with-Bluetooth/m-p/130573#M2504</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;No, It is not possible. Sorry.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Sep 2006 03:20:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Is-Zigbee-compatible-with-Bluetooth/m-p/130573#M2504</guid>
      <dc:creator>rocco</dc:creator>
      <dc:date>2006-09-19T03:20:42Z</dc:date>
    </item>
    <item>
      <title>Re: Is Zigbee compatible with Bluetooth?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Is-Zigbee-compatible-with-Bluetooth/m-p/130574#M2505</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;The problem is that even if they both work on the 2.4GHz ISM band they use completely different kind of modulation. Frequency hopping over 79 1MHz channels for bluetooth and Direct Sequence for over 16 5MHz channels for Zigbee.&lt;BR /&gt;&lt;BR /&gt;Piero&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Sep 2006 17:45:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Is-Zigbee-compatible-with-Bluetooth/m-p/130574#M2505</guid>
      <dc:creator>Zap</dc:creator>
      <dc:date>2006-09-20T17:45:50Z</dc:date>
    </item>
    <item>
      <title>Re: Is Zigbee compatible with Bluetooth?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Is-Zigbee-compatible-with-Bluetooth/m-p/130575#M2506</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;hi guys:&lt;BR /&gt;&lt;BR /&gt;in reading this brings up the question: in a area with an active zigbe network will a bluetooth signal cause interferance?&lt;BR /&gt;&lt;BR /&gt;thanks!&lt;P&gt;Message Edited by jah on &lt;SPAN class="date_text"&gt;2006-09-21&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;01:06 PM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Sep 2006 01:05:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Is-Zigbee-compatible-with-Bluetooth/m-p/130575#M2506</guid>
      <dc:creator>jah</dc:creator>
      <dc:date>2006-09-22T01:05:55Z</dc:date>
    </item>
    <item>
      <title>Re: Is Zigbee compatible with Bluetooth?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Is-Zigbee-compatible-with-Bluetooth/m-p/130576#M2507</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Yes, a lot.&lt;BR /&gt;In my lab my Zigbee network "fight" vs. 3 bluetooth network and I can barely communicate at 1m distance. Comparing to my collegues I can say that zigbee suffer of interference much more than bluetooth does, also speacking with other engeneers they told me of severe decrese in communication when a bluetooth device enter in the area of their network. There are some paper describing coexistence with other protocol (see MC13192 section)&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Nov 2006 00:00:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Is-Zigbee-compatible-with-Bluetooth/m-p/130576#M2507</guid>
      <dc:creator>Zap</dc:creator>
      <dc:date>2006-11-11T00:00:31Z</dc:date>
    </item>
  </channel>
</rss>