<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Help - My AW32 spoiled twice in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-My-AW32-spoiled-twice/m-p/130472#M2477</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello Sany,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;You do not mention the nature and extent of the failure.&amp;nbsp; The following are some things that come to mind, that you would need to check.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;You will need to have some idea of the&amp;nbsp;anticipated current draw for the board.&amp;nbsp; Do the faulty boards significantly exceed this value?&amp;nbsp; Do any of the devices on the board run unexpectedly hot to touch?&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Do your&amp;nbsp;pre-fault boards exhibit any of these symptoms?&amp;nbsp; If so, I would tend to progressively build a blank board (by hand), and measure the current draw before and after each IC is installed.&amp;nbsp; Perhaps I would start with the MCU, and then add the peripheral devices one by one.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Do you still have any communications with&amp;nbsp;the faulty boards, via BDM module?&amp;nbsp; If so, you could test individual I/O lines, via debug, for remaining functionality.&amp;nbsp; You would particularly want to check that output lines are not "stuck at" either 0 or 1, and that you are achieving the full logic swing.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;I have great difficulty in reading your "schematic" - it is not really a schematic, but a type of net list, since the&amp;nbsp;interconnections between many of the&amp;nbsp;major devices are not explicitly shown.&amp;nbsp; And the size reduction from an original A3 sheet size to A4 does not aid clarity.&amp;nbsp; So it is not obvious which MCU&amp;nbsp;I/O pins are directly exposed to the "outside world".&amp;nbsp; It is also not clear whether you use any external pull-up resistors on unused, or exposed input pins.&amp;nbsp; This would possibly lessen the chance of damage caused by static discharge.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Sep 2006 11:02:39 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2006-09-20T11:02:39Z</dc:date>
    <item>
      <title>Help - My AW32 spoiled twice</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-My-AW32-spoiled-twice/m-p/130468#M2473</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I will be very appreciate if anyone could troubleshoot with me. I using this AW32 S08 MCU with 5V. The whole PCB with this AW32 was working fine. It just suddenly spoiled for no reason. And&amp;nbsp;it happend&amp;nbsp;twice for two of my PCB.&amp;nbsp;I didn't run this MCU for more than 10 minutes everytime.&amp;nbsp;Assuming there isn't any short circuit problem. No over voltage. I believe is the hardware circuit problem.&amp;nbsp;I double checked all the pins and voltage everything look fine. Any other reason that can cause a MCU spoil? My PCB has these loads: GLCD, max232, max485, MC7805T, 4xEEPROM 95256, DS1305, buzzer, 16MHz crystal, relayand a EM card reader module. Thank you in advance.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 17 Sep 2006 12:34:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-My-AW32-spoiled-twice/m-p/130468#M2473</guid>
      <dc:creator>Sany</dc:creator>
      <dc:date>2006-09-17T12:34:36Z</dc:date>
    </item>
    <item>
      <title>Re: Help - My AW32 spoiled twice</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-My-AW32-spoiled-twice/m-p/130469#M2474</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Is there any way you can send me more information on the physical layout of your board?&lt;BR /&gt;&lt;BR /&gt;A good start will be if you can send me two high definition pics of the two sides of the board.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 17 Sep 2006 17:43:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-My-AW32-spoiled-twice/m-p/130469#M2474</guid>
      <dc:creator>Jaux</dc:creator>
      <dc:date>2006-09-17T17:43:51Z</dc:date>
    </item>
    <item>
      <title>Re: Help - My AW32 spoiled twice</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-My-AW32-spoiled-twice/m-p/130470#M2475</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;These links have all the pictures.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;A href="http://www25.brinkster.com/sanylcs/pcbback.html" rel="nofollow" target="_blank"&gt;http://www25.brinkster.com/sanylcs/pcbback.html&lt;/A&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;A href="http://www25.brinkster.com/sanylcs/pcbfrnt.html" rel="nofollow" target="_blank"&gt;http://www25.brinkster.com/sanylcs/pcbfrnt.html&lt;/A&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;A href="http://www25.brinkster.com/sanylcs/sch.html" rel="nofollow" target="_blank"&gt;http://www25.brinkster.com/sanylcs/sch.html&lt;/A&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;ty for reply.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Sep 2006 18:15:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-My-AW32-spoiled-twice/m-p/130470#M2475</guid>
      <dc:creator>Sany</dc:creator>
      <dc:date>2006-09-19T18:15:06Z</dc:date>
    </item>
    <item>
      <title>Re: Help - My AW32 spoiled twice</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-My-AW32-spoiled-twice/m-p/130471#M2476</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Some quick remarks:&lt;BR /&gt;&lt;BR /&gt;1. The MAX232A normally uses 0.1uF caps for the charge pump ( MAX232 uses 1.0 uF ) 10uF is way out of the spec.&lt;BR /&gt;&lt;BR /&gt;2. LP1 and LP2 I presume are "normal" LED's - with the bias resistors of 330E you would sink 10mA thru PTE0 and PTE1. Make sure you configure these as 'high output drive' in register PTEDS. This is a bit high for my liking - and I do not drive LED's directly from MCU pins&lt;BR /&gt;&lt;BR /&gt;3. The physical layout look ok - but the schematic is difficult to read. Also I tend to be rather conservative with pin loadings and fan-outs - I have seen a couple of 'adventurous' &lt;BR /&gt;moves in the design - I would advise to check all pin loadings against the spec and make sure the chip can handle it.&lt;BR /&gt;&lt;BR /&gt;Freescale MCU's are tough little suckers, and you must have done something serious to blow it. I see you have several unbuffered output pins directly from the MCU - what goes in there?&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Sep 2006 21:55:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-My-AW32-spoiled-twice/m-p/130471#M2476</guid>
      <dc:creator>Jaux</dc:creator>
      <dc:date>2006-09-19T21:55:31Z</dc:date>
    </item>
    <item>
      <title>Re: Help - My AW32 spoiled twice</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-My-AW32-spoiled-twice/m-p/130472#M2477</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello Sany,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;You do not mention the nature and extent of the failure.&amp;nbsp; The following are some things that come to mind, that you would need to check.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;You will need to have some idea of the&amp;nbsp;anticipated current draw for the board.&amp;nbsp; Do the faulty boards significantly exceed this value?&amp;nbsp; Do any of the devices on the board run unexpectedly hot to touch?&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Do your&amp;nbsp;pre-fault boards exhibit any of these symptoms?&amp;nbsp; If so, I would tend to progressively build a blank board (by hand), and measure the current draw before and after each IC is installed.&amp;nbsp; Perhaps I would start with the MCU, and then add the peripheral devices one by one.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Do you still have any communications with&amp;nbsp;the faulty boards, via BDM module?&amp;nbsp; If so, you could test individual I/O lines, via debug, for remaining functionality.&amp;nbsp; You would particularly want to check that output lines are not "stuck at" either 0 or 1, and that you are achieving the full logic swing.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;I have great difficulty in reading your "schematic" - it is not really a schematic, but a type of net list, since the&amp;nbsp;interconnections between many of the&amp;nbsp;major devices are not explicitly shown.&amp;nbsp; And the size reduction from an original A3 sheet size to A4 does not aid clarity.&amp;nbsp; So it is not obvious which MCU&amp;nbsp;I/O pins are directly exposed to the "outside world".&amp;nbsp; It is also not clear whether you use any external pull-up resistors on unused, or exposed input pins.&amp;nbsp; This would possibly lessen the chance of damage caused by static discharge.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Sep 2006 11:02:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-My-AW32-spoiled-twice/m-p/130472#M2477</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2006-09-20T11:02:39Z</dc:date>
    </item>
    <item>
      <title>Re: Help - My AW32 spoiled twice</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-My-AW32-spoiled-twice/m-p/130473#M2478</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;ty for all the troubleshootings. I think I must have done something seriously damaged the MCU. Because I did some solderings before that. And some component onboard testings which probably over voltage and damged it.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Sep 2006 11:13:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-My-AW32-spoiled-twice/m-p/130473#M2478</guid>
      <dc:creator>Sany</dc:creator>
      <dc:date>2006-09-20T11:13:18Z</dc:date>
    </item>
  </channel>
</rss>