<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: High Temperature Application</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/High-Temperature-Application/m-p/130467#M2472</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Hi mikefr&lt;/DIV&gt;&lt;DIV&gt;A design that runs a 125C part at 180C would be on "thin ice" indeed&lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;In testing parts at elevated temps (_not_ Freescale's, so can't speak for them), a fairly common result is a gradual increase in die leakage currents until catastrophic failure occurs.&amp;nbsp;&amp;nbsp; This happens sooner rather than later.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;So this makes the question not "will it work at 180C" -- but "how long will it work at 180C,"&amp;nbsp; and the answer is usually "not very long."&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Hope your equipment isn't going into commercial aircraft -- is it?&lt;IMG alt=":smileysurprised:" class="emoticon emoticon-smileysurprised" id="smileysurprised" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-surprised.gif" title="Smiley Surprised" /&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 14 Apr 2007 02:06:09 GMT</pubDate>
    <dc:creator>Curt</dc:creator>
    <dc:date>2007-04-14T02:06:09Z</dc:date>
    <item>
      <title>High Temperature Application</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/High-Temperature-Application/m-p/130464#M2469</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Forum,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I am searching for an HCS08 part, that has a history of operating at 165 degrees Centigrade.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Anyone had any success with a HCS08 at this temperature ????&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks,&lt;/DIV&gt;&lt;DIV&gt;MikeF&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Apr 2007 11:41:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/High-Temperature-Application/m-p/130464#M2469</guid>
      <dc:creator>mikefr</dc:creator>
      <dc:date>2007-04-13T11:41:24Z</dc:date>
    </item>
    <item>
      <title>Re: High Temperature Application</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/High-Temperature-Application/m-p/130465#M2470</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Mike,&lt;BR /&gt;&lt;BR /&gt;165°C is well above the maximum junction temperature they currently support: 135°C.&lt;BR /&gt;And that 135°C is supporting without damage, it is not under normally operating conditions above 125°C.&lt;BR /&gt;&lt;BR /&gt;I think you need to wait for new special high temperature designs, if you wish to use an S08.&lt;BR /&gt;&lt;BR /&gt;Alban.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Apr 2007 16:43:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/High-Temperature-Application/m-p/130465#M2470</guid>
      <dc:creator>Alban</dc:creator>
      <dc:date>2007-04-13T16:43:46Z</dc:date>
    </item>
    <item>
      <title>Re: High Temperature Application</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/High-Temperature-Application/m-p/130466#M2471</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;This is above the recommended, but we use sevel uC which are rated at 125 degC, in a 180 degC environment.&amp;nbsp; We just have no history with the HCS08 at this temperature.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;We use HC11 @ elevetated temp's.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;---Mike&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Hi Mike,&lt;BR /&gt;&lt;BR /&gt;165°C is well above the maximum junction temperature they currently support: 135°C.&lt;BR /&gt;And that 135°C is supporting without damage, it is not under normally operating conditions above 125°C.&lt;BR /&gt;&lt;BR /&gt;I think you need to wait for new special high temperature designs, if you wish to use an S08.&lt;BR /&gt;&lt;BR /&gt;Alban.&lt;BR /&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Apr 2007 22:53:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/High-Temperature-Application/m-p/130466#M2471</guid>
      <dc:creator>mikefr</dc:creator>
      <dc:date>2007-04-13T22:53:26Z</dc:date>
    </item>
    <item>
      <title>Re: High Temperature Application</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/High-Temperature-Application/m-p/130467#M2472</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Hi mikefr&lt;/DIV&gt;&lt;DIV&gt;A design that runs a 125C part at 180C would be on "thin ice" indeed&lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;In testing parts at elevated temps (_not_ Freescale's, so can't speak for them), a fairly common result is a gradual increase in die leakage currents until catastrophic failure occurs.&amp;nbsp;&amp;nbsp; This happens sooner rather than later.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;So this makes the question not "will it work at 180C" -- but "how long will it work at 180C,"&amp;nbsp; and the answer is usually "not very long."&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Hope your equipment isn't going into commercial aircraft -- is it?&lt;IMG alt=":smileysurprised:" class="emoticon emoticon-smileysurprised" id="smileysurprised" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-surprised.gif" title="Smiley Surprised" /&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 14 Apr 2007 02:06:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/High-Temperature-Application/m-p/130467#M2472</guid>
      <dc:creator>Curt</dc:creator>
      <dc:date>2007-04-14T02:06:09Z</dc:date>
    </item>
  </channel>
</rss>